<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: DCIC IMX6 Solo</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DCIC-IMX6-Solo/m-p/1345916#M180599</link>
    <description>&lt;P&gt;Thank you for you reply.&amp;nbsp; We wrote a custom kernel for our needs so I'd like to just stick with this to get this working.&amp;nbsp; I've no doubt the DCIC test would work accordingly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I set the&amp;nbsp;&lt;FONT&gt;IOMUXC_GPR10&lt;/FONT&gt; register to HDMI for DCIC1 and things seem to be updating.&amp;nbsp; We are using IPU1 DI0 do you know why this wouldn't work but HDMI would?&lt;/P&gt;&lt;P&gt;Also DCIC chapter mentions 16 ROI's for each DCIC but the register memory map doesn't mention where to set the additional ROI's.&amp;nbsp; Do you know the register locations to set up additional regions?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Micah Rudy&lt;/P&gt;</description>
    <pubDate>Fri, 24 Sep 2021 13:34:07 GMT</pubDate>
    <dc:creator>mjrudy</dc:creator>
    <dc:date>2021-09-24T13:34:07Z</dc:date>
    <item>
      <title>DCIC IMX6 Solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DCIC-IMX6-Solo/m-p/1339986#M180081</link>
      <description>&lt;P&gt;I'm trying to configure the DCIC checking for an IMX6 SOLO.&amp;nbsp; We run a bare metal BSP so I'm basically just trying to setup the registers and get a CRC to output.&lt;/P&gt;&lt;P&gt;I've followed the chapter 20 of the i.MX 6 SOLO/Dual Lite Reference Manual to set the values in the registers to use IPU1 and DCIC 1.&amp;nbsp; I turned on the clock via CG12 register bit.&amp;nbsp; I'm only trying to get 1 ROI to generate a CRC at the moment.&amp;nbsp; The ROI calculated signature register is always 0.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried following the Linux kernel's logic to set this up&amp;nbsp; but can someone tell me what I'm missing?&lt;/P&gt;&lt;P&gt;Steps:&lt;/P&gt;&lt;P&gt;Turn on the Clock.&lt;/P&gt;&lt;P&gt;Mux the GRP10 register to configure DCIC 1 to IPU 1&lt;/P&gt;&lt;P&gt;configure the ROI just using offsets of 10 for x and y with a size of 100 for x and y display is 480x800&lt;/P&gt;&lt;P&gt;Enable the&amp;nbsp; checking and ROI.&lt;/P&gt;&lt;P&gt;I would expect based on the document that is would be seeing come calculated CRC in the register but it is always 0.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 19:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DCIC-IMX6-Solo/m-p/1339986#M180081</guid>
      <dc:creator>mjrudy</dc:creator>
      <dc:date>2021-09-14T19:41:18Z</dc:date>
    </item>
    <item>
      <title>Re: DCIC IMX6 Solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DCIC-IMX6-Solo/m-p/1345896#M180598</link>
      <description>&lt;P&gt;I would suggest you test it on Linux BSP.&lt;/P&gt;
&lt;P&gt;For you reference&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX6-DCIC-freeze/m-p/631743" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX6-DCIC-freeze/m-p/631743&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 13:20:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DCIC-IMX6-Solo/m-p/1345896#M180598</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-09-24T13:20:07Z</dc:date>
    </item>
    <item>
      <title>Re: DCIC IMX6 Solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DCIC-IMX6-Solo/m-p/1345916#M180599</link>
      <description>&lt;P&gt;Thank you for you reply.&amp;nbsp; We wrote a custom kernel for our needs so I'd like to just stick with this to get this working.&amp;nbsp; I've no doubt the DCIC test would work accordingly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I set the&amp;nbsp;&lt;FONT&gt;IOMUXC_GPR10&lt;/FONT&gt; register to HDMI for DCIC1 and things seem to be updating.&amp;nbsp; We are using IPU1 DI0 do you know why this wouldn't work but HDMI would?&lt;/P&gt;&lt;P&gt;Also DCIC chapter mentions 16 ROI's for each DCIC but the register memory map doesn't mention where to set the additional ROI's.&amp;nbsp; Do you know the register locations to set up additional regions?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Micah Rudy&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 13:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DCIC-IMX6-Solo/m-p/1345916#M180599</guid>
      <dc:creator>mjrudy</dc:creator>
      <dc:date>2021-09-24T13:34:07Z</dc:date>
    </item>
  </channel>
</rss>