<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic how to switch uboot debug console from uart1 to uart3 for linux 5.10.9 (uboot 2020.04) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/how-to-switch-uboot-debug-console-from-uart1-to-uart3-for-linux/m-p/1345307#M180551</link>
    <description>&lt;P&gt;dear friends,&lt;/P&gt;&lt;P&gt;I am porting uboot code based on linux 5.10.9 for&amp;nbsp; imx6 solo processor, I plan to use uart3 as the uboot debug console port. I modified the device tree as:&lt;/P&gt;&lt;P&gt;chosen {&lt;/P&gt;&lt;P&gt;stdout-path=&amp;amp;uart3;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;I also modified&amp;nbsp; mx6sabresd.c file as:&lt;/P&gt;&lt;P&gt;setup_iOmux_uart(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;SETUP_IOMUX_PADS(uart3_pads);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;and modified the uart3_pads definitions correspondingly.&lt;/P&gt;&lt;P&gt;Do I need to modify the CONS_INDEX =1 to CONS_INDEX=3?&lt;/P&gt;&lt;P&gt;any other modifications needed?&lt;/P&gt;&lt;P&gt;would you please direct me to the documentation if possible.&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;Hai&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 22:05:22 GMT</pubDate>
    <dc:creator>hailiu</dc:creator>
    <dc:date>2021-09-23T22:05:22Z</dc:date>
    <item>
      <title>how to switch uboot debug console from uart1 to uart3 for linux 5.10.9 (uboot 2020.04)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-switch-uboot-debug-console-from-uart1-to-uart3-for-linux/m-p/1345307#M180551</link>
      <description>&lt;P&gt;dear friends,&lt;/P&gt;&lt;P&gt;I am porting uboot code based on linux 5.10.9 for&amp;nbsp; imx6 solo processor, I plan to use uart3 as the uboot debug console port. I modified the device tree as:&lt;/P&gt;&lt;P&gt;chosen {&lt;/P&gt;&lt;P&gt;stdout-path=&amp;amp;uart3;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;I also modified&amp;nbsp; mx6sabresd.c file as:&lt;/P&gt;&lt;P&gt;setup_iOmux_uart(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;SETUP_IOMUX_PADS(uart3_pads);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;and modified the uart3_pads definitions correspondingly.&lt;/P&gt;&lt;P&gt;Do I need to modify the CONS_INDEX =1 to CONS_INDEX=3?&lt;/P&gt;&lt;P&gt;any other modifications needed?&lt;/P&gt;&lt;P&gt;would you please direct me to the documentation if possible.&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;Hai&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 22:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-switch-uboot-debug-console-from-uart1-to-uart3-for-linux/m-p/1345307#M180551</guid>
      <dc:creator>hailiu</dc:creator>
      <dc:date>2021-09-23T22:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: how to switch uboot debug console from uart1 to uart3 for linux 5.10.9 (uboot 2020.04)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-switch-uboot-debug-console-from-uart1-to-uart3-for-linux/m-p/1345336#M180555</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can look at #define CONSOLE_DEV in&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6sabresd.h?h=lf_v2021.04" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6sabresd.h?h=lf_v2021.04&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 00:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-switch-uboot-debug-console-from-uart1-to-uart3-for-linux/m-p/1345336#M180555</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-09-24T00:33:21Z</dc:date>
    </item>
  </channel>
</rss>