<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C1 on pads GPIO_SD_B1_04 &amp;amp; GPIO_AD_B1_05 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I2C1-on-pads-GPIO-SD-B1-04-amp-GPIO-AD-B1-05/m-p/1345037#M180537</link>
    <description>&lt;P&gt;Seems like this post,&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT/target-crashes-writing-to-register-SW-MUX-CTL-PAD-GPIO-SD-B1-05/m-p/1148049" target="_blank"&gt;Re: target crashes writing to register SW_MUX_CTL_... - NXP Community&lt;/A&gt;, confirms that using&amp;nbsp;.readSampleClksrc=kFlexSPIReadSampleClk_LoopbackInternally; will work and it seems to work for me, so far.&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 11:45:42 GMT</pubDate>
    <dc:creator>markdodd</dc:creator>
    <dc:date>2021-09-23T11:45:42Z</dc:date>
    <item>
      <title>I2C1 on pads GPIO_SD_B1_04 &amp; GPIO_AD_B1_05</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C1-on-pads-GPIO-SD-B1-04-amp-GPIO-AD-B1-05/m-p/1345004#M180532</link>
      <description>&lt;P&gt;MIMXRT1061DVL6&lt;BR /&gt;Is it possible to use I2C1 on pads GPIO_SD_B1_04 &amp;amp; GPIO_AD_B1_05 when booting and running XIP from QSPI NOR Flash?&lt;/P&gt;&lt;P&gt;On an XIP application being started, GPIO_SD_B1_04 is FLEXSPIB_SCLK and GPIO_AD_B1_05 is FLEXSPIA_DQS.&lt;/P&gt;&lt;P&gt;We are using FLEXSPIA, with a 3.3V IS25LP064A-JBLE.&lt;/P&gt;&lt;P&gt;Configuration:&lt;/P&gt;&lt;P&gt;const flexspi_nor_config_t qspiflash_config = {&lt;BR /&gt;.memConfig =&lt;BR /&gt;{&lt;BR /&gt;.tag = FLEXSPI_CFG_BLK_TAG,&lt;BR /&gt;.version = FLEXSPI_CFG_BLK_VERSION,&lt;BR /&gt;.readSampleClksrc=kFlexSPIReadSampleClk_LoopbackFromDqsPad,&lt;BR /&gt;.csHoldTime = 3u,&lt;BR /&gt;.csSetupTime = 3u,&lt;BR /&gt;.sflashPadType = kSerialFlash_4Pads,&lt;BR /&gt;.serialClkFreq = kFlexSpiSerialClk_100MHz,&lt;BR /&gt;.sflashA1Size = 8u * 1024u * 1024u,&lt;BR /&gt;.lookupTable =&lt;BR /&gt;{&lt;BR /&gt;// Read LUTs&lt;BR /&gt;FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),&lt;BR /&gt;FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),&lt;BR /&gt;},&lt;BR /&gt;},&lt;BR /&gt;.pageSize = 256u,&lt;BR /&gt;.sectorSize = 4u * 1024u,&lt;BR /&gt;.blockSize = 64u * 1024u,&lt;BR /&gt;.isUniformBlockSize = false,&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Can I use some other setting for .readSampleClkSrc, still run at 100MHz and free up GPIO_AD_B1_04/5?&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 10:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C1-on-pads-GPIO-SD-B1-04-amp-GPIO-AD-B1-05/m-p/1345004#M180532</guid>
      <dc:creator>markdodd</dc:creator>
      <dc:date>2021-09-23T10:17:14Z</dc:date>
    </item>
    <item>
      <title>Re: I2C1 on pads GPIO_SD_B1_04 &amp; GPIO_AD_B1_05</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C1-on-pads-GPIO-SD-B1-04-amp-GPIO-AD-B1-05/m-p/1345037#M180537</link>
      <description>&lt;P&gt;Seems like this post,&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT/target-crashes-writing-to-register-SW-MUX-CTL-PAD-GPIO-SD-B1-05/m-p/1148049" target="_blank"&gt;Re: target crashes writing to register SW_MUX_CTL_... - NXP Community&lt;/A&gt;, confirms that using&amp;nbsp;.readSampleClksrc=kFlexSPIReadSampleClk_LoopbackInternally; will work and it seems to work for me, so far.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 11:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C1-on-pads-GPIO-SD-B1-04-amp-GPIO-AD-B1-05/m-p/1345037#M180537</guid>
      <dc:creator>markdodd</dc:creator>
      <dc:date>2021-09-23T11:45:42Z</dc:date>
    </item>
  </channel>
</rss>