<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MSCALE-Can't open USB device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1344868#M180519</link>
    <description>&lt;P&gt;Hello Aldo,&lt;/P&gt;&lt;P&gt;Yes, I have understood we can create a CFG file with the contents of the worksheet "DCD CFG" tab but my problem is how to use it.&lt;/P&gt;&lt;P&gt;I have a iMX8QxP MEK evaluation board and I am using Yocto project.&lt;BR /&gt;I have the UM11455-V2X_RoadLINK_Software_User_Manual.pdf and the UM11456-V2X_RoadLINK_Software_Developer_Manual.pdf documents.&lt;BR /&gt;But unfortunately I have no clue about SCU or SCFW.&lt;/P&gt;&lt;P&gt;So I would like to know:&lt;BR /&gt;- where I could find SCFW sources&lt;BR /&gt;- how to build SCFW with the "DCD CFG" file&lt;BR /&gt;- how to integrate in the Yocto project.&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;BR /&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 08:17:47 GMT</pubDate>
    <dc:creator>PBR</dc:creator>
    <dc:date>2021-09-23T08:17:47Z</dc:date>
    <item>
      <title>MSCALE-Can't open USB device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1340665#M180153</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using a iMX8QxP MEK evaluation board and I would like to use NXP i.MX/Mscale DDR Tool V3.20.&lt;/P&gt;&lt;P&gt;- The MEK eval board is in Serial mode (switches: 0001)&lt;/P&gt;&lt;P&gt;- I open Mscale as administrator on a Windows PC&lt;/P&gt;&lt;P&gt;- I plug USB-C from the MEK eval board to the Win PC: on the Device Manager window, I can see HID-compliant device + USB Input device displayed&lt;/P&gt;&lt;P&gt;- I plug the debug USB from the MEK eval board to the Win PC: now, when I click "Search" button of the Mscale window, I can see 4 COMs.&lt;/P&gt;&lt;P&gt;- In the Mscale window:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; o I select one of the 4 COMs&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; o I click on "Connect" button&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; o I select a DDR script (for example,.../script/mx8m/mx8m_micron_lpddr4_3gb_2d_1600m_200m_50m_32bit_RPAv25.ds)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; o Target =MX8M, Clock=Default, DDR=LPDDR4, Density=Default (values by default but are they correct?)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; o I click on "Download" button&lt;/P&gt;&lt;P&gt;I have this message:&lt;/P&gt;&lt;P&gt;ERROR: Can't open USB device!!!&lt;BR /&gt;Please check if the correct target is selected and set to the serial download mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried with the 4 COMs, same result.&lt;/P&gt;&lt;P&gt;I tried with another PC, same result.&lt;/P&gt;&lt;P&gt;I am sure the MEK board is in serial mode as I can use uuu to download a new program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is my Mscale version correct? (V3.20)&lt;/P&gt;&lt;P&gt;I run out of ideas... If you have any suggestions, please tell me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 14:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1340665#M180153</guid>
      <dc:creator>PBR</dc:creator>
      <dc:date>2021-09-15T14:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: MSCALE-Can't open USB device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1342908#M180369</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You're using the incorrect version of the tool, please try with this one:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There you'll find the mx8_ddr_stress_test_ER14_installation.zip for download, please try it.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 19:24:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1342908#M180369</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-09-20T19:24:46Z</dc:date>
    </item>
    <item>
      <title>Re: MSCALE-Can't open USB device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1344039#M180476</link>
      <description>&lt;P&gt;Hello Aldo,&lt;/P&gt;&lt;P&gt;Thank you for your help, yes it works.&lt;/P&gt;&lt;P&gt;The win app does not generate code and it is now the Excel file which generates the code to program DDR memory with the SCU firmware.&lt;/P&gt;&lt;P&gt;My understanding is the Uboot does not have to be changed anymore but I have to rebuild SCU firmware. Am I right?&lt;/P&gt;&lt;P&gt;I am using Yocto project. How could I integrate data from "DCD CFG" excel's tab in the bootloader's code?&lt;BR /&gt;Do you have any document which explains how to build SCU firmware?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you for your help.&lt;BR /&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 12:38:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1344039#M180476</guid>
      <dc:creator>PBR</dc:creator>
      <dc:date>2021-09-22T12:38:18Z</dc:date>
    </item>
    <item>
      <title>Re: MSCALE-Can't open USB device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1344323#M180491</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Glad to hear that it is now working, it is pretty straight forward, as specified in the community document:&lt;/P&gt;
&lt;P&gt;DCD CFG file: This format is the configuration file used specifically by the SCU Firmware (SCFW). In this scenario, the user copies the contents in this worksheet tab and pastes it to a text file, naming the document with the “.cfg” file extension and placing this file in the appropriate SCFW board file directory.&lt;BR /&gt;&lt;BR /&gt;Hope this helps,&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 18:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1344323#M180491</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-09-22T18:51:17Z</dc:date>
    </item>
    <item>
      <title>Re: MSCALE-Can't open USB device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1344868#M180519</link>
      <description>&lt;P&gt;Hello Aldo,&lt;/P&gt;&lt;P&gt;Yes, I have understood we can create a CFG file with the contents of the worksheet "DCD CFG" tab but my problem is how to use it.&lt;/P&gt;&lt;P&gt;I have a iMX8QxP MEK evaluation board and I am using Yocto project.&lt;BR /&gt;I have the UM11455-V2X_RoadLINK_Software_User_Manual.pdf and the UM11456-V2X_RoadLINK_Software_Developer_Manual.pdf documents.&lt;BR /&gt;But unfortunately I have no clue about SCU or SCFW.&lt;/P&gt;&lt;P&gt;So I would like to know:&lt;BR /&gt;- where I could find SCFW sources&lt;BR /&gt;- how to build SCFW with the "DCD CFG" file&lt;BR /&gt;- how to integrate in the Yocto project.&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;BR /&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 08:17:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1344868#M180519</guid>
      <dc:creator>PBR</dc:creator>
      <dc:date>2021-09-23T08:17:47Z</dc:date>
    </item>
    <item>
      <title>Re: MSCALE-Can't open USB device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1346009#M180608</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;for this you may refer to the following guide, I think this may be useful to understand more about the SCFW:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-started/ta-p/1121153" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-started/ta-p/1121153&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, you may refer to the documentation inside the porting kit.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 19:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1346009#M180608</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-09-24T19:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: MSCALE-Can't open USB device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1349039#M180879</link>
      <description>&lt;P&gt;Thank you Aldo, it works.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 09:05:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MSCALE-Can-t-open-USB-device/m-p/1349039#M180879</guid>
      <dc:creator>PBR</dc:creator>
      <dc:date>2021-09-30T09:05:04Z</dc:date>
    </item>
  </channel>
</rss>