<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8QuadXPlus LPDDR4 CA SWAP in Channel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QuadXPlus-LPDDR4-CA-SWAP-in-Channel/m-p/1343601#M180427</link>
    <description>&lt;P&gt;Dear&lt;/P&gt;&lt;P&gt;Could you confirm if there is any restriction of CA(Command &amp;amp; Address) swapping on LPDDR4?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 22 Sep 2021 02:58:36 GMT</pubDate>
    <dc:creator>Wenhai_05</dc:creator>
    <dc:date>2021-09-22T02:58:36Z</dc:date>
    <item>
      <title>IMX8QuadXPlus LPDDR4 CA SWAP in Channel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QuadXPlus-LPDDR4-CA-SWAP-in-Channel/m-p/1343601#M180427</link>
      <description>&lt;P&gt;Dear&lt;/P&gt;&lt;P&gt;Could you confirm if there is any restriction of CA(Command &amp;amp; Address) swapping on LPDDR4?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 02:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QuadXPlus-LPDDR4-CA-SWAP-in-Channel/m-p/1343601#M180427</guid>
      <dc:creator>Wenhai_05</dc:creator>
      <dc:date>2021-09-22T02:58:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QuadXPlus LPDDR4 CA SWAP in Channel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QuadXPlus-LPDDR4-CA-SWAP-in-Channel/m-p/1343777#M180447</link>
      <description>&lt;P&gt;As long as it complies with JEDEC specifications，no special. The details design you can refer to our hardware user guide document.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 07:16:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QuadXPlus-LPDDR4-CA-SWAP-in-Channel/m-p/1343777#M180447</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-09-22T07:16:24Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QuadXPlus LPDDR4 CA SWAP in Channel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QuadXPlus-LPDDR4-CA-SWAP-in-Channel/m-p/1343809#M180454</link>
      <description>&lt;P&gt;Dear&lt;/P&gt;&lt;P&gt;It is not stated in JEDEC specification.&amp;nbsp;I think it depends on the features of DDR PHY and Controller.&lt;/P&gt;&lt;P&gt;As I know, IMX8QXP support data bus swapping. I can fill in my data configuration to get corresponding code. Refer to attachment, which is snapped in worksheet (BoardDataBusConfig) of&amp;nbsp; MX8QXP_C0_B0_LPDDR4_RPA_1.2GHz_V15.xlsx.&lt;/P&gt;&lt;P&gt;Similarly, due to layout, I have the requirement of CA swapping. Such as, DDR_DCF00 is configured to CA2_A, I want to configure it as CA5_A.&lt;/P&gt;&lt;P&gt;There are not these information in user guide .&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 07:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QuadXPlus-LPDDR4-CA-SWAP-in-Channel/m-p/1343809#M180454</guid>
      <dc:creator>Wenhai_05</dc:creator>
      <dc:date>2021-09-22T07:57:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QuadXPlus LPDDR4 CA SWAP in Channel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QuadXPlus-LPDDR4-CA-SWAP-in-Channel/m-p/1343872#M180463</link>
      <description>&lt;P&gt;Swapping of the CA lines is not supported.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 09:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QuadXPlus-LPDDR4-CA-SWAP-in-Channel/m-p/1343872#M180463</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-09-22T09:14:48Z</dc:date>
    </item>
  </channel>
</rss>