<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: googletest shared library</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/googletest-shared-library/m-p/1343316#M180409</link>
    <description>&lt;P&gt;Hello lchen,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think you might consult the community from yocto since you are using googletest and its not part of the BSP:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.yoctoproject.org/community/mailing-lists/" target="_blank"&gt;https://www.yoctoproject.org/community/mailing-lists/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 21 Sep 2021 14:00:51 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2021-09-21T14:00:51Z</dc:date>
    <item>
      <title>googletest shared library</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/googletest-shared-library/m-p/1342880#M180366</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to include libgtest.so into the iMX8 image. I added googletest to IMAGE_INSTALL and added the following line to sources/meta-openembedded/meta-oe/recipes-test/googletest/googletest_git.bb:&lt;/P&gt;&lt;P&gt;EXTRA_OECMAKE = "-DBUILD_SHARED_LIBS=ON "&lt;/P&gt;&lt;P&gt;The shared libraries were built successfully. However, there are errors in do_package_qc as following:&lt;/P&gt;&lt;P&gt;ERROR: googletest-1.10.0-r0 do_package_qa: QA Issue: -dev package googletest-dev contains non-symlink .so '/usr/lib/libgmock.so'&lt;BR /&gt;-dev package googletest-dev contains non-symlink .so '/usr/lib/libgtest_main.so'&lt;BR /&gt;-dev package googletest-dev contains non-symlink .so '/usr/lib/libgmock_main.so'&lt;BR /&gt;-dev package googletest-dev contains non-symlink .so '/usr/lib/libgtest.so' [dev-elf]&lt;BR /&gt;ERROR: googletest-1.10.0-r0 do_package_qa: QA run found fatal errors. Please consider fixing them.&lt;/P&gt;&lt;P&gt;Any idea to fix this?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lijun&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 17:37:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/googletest-shared-library/m-p/1342880#M180366</guid>
      <dc:creator>lchen</dc:creator>
      <dc:date>2021-09-20T17:37:41Z</dc:date>
    </item>
    <item>
      <title>Re: googletest shared library</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/googletest-shared-library/m-p/1343316#M180409</link>
      <description>&lt;P&gt;Hello lchen,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think you might consult the community from yocto since you are using googletest and its not part of the BSP:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.yoctoproject.org/community/mailing-lists/" target="_blank"&gt;https://www.yoctoproject.org/community/mailing-lists/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 14:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/googletest-shared-library/m-p/1343316#M180409</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-09-21T14:00:51Z</dc:date>
    </item>
  </channel>
</rss>