<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using GPT1 in Linux on iMX8MPlus in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-GPT1-in-Linux-on-iMX8MPlus/m-p/1343135#M180391</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;We have a custom board based on iMX8MPlus. We want to use GPT1 to capture a signal on&amp;nbsp;SAI3_TXC. We are using kernel revision imx-5.4.47_2.2.0 and revision imx-atf&amp;nbsp;imx_5.4.47_2.2.0.&lt;/P&gt;&lt;P&gt;Is it possible to use GPT1 in Linux? Will adding a DTS node for GPT be enough? Or we also should patch imx8mp_bl31_setup.c in imx-atf?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 21 Sep 2021 09:09:32 GMT</pubDate>
    <dc:creator>alexeyfirago</dc:creator>
    <dc:date>2021-09-21T09:09:32Z</dc:date>
    <item>
      <title>Using GPT1 in Linux on iMX8MPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-GPT1-in-Linux-on-iMX8MPlus/m-p/1343135#M180391</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;We have a custom board based on iMX8MPlus. We want to use GPT1 to capture a signal on&amp;nbsp;SAI3_TXC. We are using kernel revision imx-5.4.47_2.2.0 and revision imx-atf&amp;nbsp;imx_5.4.47_2.2.0.&lt;/P&gt;&lt;P&gt;Is it possible to use GPT1 in Linux? Will adding a DTS node for GPT be enough? Or we also should patch imx8mp_bl31_setup.c in imx-atf?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 09:09:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-GPT1-in-Linux-on-iMX8MPlus/m-p/1343135#M180391</guid>
      <dc:creator>alexeyfirago</dc:creator>
      <dc:date>2021-09-21T09:09:32Z</dc:date>
    </item>
    <item>
      <title>Re: Using GPT1 in Linux on iMX8MPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-GPT1-in-Linux-on-iMX8MPlus/m-p/1343220#M180399</link>
      <description>&lt;P&gt;Hi Alexey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;patch was sent via mail.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 10:52:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-GPT1-in-Linux-on-iMX8MPlus/m-p/1343220#M180399</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-09-21T10:52:32Z</dc:date>
    </item>
  </channel>
</rss>