<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.Mx6 Question</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-Question/m-p/1342420#M180312</link>
    <description>&lt;P&gt;hello, I have a couple of questions:&lt;/P&gt;&lt;P&gt;1- How many threads does i.MX6Solo have?&lt;/P&gt;&lt;P&gt;2- I am looking at i.MX6Solo for an application where I need to process two (real-time) inputs, process it, do some (how speed) computation and then perform a voting logic on the results.&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;2a) Can i.MX6Solo handle this?&amp;nbsp; or do I need the .MX6Dual so the processing is done by one core and the voting logic is accomplished by the other?&lt;/P&gt;</description>
    <pubDate>Fri, 17 Sep 2021 18:58:04 GMT</pubDate>
    <dc:creator>lnguyen</dc:creator>
    <dc:date>2021-09-17T18:58:04Z</dc:date>
    <item>
      <title>i.Mx6 Question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-Question/m-p/1342420#M180312</link>
      <description>&lt;P&gt;hello, I have a couple of questions:&lt;/P&gt;&lt;P&gt;1- How many threads does i.MX6Solo have?&lt;/P&gt;&lt;P&gt;2- I am looking at i.MX6Solo for an application where I need to process two (real-time) inputs, process it, do some (how speed) computation and then perform a voting logic on the results.&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;2a) Can i.MX6Solo handle this?&amp;nbsp; or do I need the .MX6Dual so the processing is done by one core and the voting logic is accomplished by the other?&lt;/P&gt;</description>
      <pubDate>Fri, 17 Sep 2021 18:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-Question/m-p/1342420#M180312</guid>
      <dc:creator>lnguyen</dc:creator>
      <dc:date>2021-09-17T18:58:04Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6 Question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-Question/m-p/1348583#M180837</link>
      <description>&lt;P&gt;Hi lnguyen,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. It just has one, as is a single core.&lt;/P&gt;
&lt;P&gt;2. We do not have an application note focus on that, sorry for the problems, but the i.MX6 solo can't process 2 inputs at the same time (real-time).&lt;/P&gt;
&lt;P&gt;We recommend using the i.MX6 Dual-core to handle this.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 17:40:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6-Question/m-p/1348583#M180837</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-09-29T17:40:40Z</dc:date>
    </item>
  </channel>
</rss>