<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Board won't boot from SD card in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1341637#M180248</link>
    <description>&lt;P&gt;I set cma size to &amp;lt;0x10000000&amp;gt;, but it hasn't affected booting.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I contacted the vendor tech support, they run my image without a problem. I attached their log.&lt;/P&gt;&lt;P&gt;Could I burn the image in a wrong way? I tried &lt;EM&gt;Win32DiskImager&lt;/EM&gt; on Windows and &lt;EM&gt;dd&lt;/EM&gt; command on Ubuntu (to be precise,&amp;nbsp;&lt;EM&gt;sudo dd if=core-image-base-mys6ull14x14.rootfs.sdcard of=/dev/sdb1 bs=4M&lt;/EM&gt;), but result is always the same.&lt;/P&gt;</description>
    <pubDate>Thu, 16 Sep 2021 14:26:02 GMT</pubDate>
    <dc:creator>totalit</dc:creator>
    <dc:date>2021-09-16T14:26:02Z</dc:date>
    <item>
      <title>Board won't boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1340662#M180151</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I'm using &lt;STRONG&gt;MYS-6ULY2-256N2&lt;/STRONG&gt;. I built a&amp;nbsp;&lt;STRONG&gt;mys6ull14x14&lt;/STRONG&gt; image, loaded it into the board. Boot won't go further the line "Normal boot", waiting for input. Here's a log:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;U-Boot 2016.03-mys-6ulx+ga175019 (Aug 31 2021 - 00:42:41 -0700)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;CPU: Freescale i.MX6ULL rev1.1 528 MHz (running at 396 MHz)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU: Industrial temperature grade (-40C to 115C) at 41C&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Reset cause: POR&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Board: MYS-MX6ULL 14x14&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;I2C: ready&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DRAM: 256 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NAND: 256 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC: FSL_SDHC: 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Display: TFT43AB (480x272)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Video: 480x272x24&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;In: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Out: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Err: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Net: FEC0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Normal Boot&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;And environment variables:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;baudrate=115200&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;board_name=MYS6ULL&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;board_rev=14X14&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;bootargs=console=ttymxc0,115200 ubi.mtd=4 root=ubi0:rootfs rootfstype=ubifs mtdparts=gpmi-nand:5m(boot),1m(env),8m(kernel),2m(dtb),160m(rootfs1),-(userdata)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;bootdelay=3&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;console=ttymxc0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;envflag=1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ethact=FEC0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ethaddr=f4:4d:30:53:40:11&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ethprime=FEC&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fdt_addr=0x83000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fdt_high=0xffffffff&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;initrd_addr=0x83800000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;initrd_high=0xffffffff&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;loadaddr=0x80800000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" mtdparts=5m(boot),1m(env),8m(kernel),2m(dtb),160m(rootfs1),-(userdata) clk_ignore_unused&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mtdids=nand0=gpmi-nand&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;nand_erasesize=20000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;nand_oobsize=40&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;nand_writesize=800&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;panel=TFT43AB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;partition=nand0,0&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Environment size: 993/1048572 bytes&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 13:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1340662#M180151</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-09-15T13:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: Board won't boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1340930#M180171</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try to decrease cma size, "linux,cma" in dts&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ull-14x14-evk.dts?h=imx_4.1.15_2.0.0_ga" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ull-14x14-evk.dts?h=imx_4.1.15_2.0.0_ga&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;also recommended to debug it using AN4553 Using Open Source Debugging Tools&lt;/P&gt;
&lt;P&gt;for Linux on i.MX Processors&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4553.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4553.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 23:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1340930#M180171</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-09-15T23:16:06Z</dc:date>
    </item>
    <item>
      <title>Re: Board won't boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1341637#M180248</link>
      <description>&lt;P&gt;I set cma size to &amp;lt;0x10000000&amp;gt;, but it hasn't affected booting.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I contacted the vendor tech support, they run my image without a problem. I attached their log.&lt;/P&gt;&lt;P&gt;Could I burn the image in a wrong way? I tried &lt;EM&gt;Win32DiskImager&lt;/EM&gt; on Windows and &lt;EM&gt;dd&lt;/EM&gt; command on Ubuntu (to be precise,&amp;nbsp;&lt;EM&gt;sudo dd if=core-image-base-mys6ull14x14.rootfs.sdcard of=/dev/sdb1 bs=4M&lt;/EM&gt;), but result is always the same.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 14:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1341637#M180248</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-09-16T14:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: Board won't boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344129#M180481</link>
      <description>&lt;P&gt;So, no clue? Can I enable Earlycon in linux kernel to debug it? Is there a guide for earlycon (haven't found it via google)?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 14:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344129#M180481</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-09-22T14:07:31Z</dc:date>
    </item>
    <item>
      <title>Re: Board won't boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344485#M180499</link>
      <description>&lt;P&gt;suggest to apply for support to vendor of MYS-6ULY2-256N2 board:&lt;BR /&gt;&lt;A href="http://www.myirtech.com/support.asp" target="_blank"&gt;http://www.myirtech.com/support.asp&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 00:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344485#M180499</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-09-23T00:36:16Z</dc:date>
    </item>
    <item>
      <title>Re: Board won't boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344844#M180517</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I've already contacted the vendor tech support, they run my image without a problem.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 07:43:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344844#M180517</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-09-23T07:43:29Z</dc:date>
    </item>
    <item>
      <title>Re: Board won't boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344952#M180526</link>
      <description>&lt;P&gt;I manually wrote those commands from &lt;STRONG&gt;boot.scr&lt;/STRONG&gt; in the terminal and kernel has been loaded:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;setenv mmcroot '/dev/mmcblk0p2 rootwait rw rootdelay=5 mem=256M'&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;setenv mmcargs 'setenv bootargs console=${console},${baudrate} \ root=${mmcroot} mtdparts=gpmi-nand:5m(boot),10m(kernel),\ 1m(dtb),-(rootfs)'&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;run mmcargs&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fatload mmc 0 0x83000000 zImage&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fatload mmc 0 0x84000000 mys-imx6ull-14x14-evk-emmc.dtb&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;bootz 0x83000000 - 0x84000000&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;But why does it work that way? According to the guide, &lt;STRONG&gt;boot.scr&lt;/STRONG&gt; is necessary for &lt;STRONG&gt;eMMC&lt;/STRONG&gt;, not &lt;STRONG&gt;NAND&lt;/STRONG&gt;.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 09:21:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Board-won-t-boot-from-SD-card/m-p/1344952#M180526</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-09-23T09:21:18Z</dc:date>
    </item>
  </channel>
</rss>