<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Iperf server crash on FEC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Iperf-server-crash-on-FEC/m-p/1341544#M180237</link>
    <description>&lt;P&gt;We have a custom Hardware where in i.MX6SoloX processor is being used. A microchip KSZ9477 ethernet switch IC is interfaced with processor using RGMII interface to FEC1 controller of i.MX6SoloX processor. The Linux kernel version 4.14.200 is being used. We have enabled CONFIG_1588_PTP.&lt;/P&gt;&lt;P&gt;The KSZ9477 ethernet switch driver is available at following location:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/Microchip-Ethernet/EVB-KSZ9477/tree/master/KSZ/linux-drivers/ksz9897/linux-4.14/drivers" target="_blank"&gt;https://github.com/Microchip-Ethernet/EVB-KSZ9477/tree/master/KSZ/linux-drivers/ksz9897/linux-4.14/drivers&lt;/A&gt;&lt;/P&gt;&lt;P&gt;We are connecting 2 such customer hardware and making them client and server.&amp;nbsp;&lt;/P&gt;&lt;P&gt;To check the network performance, we are using iperf3. But we see a crash on iperf3 server. Please find attached logs.&lt;/P&gt;&lt;P&gt;We suspect that this crash is because of PTP is enabled in both FEC controller and KSZ9477 Switch driver.&lt;/P&gt;&lt;P&gt;Any suggestion is highly appreciated.&lt;/P&gt;</description>
    <pubDate>Thu, 16 Sep 2021 11:24:13 GMT</pubDate>
    <dc:creator>parth_shah</dc:creator>
    <dc:date>2021-09-16T11:24:13Z</dc:date>
    <item>
      <title>Iperf server crash on FEC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Iperf-server-crash-on-FEC/m-p/1341544#M180237</link>
      <description>&lt;P&gt;We have a custom Hardware where in i.MX6SoloX processor is being used. A microchip KSZ9477 ethernet switch IC is interfaced with processor using RGMII interface to FEC1 controller of i.MX6SoloX processor. The Linux kernel version 4.14.200 is being used. We have enabled CONFIG_1588_PTP.&lt;/P&gt;&lt;P&gt;The KSZ9477 ethernet switch driver is available at following location:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/Microchip-Ethernet/EVB-KSZ9477/tree/master/KSZ/linux-drivers/ksz9897/linux-4.14/drivers" target="_blank"&gt;https://github.com/Microchip-Ethernet/EVB-KSZ9477/tree/master/KSZ/linux-drivers/ksz9897/linux-4.14/drivers&lt;/A&gt;&lt;/P&gt;&lt;P&gt;We are connecting 2 such customer hardware and making them client and server.&amp;nbsp;&lt;/P&gt;&lt;P&gt;To check the network performance, we are using iperf3. But we see a crash on iperf3 server. Please find attached logs.&lt;/P&gt;&lt;P&gt;We suspect that this crash is because of PTP is enabled in both FEC controller and KSZ9477 Switch driver.&lt;/P&gt;&lt;P&gt;Any suggestion is highly appreciated.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 11:24:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Iperf-server-crash-on-FEC/m-p/1341544#M180237</guid>
      <dc:creator>parth_shah</dc:creator>
      <dc:date>2021-09-16T11:24:13Z</dc:date>
    </item>
  </channel>
</rss>