<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question about imxvideoconvert_g2d with IMX8QM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-imxvideoconvert-g2d-with-IMX8QM/m-p/1341173#M180195</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm testing with IMX8 QaudMax MEK and OV10635 cameras.&lt;/P&gt;&lt;P&gt;I can run below two gstreamer pipelines and see the fps in the display message.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,format=NV12 ! fpsdisplaysink&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,format=NV12 ! imxvideoconvert_g2d ! fpsdisplaysink&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when I check fps, case1 is 18 and case2 is 30.&lt;/P&gt;&lt;P&gt;Could you let me know what does imxvideoconvert_g2d do for making fps as 30?&lt;/P&gt;&lt;P&gt;Actually fpsdisplaysink can handle NV12 format so it doesn't need to convert image format to display. But if I skip imxvideoconvert_g2d before fpsdisplaysink, I can see frame drop.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I could see below message about imxvideoconvert_g2d in the 'imx8 gstreamer user guide' but I don't know it's related with my problem or not.&lt;/P&gt;&lt;P&gt;'The Amphion VPU IP uses a specific tiling format, so it requires the imxvideoconvert_g2d plugin&lt;BR /&gt;usage.'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Thu, 16 Sep 2021 05:46:58 GMT</pubDate>
    <dc:creator>dongjin</dc:creator>
    <dc:date>2021-09-16T05:46:58Z</dc:date>
    <item>
      <title>Question about imxvideoconvert_g2d with IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-imxvideoconvert-g2d-with-IMX8QM/m-p/1341173#M180195</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm testing with IMX8 QaudMax MEK and OV10635 cameras.&lt;/P&gt;&lt;P&gt;I can run below two gstreamer pipelines and see the fps in the display message.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,format=NV12 ! fpsdisplaysink&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,format=NV12 ! imxvideoconvert_g2d ! fpsdisplaysink&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when I check fps, case1 is 18 and case2 is 30.&lt;/P&gt;&lt;P&gt;Could you let me know what does imxvideoconvert_g2d do for making fps as 30?&lt;/P&gt;&lt;P&gt;Actually fpsdisplaysink can handle NV12 format so it doesn't need to convert image format to display. But if I skip imxvideoconvert_g2d before fpsdisplaysink, I can see frame drop.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I could see below message about imxvideoconvert_g2d in the 'imx8 gstreamer user guide' but I don't know it's related with my problem or not.&lt;/P&gt;&lt;P&gt;'The Amphion VPU IP uses a specific tiling format, so it requires the imxvideoconvert_g2d plugin&lt;BR /&gt;usage.'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 05:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-imxvideoconvert-g2d-with-IMX8QM/m-p/1341173#M180195</guid>
      <dc:creator>dongjin</dc:creator>
      <dc:date>2021-09-16T05:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: Question about imxvideoconvert_g2d with IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-imxvideoconvert-g2d-with-IMX8QM/m-p/1342198#M180295</link>
      <description>&lt;P&gt;could you get the same display result when you use these two commands? I mean that these two commands both work for your camera preview?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Sep 2021 12:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-imxvideoconvert-g2d-with-IMX8QM/m-p/1342198#M180295</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-09-17T12:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: Question about imxvideoconvert_g2d with IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-imxvideoconvert-g2d-with-IMX8QM/m-p/1344824#M180516</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I could run both two commands but the results are different.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,format=NV12 ! fpsdisplaysink&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,format=NV12 ! imxvideoconvert_g2d ! fpsdisplaysink&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;case 1 is running as 18fps but case 2 is running as 30 fps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dongjin Ha.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 07:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-imxvideoconvert-g2d-with-IMX8QM/m-p/1344824#M180516</guid>
      <dc:creator>dongjin</dc:creator>
      <dc:date>2021-09-23T07:20:23Z</dc:date>
    </item>
    <item>
      <title>Re: Question about imxvideoconvert_g2d with IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-imxvideoconvert-g2d-with-IMX8QM/m-p/1393526#M185255</link>
      <description>&lt;P&gt;I tested on my board,&amp;nbsp; I didn't find big difference with imxvideoconvert_g2d&amp;nbsp; or without, and your command is just preview, VPU didn't be used&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 31 Dec 2021 10:04:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-imxvideoconvert-g2d-with-IMX8QM/m-p/1393526#M185255</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-12-31T10:04:03Z</dc:date>
    </item>
  </channel>
</rss>