<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Sharing boot_cfg lines</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Sharing-boot-cfg-lines/m-p/1340200#M180097</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/100044"&gt;@jautry&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Section 9.4.2 (GPIO boot overrides) of the RM contains information about the boot override pins.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMXRT1060RM" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=IMXRT1060RM&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; After boot these pins can be used for other functionality.&lt;BR /&gt;Use i.MX Pins tool for possible configurations.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/pages/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX" target="_blank"&gt;https://www.nxp.com/pages/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
    <pubDate>Wed, 15 Sep 2021 03:46:40 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2021-09-15T03:46:40Z</dc:date>
    <item>
      <title>Sharing boot_cfg lines</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sharing-boot-cfg-lines/m-p/1340066#M180087</link>
      <description>&lt;P&gt;I noted on the eval board that Boot-Cfg input lines to the processor MIMXRT 1062&amp;nbsp; were shared.&amp;nbsp; Is it possible to share these lines since they are only accessed at startup for config data?&amp;nbsp; Is the way to do this is to start with them configured for Boot-Cfg and after boot changing the line configuration?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 00:32:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sharing-boot-cfg-lines/m-p/1340066#M180087</guid>
      <dc:creator>jautry</dc:creator>
      <dc:date>2021-09-15T00:32:57Z</dc:date>
    </item>
    <item>
      <title>Re: Sharing boot_cfg lines</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sharing-boot-cfg-lines/m-p/1340200#M180097</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/100044"&gt;@jautry&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Section 9.4.2 (GPIO boot overrides) of the RM contains information about the boot override pins.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMXRT1060RM" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=IMXRT1060RM&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; After boot these pins can be used for other functionality.&lt;BR /&gt;Use i.MX Pins tool for possible configurations.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/pages/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX" target="_blank"&gt;https://www.nxp.com/pages/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 03:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sharing-boot-cfg-lines/m-p/1340200#M180097</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-09-15T03:46:40Z</dc:date>
    </item>
    <item>
      <title>Re: Sharing boot_cfg lines</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sharing-boot-cfg-lines/m-p/1340643#M180145</link>
      <description>&lt;P&gt;I just want to make sure.&amp;nbsp; The config tool lists the GPIO as the default at power up but not the config option.&amp;nbsp; So the default is actually the config option for reading the boot configs and then the mux is executed to direct the pins to proper configuration.&amp;nbsp; We do not have to specifically define the pin for config option.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 13:18:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sharing-boot-cfg-lines/m-p/1340643#M180145</guid>
      <dc:creator>jautry</dc:creator>
      <dc:date>2021-09-15T13:18:54Z</dc:date>
    </item>
    <item>
      <title>Re: Sharing boot_cfg lines</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sharing-boot-cfg-lines/m-p/1341133#M180189</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/100044"&gt;@jautry&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; The default pins state are configured after boot configuration is latched.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 04:41:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sharing-boot-cfg-lines/m-p/1341133#M180189</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-09-16T04:41:40Z</dc:date>
    </item>
  </channel>
</rss>