<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックscreen blur problem on imx8qm</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/screen-blur-problem-on-imx8qm/m-p/1340195#M180096</link>
    <description>&lt;P&gt;Hi :&lt;/P&gt;&lt;P&gt;we are trying to bringup a panel.&lt;/P&gt;&lt;P&gt;Our hardware is dsi1-&amp;gt;max96789-&amp;gt;max96752-&amp;gt;lvds panel. An now the panel can shows normal except a litter blur of the screen.&lt;/P&gt;&lt;P&gt;The display parameter we used is like below:&lt;/P&gt;&lt;P&gt;static const struct drm_display_mode test_1920x1200_mode = {&lt;BR /&gt;.clock = 148500,&lt;BR /&gt;.hdisplay = 1920,&lt;BR /&gt;.hsync_start = 1920 + 88,&lt;BR /&gt;.hsync_end = 1920 + 88 + 44,&lt;BR /&gt;.htotal = 1920 + 88 + 44 + 148,&lt;BR /&gt;.vdisplay = 1080,&lt;BR /&gt;.vsync_start = 1080 + 4,&lt;BR /&gt;.vsync_end = 1080 + 4 + 5,&lt;BR /&gt;.vtotal = 1080 + 4 + 5 + 36,&lt;BR /&gt;.vrefresh = 60,&lt;BR /&gt;.flags = DRM_MODE_FLAG_NVSYNC | DRM_MODE_FLAG_NHSYNC,&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;also if we enable the deskew function of max96789, which remove jitter from the timing uncertainties introduced from the mipi-to-parallel clock-domain crossing and low power - high speed transition. The blur problem would be gone.&lt;/P&gt;&lt;P&gt;Could you help us to check why it happened blur problem.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Sep 2021 03:31:27 GMT</pubDate>
    <dc:creator>wulizhi</dc:creator>
    <dc:date>2021-09-15T03:31:27Z</dc:date>
    <item>
      <title>screen blur problem on imx8qm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/screen-blur-problem-on-imx8qm/m-p/1340195#M180096</link>
      <description>&lt;P&gt;Hi :&lt;/P&gt;&lt;P&gt;we are trying to bringup a panel.&lt;/P&gt;&lt;P&gt;Our hardware is dsi1-&amp;gt;max96789-&amp;gt;max96752-&amp;gt;lvds panel. An now the panel can shows normal except a litter blur of the screen.&lt;/P&gt;&lt;P&gt;The display parameter we used is like below:&lt;/P&gt;&lt;P&gt;static const struct drm_display_mode test_1920x1200_mode = {&lt;BR /&gt;.clock = 148500,&lt;BR /&gt;.hdisplay = 1920,&lt;BR /&gt;.hsync_start = 1920 + 88,&lt;BR /&gt;.hsync_end = 1920 + 88 + 44,&lt;BR /&gt;.htotal = 1920 + 88 + 44 + 148,&lt;BR /&gt;.vdisplay = 1080,&lt;BR /&gt;.vsync_start = 1080 + 4,&lt;BR /&gt;.vsync_end = 1080 + 4 + 5,&lt;BR /&gt;.vtotal = 1080 + 4 + 5 + 36,&lt;BR /&gt;.vrefresh = 60,&lt;BR /&gt;.flags = DRM_MODE_FLAG_NVSYNC | DRM_MODE_FLAG_NHSYNC,&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;also if we enable the deskew function of max96789, which remove jitter from the timing uncertainties introduced from the mipi-to-parallel clock-domain crossing and low power - high speed transition. The blur problem would be gone.&lt;/P&gt;&lt;P&gt;Could you help us to check why it happened blur problem.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 03:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/screen-blur-problem-on-imx8qm/m-p/1340195#M180096</guid>
      <dc:creator>wulizhi</dc:creator>
      <dc:date>2021-09-15T03:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: screen blur problem on imx8qm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/screen-blur-problem-on-imx8qm/m-p/1976740#M229831</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Have you resolved your issue&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Oct 2024 06:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/screen-blur-problem-on-imx8qm/m-p/1976740#M229831</guid>
      <dc:creator>hymmsx</dc:creator>
      <dc:date>2024-10-18T06:40:12Z</dc:date>
    </item>
  </channel>
</rss>