<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8MM  - IOMUXC_SAI2_RXC_UART1_TX on  pad AB22 fails. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-IOMUXC-SAI2-RXC-UART1-TX-on-pad-AB22-fails/m-p/1339894#M180070</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;CPU : IMX8MM,&lt;/P&gt;&lt;P&gt;Using/building : linux-imx_4.14.98_2.3.0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;HARDWARE: custom PCB design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to re-route uart1 and uart2 to&amp;nbsp; SAI2&amp;nbsp; SAI3 pads but for some reason, when trying to configure for example uart1 as below .&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;pinctrl_uart1: uart1grp {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX8MM_IOMUXC_SAI2_RXC_UART1_DTE_TX 0x140&lt;BR /&gt;MX8MM_IOMUXC_SAI2_RXFS_UART1_DTE_RX 0x140&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;I don't see my tx-bytes at PAD-AB22 it seems as if this is still an RX-pin in stead of a TX-pin of the uart.&amp;nbsp;( when putting my oscilloscope on PAD-AC19 I see the TX coming out here and not on PAD-AB22.)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the 2nd uart I can send bytes&amp;nbsp; , but when connecting TX to RX I can't receive my own bytes ( it look is if there is no reception, while to oscilloscope proves that the bytes are arriving on the intended&amp;nbsp;MX8MM_IOMUXC_SAI3_TXFS_UART2_DCE_RX pad)&lt;/P&gt;&lt;P&gt;pinctrl_uart2: uart2grp {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX8MM_IOMUXC_SAI3_TXC_UART2_DCE_TX 0x140&lt;BR /&gt;MX8MM_IOMUXC_SAI3_TXFS_UART2_DCE_RX 0x140&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Any hints ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Sep 2021 15:17:15 GMT</pubDate>
    <dc:creator>Noel_V</dc:creator>
    <dc:date>2021-09-14T15:17:15Z</dc:date>
    <item>
      <title>IMX8MM  - IOMUXC_SAI2_RXC_UART1_TX on  pad AB22 fails.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-IOMUXC-SAI2-RXC-UART1-TX-on-pad-AB22-fails/m-p/1339894#M180070</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;CPU : IMX8MM,&lt;/P&gt;&lt;P&gt;Using/building : linux-imx_4.14.98_2.3.0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;HARDWARE: custom PCB design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to re-route uart1 and uart2 to&amp;nbsp; SAI2&amp;nbsp; SAI3 pads but for some reason, when trying to configure for example uart1 as below .&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;pinctrl_uart1: uart1grp {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX8MM_IOMUXC_SAI2_RXC_UART1_DTE_TX 0x140&lt;BR /&gt;MX8MM_IOMUXC_SAI2_RXFS_UART1_DTE_RX 0x140&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;I don't see my tx-bytes at PAD-AB22 it seems as if this is still an RX-pin in stead of a TX-pin of the uart.&amp;nbsp;( when putting my oscilloscope on PAD-AC19 I see the TX coming out here and not on PAD-AB22.)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the 2nd uart I can send bytes&amp;nbsp; , but when connecting TX to RX I can't receive my own bytes ( it look is if there is no reception, while to oscilloscope proves that the bytes are arriving on the intended&amp;nbsp;MX8MM_IOMUXC_SAI3_TXFS_UART2_DCE_RX pad)&lt;/P&gt;&lt;P&gt;pinctrl_uart2: uart2grp {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX8MM_IOMUXC_SAI3_TXC_UART2_DCE_TX 0x140&lt;BR /&gt;MX8MM_IOMUXC_SAI3_TXFS_UART2_DCE_RX 0x140&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Any hints ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 15:17:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-IOMUXC-SAI2-RXC-UART1-TX-on-pad-AB22-fails/m-p/1339894#M180070</guid>
      <dc:creator>Noel_V</dc:creator>
      <dc:date>2021-09-14T15:17:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM  - IOMUXC_SAI2_RXC_UART1_TX on  pad AB22 fails.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-IOMUXC-SAI2-RXC-UART1-TX-on-pad-AB22-fails/m-p/1340052#M180084</link>
      <description>&lt;P&gt;Hi Noel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;.. it seems as if this is still an RX-pin in stead of a TX-pin of the uart&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;in general this may be due to DCE/DTE described in Figure 16-10. UART external signals to&lt;/P&gt;
&lt;P&gt;module signals routing with respect to DCE/DTE mode&amp;nbsp;&amp;nbsp; &lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=IMX8MMRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Mini Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;dts example :&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/serial/fsl-imx-uart.txt?h=imx_4.14.98_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/serial/fsl-imx-uart.txt?h=imx_4.14.98_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 23:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-IOMUXC-SAI2-RXC-UART1-TX-on-pad-AB22-fails/m-p/1340052#M180084</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-09-14T23:30:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM  - IOMUXC_SAI2_RXC_UART1_TX on  pad AB22 fails.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-IOMUXC-SAI2-RXC-UART1-TX-on-pad-AB22-fails/m-p/1340567#M180139</link>
      <description>&lt;P&gt;Igor,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You made may day&amp;nbsp; , iow SOLVED !&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for the hint !&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Noel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 11:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-IOMUXC-SAI2-RXC-UART1-TX-on-pad-AB22-fails/m-p/1340567#M180139</guid>
      <dc:creator>Noel_V</dc:creator>
      <dc:date>2021-09-15T11:40:48Z</dc:date>
    </item>
  </channel>
</rss>