<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8MMEVK: H264 encoder chromaoffset value in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MMEVK-H264-encoder-chromaoffset-value/m-p/1337742#M179843</link>
    <description>&lt;P&gt;Hello Santhosh2,&lt;/P&gt;
&lt;P&gt;You can check the VPU Application programming reference for usage and programming the VPU, and&lt;/P&gt;
&lt;P&gt;this is a data structure for configuring MJPEG-specific parameters in encoder applications.&lt;BR /&gt;mjpg_sourceFormat is the chroma format. The format means chrominance size of source image and can be a value&lt;BR /&gt;between 0 and 4: 0 = 4:2:0, 1 = 4:2:2 horizontal, 2 = 4:2:2 vertical, 3 = 4:4:4, 4 = 4:0:0.&lt;/P&gt;
&lt;P&gt;But, it never said about the h264 I guess it don't but you can check the manual.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 09 Sep 2021 13:05:32 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2021-09-09T13:05:32Z</dc:date>
    <item>
      <title>IMX8MMEVK: H264 encoder chromaoffset value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MMEVK-H264-encoder-chromaoffset-value/m-p/1337399#M179811</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;In h264 encoder, Is it possible to change chromaoffset value from 2 to 0 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Santhosh kumar&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Sep 2021 05:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MMEVK-H264-encoder-chromaoffset-value/m-p/1337399#M179811</guid>
      <dc:creator>santhosh2</dc:creator>
      <dc:date>2021-09-09T05:29:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MMEVK: H264 encoder chromaoffset value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MMEVK-H264-encoder-chromaoffset-value/m-p/1337742#M179843</link>
      <description>&lt;P&gt;Hello Santhosh2,&lt;/P&gt;
&lt;P&gt;You can check the VPU Application programming reference for usage and programming the VPU, and&lt;/P&gt;
&lt;P&gt;this is a data structure for configuring MJPEG-specific parameters in encoder applications.&lt;BR /&gt;mjpg_sourceFormat is the chroma format. The format means chrominance size of source image and can be a value&lt;BR /&gt;between 0 and 4: 0 = 4:2:0, 1 = 4:2:2 horizontal, 2 = 4:2:2 vertical, 3 = 4:4:4, 4 = 4:0:0.&lt;/P&gt;
&lt;P&gt;But, it never said about the h264 I guess it don't but you can check the manual.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 09 Sep 2021 13:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MMEVK-H264-encoder-chromaoffset-value/m-p/1337742#M179843</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-09-09T13:05:32Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MMEVK: H264 encoder chromaoffset value</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MMEVK-H264-encoder-chromaoffset-value/m-p/1338659#M179937</link>
      <description>&lt;P&gt;Thanks, I will check&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Santhosh Kumar S&lt;/P&gt;</description>
      <pubDate>Sun, 12 Sep 2021 11:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MMEVK-H264-encoder-chromaoffset-value/m-p/1338659#M179937</guid>
      <dc:creator>santhosh2</dc:creator>
      <dc:date>2021-09-12T11:53:10Z</dc:date>
    </item>
  </channel>
</rss>