<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 SDK: Compile a kernel: Can't locate integer.pm in @INC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SDK-Compile-a-kernel-Can-t-locate-integer-pm-in-INC/m-p/1336477#M179737</link>
    <description>&lt;P&gt;Just try to compile a 5.14 kernel with the Yocto created SDK (2.0.0). It seems to start properly but than it fails due to a missing perl module.&lt;/P&gt;&lt;P&gt;How can I add this integer.pm to my SDK (automatically)? I copied it from the ../tmp/work directory as it is used several times there, but it is not part of SDK!?!?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fs/configfs/item.o&lt;/P&gt;&lt;P&gt;CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kernel/cgroup/rstat.o&lt;/P&gt;&lt;P&gt;PERLASM arch/arm64/crypto/sha256-core.S&lt;/P&gt;&lt;P&gt;CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mm/mprotect.o&lt;/P&gt;&lt;P&gt;Can't locate integer.pm in @INC (you may need to install the integer module) (@INC contains: /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/site_perl/5.32.1/x86_64-linux /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/site_perl/5.32.1 /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/vendor_perl/5.32.1 /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/5.32.1/x86_64-linux /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/5.32.1 /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/site_perl/5.32.1/x86_64-linux /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/site_perl/5.32.1 /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/vendor_perl/5.32.1/x86_64-linux /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/vendor_perl/5.32.1 /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/5.32.1/x86_64-linux /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/5.32.1) at arch/arm64/crypto/sha512-armv8.pl line 478.&lt;/P&gt;&lt;P&gt;BEGIN failed--compilation aborted at arch/arm64/crypto/sha512-armv8.pl line 478.&lt;/P&gt;&lt;P&gt;make[2]: *** [arch/arm64/crypto/Makefile:78: arch/arm64/crypto/sha256-core.S] Error 2&lt;/P&gt;&lt;P&gt;make[1]: *** [scripts/Makefile.build:514: arch/arm64/crypto] Error 2&lt;/P&gt;&lt;P&gt;make: *** [Makefile:1851: arch/arm64] Error 2&lt;/P&gt;&lt;P&gt;make: *** Waiting for unfinished jobs....&lt;/P&gt;</description>
    <pubDate>Wed, 08 Sep 2021 04:57:14 GMT</pubDate>
    <dc:creator>arno_0</dc:creator>
    <dc:date>2021-09-08T04:57:14Z</dc:date>
    <item>
      <title>SDK: Compile a kernel: Can't locate integer.pm in @INC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDK-Compile-a-kernel-Can-t-locate-integer-pm-in-INC/m-p/1336477#M179737</link>
      <description>&lt;P&gt;Just try to compile a 5.14 kernel with the Yocto created SDK (2.0.0). It seems to start properly but than it fails due to a missing perl module.&lt;/P&gt;&lt;P&gt;How can I add this integer.pm to my SDK (automatically)? I copied it from the ../tmp/work directory as it is used several times there, but it is not part of SDK!?!?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fs/configfs/item.o&lt;/P&gt;&lt;P&gt;CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kernel/cgroup/rstat.o&lt;/P&gt;&lt;P&gt;PERLASM arch/arm64/crypto/sha256-core.S&lt;/P&gt;&lt;P&gt;CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mm/mprotect.o&lt;/P&gt;&lt;P&gt;Can't locate integer.pm in @INC (you may need to install the integer module) (@INC contains: /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/site_perl/5.32.1/x86_64-linux /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/site_perl/5.32.1 /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/vendor_perl/5.32.1 /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/5.32.1/x86_64-linux /home/user/y/sdk_imx_5.10.35/sysroots/x86_64-pokysdk-linux/usr/bin/../..//usr/lib/perl5/5.32.1 /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/site_perl/5.32.1/x86_64-linux /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/site_perl/5.32.1 /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/vendor_perl/5.32.1/x86_64-linux /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/vendor_perl/5.32.1 /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/5.32.1/x86_64-linux /opt/fsl-imx-wayland/5.10-hardknott/sysroots/x86_64-pokysdk-linux/usr/lib/perl5/5.32.1) at arch/arm64/crypto/sha512-armv8.pl line 478.&lt;/P&gt;&lt;P&gt;BEGIN failed--compilation aborted at arch/arm64/crypto/sha512-armv8.pl line 478.&lt;/P&gt;&lt;P&gt;make[2]: *** [arch/arm64/crypto/Makefile:78: arch/arm64/crypto/sha256-core.S] Error 2&lt;/P&gt;&lt;P&gt;make[1]: *** [scripts/Makefile.build:514: arch/arm64/crypto] Error 2&lt;/P&gt;&lt;P&gt;make: *** [Makefile:1851: arch/arm64] Error 2&lt;/P&gt;&lt;P&gt;make: *** Waiting for unfinished jobs....&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 04:57:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDK-Compile-a-kernel-Can-t-locate-integer-pm-in-INC/m-p/1336477#M179737</guid>
      <dc:creator>arno_0</dc:creator>
      <dc:date>2021-09-08T04:57:14Z</dc:date>
    </item>
    <item>
      <title>Re: SDK: Compile a kernel: Can't locate integer.pm in @INC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDK-Compile-a-kernel-Can-t-locate-integer-pm-in-INC/m-p/1336785#M179767</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;
&lt;P&gt;We didn't release&amp;nbsp; linux bsp with 5.14 kernel.&lt;/P&gt;
&lt;P&gt;The latest one is 5.10.35_2.0.0, so if you export cross compile tool chain, you should compile the version of kernel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a good day!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 10:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDK-Compile-a-kernel-Can-t-locate-integer-pm-in-INC/m-p/1336785#M179767</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-09-08T10:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: SDK: Compile a kernel: Can't locate integer.pm in @INC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDK-Compile-a-kernel-Can-t-locate-integer-pm-in-INC/m-p/1336808#M179772</link>
      <description>&lt;P&gt;I know. But I should be able to compile any kernel. Not just the given one.&lt;/P&gt;&lt;P&gt;So the question is: How can I get integer.pm into SDK? Add something to a recipe? I have which package is involved here.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 10:55:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDK-Compile-a-kernel-Can-t-locate-integer-pm-in-INC/m-p/1336808#M179772</guid>
      <dc:creator>arno_0</dc:creator>
      <dc:date>2021-09-08T10:55:01Z</dc:date>
    </item>
  </channel>
</rss>