<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RTC pcf85263 issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RTC-pcf85263-issue/m-p/1335898#M179667</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using RTC PCF85263 in our i.Mx8 M Mini board. I am always getting the below error when date setting at the time of booting.&lt;/P&gt;&lt;P&gt;[ 12.483309] rtc-pcf85263 0-0051: No century in NVRAM - assume 2000&lt;BR /&gt;[ 12.491758] rtc-pcf85263 0-0051: Oscillator stop detected, date/time is not reliable.&lt;BR /&gt;[ 12.499730] rtc-pcf85263 0-0051: rtc core: registered rtc-pcf85263 as rtc0&lt;BR /&gt;[ 12.506619] rtc-pcf85263 0-0051: PCF85263 RTC (irqpin=INTA irq=139)&lt;BR /&gt;[ 12.513875] snvs_rtc 30370000.snvs:snvs-rtc-lp: rtc core: registered 30370000.snvs:snvs-rtc-lp as rtc1&lt;BR /&gt;[ 14.736322] rtc-pcf85263 0-0051: Oscillator stop detected, date/time is not reliable.&lt;BR /&gt;[ 14.744164] rtc-pcf85263 0-0051: hctosys: unable to read the hardware clock&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This error will not come when we write the date and try to read the same. The steps which I followed&lt;/P&gt;&lt;P&gt;1. Set current date using "date -s" command&lt;/P&gt;&lt;P&gt;2. hwclock -w&lt;/P&gt;&lt;P&gt;3. hwclock&lt;/P&gt;&lt;P&gt;Issue observed :&lt;/P&gt;&lt;P&gt;If I try to set future date from current date , it is getting set but if I try to set past date from current date , it is not getting set after every reboot&lt;/P&gt;&lt;P&gt;Any configuration is required for solving the issue ?&lt;/P&gt;&lt;P&gt;Please provide the input for the same&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Deeksha&lt;/P&gt;</description>
    <pubDate>Tue, 07 Sep 2021 07:32:22 GMT</pubDate>
    <dc:creator>deeksha</dc:creator>
    <dc:date>2021-09-07T07:32:22Z</dc:date>
    <item>
      <title>RTC pcf85263 issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-pcf85263-issue/m-p/1335898#M179667</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using RTC PCF85263 in our i.Mx8 M Mini board. I am always getting the below error when date setting at the time of booting.&lt;/P&gt;&lt;P&gt;[ 12.483309] rtc-pcf85263 0-0051: No century in NVRAM - assume 2000&lt;BR /&gt;[ 12.491758] rtc-pcf85263 0-0051: Oscillator stop detected, date/time is not reliable.&lt;BR /&gt;[ 12.499730] rtc-pcf85263 0-0051: rtc core: registered rtc-pcf85263 as rtc0&lt;BR /&gt;[ 12.506619] rtc-pcf85263 0-0051: PCF85263 RTC (irqpin=INTA irq=139)&lt;BR /&gt;[ 12.513875] snvs_rtc 30370000.snvs:snvs-rtc-lp: rtc core: registered 30370000.snvs:snvs-rtc-lp as rtc1&lt;BR /&gt;[ 14.736322] rtc-pcf85263 0-0051: Oscillator stop detected, date/time is not reliable.&lt;BR /&gt;[ 14.744164] rtc-pcf85263 0-0051: hctosys: unable to read the hardware clock&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This error will not come when we write the date and try to read the same. The steps which I followed&lt;/P&gt;&lt;P&gt;1. Set current date using "date -s" command&lt;/P&gt;&lt;P&gt;2. hwclock -w&lt;/P&gt;&lt;P&gt;3. hwclock&lt;/P&gt;&lt;P&gt;Issue observed :&lt;/P&gt;&lt;P&gt;If I try to set future date from current date , it is getting set but if I try to set past date from current date , it is not getting set after every reboot&lt;/P&gt;&lt;P&gt;Any configuration is required for solving the issue ?&lt;/P&gt;&lt;P&gt;Please provide the input for the same&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Deeksha&lt;/P&gt;</description>
      <pubDate>Tue, 07 Sep 2021 07:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-pcf85263-issue/m-p/1335898#M179667</guid>
      <dc:creator>deeksha</dc:creator>
      <dc:date>2021-09-07T07:32:22Z</dc:date>
    </item>
  </channel>
</rss>