<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX8M Plus PCIe prefetchable memory</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-PCIe-prefetchable-memory/m-p/1334350#M179520</link>
    <description>&lt;P&gt;Per the post&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Can-not-allocate-PCIe-region-when-size-is-8M-on-Sabre-platform/m-p/455831" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Can-not-allocate-PCIe-region-when-size-is-8M-on-Sabre-platform/m-p/455831&lt;/A&gt;&amp;nbsp;we see that the IMX6 PCIe driver cannot support&amp;nbsp;prefetchable memory regions of more than 16MBytes in the&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this limitation still in place and applicable to the IMX8M Plus PCIe as well?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 02 Sep 2021 21:06:04 GMT</pubDate>
    <dc:creator>kentmeyer</dc:creator>
    <dc:date>2021-09-02T21:06:04Z</dc:date>
    <item>
      <title>iMX8M Plus PCIe prefetchable memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-PCIe-prefetchable-memory/m-p/1334350#M179520</link>
      <description>&lt;P&gt;Per the post&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Can-not-allocate-PCIe-region-when-size-is-8M-on-Sabre-platform/m-p/455831" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Can-not-allocate-PCIe-region-when-size-is-8M-on-Sabre-platform/m-p/455831&lt;/A&gt;&amp;nbsp;we see that the IMX6 PCIe driver cannot support&amp;nbsp;prefetchable memory regions of more than 16MBytes in the&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this limitation still in place and applicable to the IMX8M Plus PCIe as well?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Sep 2021 21:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-PCIe-prefetchable-memory/m-p/1334350#M179520</guid>
      <dc:creator>kentmeyer</dc:creator>
      <dc:date>2021-09-02T21:06:04Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus PCIe prefetchable memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-PCIe-prefetchable-memory/m-p/1334529#M179531</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/42718"&gt;@kentmeyer&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; According to section 2.2 (Cortex-A53 Memory Map) of i.MX 8M Plus &lt;BR /&gt;Reference Manual (Rev. 1, 06/2021) the following memory address &lt;BR /&gt;area of 128MB is located for the PCIe: 1800_0000 - 1FFF_FFFF&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Under Linux:&lt;BR /&gt;— PCIe host configuration space: 0x33c0_0000 – 0x33ff_ffff (4Mbytes)&lt;BR /&gt;— PCIe device configuration space: 0x27f0_0000 – 0x27f7_ffff (512K bytes)&lt;BR /&gt;— PCIe IO space: 0x27f8_0000 – 0x27f8_ffff (64K bytes)&lt;BR /&gt;— PCIe memory space: 0x2000_0000 – 0x27ef_ffff (127M bytes)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Sep 2021 05:13:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-PCIe-prefetchable-memory/m-p/1334529#M179531</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-09-03T05:13:45Z</dc:date>
    </item>
  </channel>
</rss>