<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Gstreamer : Frame Number at application in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-Frame-Number-at-application/m-p/1334044#M179501</link>
    <description>&lt;P&gt;BSP Version :&amp;nbsp;&lt;/P&gt;&lt;P&gt;Linux imx8mmevk 5.4.24-2.1.0+ge94682e3ac7d #1 SMP PREEMPT Mon Aug 23 13:41:17 UTC 2021 aarch64 aarch64 aarch64 GNU/Linux&lt;/P&gt;</description>
    <pubDate>Thu, 02 Sep 2021 10:03:24 GMT</pubDate>
    <dc:creator>Siddharth</dc:creator>
    <dc:date>2021-09-02T10:03:24Z</dc:date>
    <item>
      <title>Gstreamer : Frame Number at application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-Frame-Number-at-application/m-p/1329724#M179100</link>
      <description>&lt;P&gt;I am working on one custom application on imx8mm using GStreamer and facing the issue of latency in RTSP while running the live video(1920x1080: 20 fps:h264 ) on VLC of around 1.5 seconds.&lt;/P&gt;&lt;P&gt;I have one question regarding the issue :&lt;BR /&gt;a) Do we have any plugins or properties on GStreamer to find the frame number on the GStreamer application?&lt;BR /&gt;do-timestamp is not working properly (offset is -1: Gstbuffer member)&lt;/P&gt;&lt;P&gt;b) Any API to get the frame number at the application to find the comparison with the frame captured at a low level?&lt;BR /&gt;c) Is latency can be reduced?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;Regards&lt;BR /&gt;Siddharth Singh&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 18:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-Frame-Number-at-application/m-p/1329724#M179100</guid>
      <dc:creator>Siddharth</dc:creator>
      <dc:date>2021-08-25T18:22:45Z</dc:date>
    </item>
    <item>
      <title>Re: Gstreamer : Frame Number at application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-Frame-Number-at-application/m-p/1331392#M179292</link>
      <description>&lt;P&gt;what bsp version do you test?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Aug 2021 03:15:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-Frame-Number-at-application/m-p/1331392#M179292</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-08-30T03:15:04Z</dc:date>
    </item>
    <item>
      <title>Re: Gstreamer : Frame Number at application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-Frame-Number-at-application/m-p/1334044#M179501</link>
      <description>&lt;P&gt;BSP Version :&amp;nbsp;&lt;/P&gt;&lt;P&gt;Linux imx8mmevk 5.4.24-2.1.0+ge94682e3ac7d #1 SMP PREEMPT Mon Aug 23 13:41:17 UTC 2021 aarch64 aarch64 aarch64 GNU/Linux&lt;/P&gt;</description>
      <pubDate>Thu, 02 Sep 2021 10:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-Frame-Number-at-application/m-p/1334044#M179501</guid>
      <dc:creator>Siddharth</dc:creator>
      <dc:date>2021-09-02T10:03:24Z</dc:date>
    </item>
    <item>
      <title>Re: Gstreamer : Frame Number at application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-Frame-Number-at-application/m-p/1338303#M179899</link>
      <description>&lt;P&gt;did you find the a/v sync issue? could you share the commands you use? if you want to get absolute timestamp, maybe you can refer to the link as below:&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://stackoverflow.com/questions/6149983/h-264-rtsp-absolute-timestamp&amp;quot;" target="_blank"&gt;https://stackoverflow.com/questions/6149983/h-264-rtsp-absolute-timestamp"&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and I found in the encoder and decoder source code, structure GstVideoCodecFrame has pts for frame timestamp, you can export this to check, and as I known the latest bsp fixed many latency or A/V sync issue, maybe you can try the latest bsp to test again&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Sep 2021 09:13:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-Frame-Number-at-application/m-p/1338303#M179899</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-09-10T09:13:40Z</dc:date>
    </item>
  </channel>
</rss>