<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックoverlay filesystem to mount root filesystem on RAM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/overlay-filesystem-to-mount-root-filesystem-on-RAM/m-p/1330332#M179160</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I'm working on imx6ull14x14evk board, and I'm new to yocto build.&lt;BR /&gt;&lt;BR /&gt;Currently I'm observing that the root filesystem is mounted in the nand-flash, but I want to create a overlay fs and mount the root filesystem in ram.&lt;BR /&gt;&lt;BR /&gt;How can this be done?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
    <pubDate>Thu, 26 Aug 2021 11:33:35 GMT</pubDate>
    <dc:creator>rvignesh496</dc:creator>
    <dc:date>2021-08-26T11:33:35Z</dc:date>
    <item>
      <title>overlay filesystem to mount root filesystem on RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/overlay-filesystem-to-mount-root-filesystem-on-RAM/m-p/1330332#M179160</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I'm working on imx6ull14x14evk board, and I'm new to yocto build.&lt;BR /&gt;&lt;BR /&gt;Currently I'm observing that the root filesystem is mounted in the nand-flash, but I want to create a overlay fs and mount the root filesystem in ram.&lt;BR /&gt;&lt;BR /&gt;How can this be done?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 11:33:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/overlay-filesystem-to-mount-root-filesystem-on-RAM/m-p/1330332#M179160</guid>
      <dc:creator>rvignesh496</dc:creator>
      <dc:date>2021-08-26T11:33:35Z</dc:date>
    </item>
    <item>
      <title>Re: overlay filesystem to mount root filesystem on RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/overlay-filesystem-to-mount-root-filesystem-on-RAM/m-p/1330618#M179188</link>
      <description>&lt;P&gt;Hi Vignesh&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;may be useful tutorial below&lt;/P&gt;
&lt;P&gt;&lt;A href="https://imxdev.gitlab.io/tutorial/How_to_boot_imx_using_ramdisk/" target="_blank"&gt;https://imxdev.gitlab.io/tutorial/How_to_boot_imx_using_ramdisk/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 23:52:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/overlay-filesystem-to-mount-root-filesystem-on-RAM/m-p/1330618#M179188</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-26T23:52:59Z</dc:date>
    </item>
  </channel>
</rss>