<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSystem hang up when running uboot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1329367#M179067</link>
    <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;We are using i.MX8MQ processor and running the mtest program on the uboot to do some memory test.&lt;/P&gt;&lt;P&gt;We found that the system may hang up after some loop tests. This hang up happens randomly and at different loop. When it happen, the processor, UART and USB have no respond. We tried to use the debugger to debug this problem. Here is the log we got. Please review and provide any solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(gdb) info reg&lt;BR /&gt;x0 0x2 2&lt;BR /&gt;x1 0xbffad2dd 3220886237&lt;BR /&gt;x2 0x5cc27dc8 1556250056&lt;BR /&gt;x3 0x4040000 67371008&lt;BR /&gt;x4 0xfffffffffffffb81 18446744073709550465&lt;BR /&gt;x5 0x10 16&lt;BR /&gt;x6 0xffffffd0 4294967248&lt;BR /&gt;x7 0x3 3&lt;BR /&gt;x8 0xbf9335f0 3214095856&lt;BR /&gt;x9 0x8 8&lt;BR /&gt;x10 0xffffffd0 4294967248&lt;BR /&gt;x11 0x6 6&lt;BR /&gt;x12 0x1869f 99999&lt;BR /&gt;x13 0xd 13&lt;BR /&gt;x14 0xc 12&lt;BR /&gt;x15 0xffffffff 4294967295&lt;BR /&gt;x16 0x1080 4224&lt;BR /&gt;x17 0x0 0&lt;BR /&gt;x18 0xbf939d70 3214122352&lt;BR /&gt;x19 0xbffd7000 3221057536&lt;BR /&gt;x20 0xbdfffff8 3187671032&lt;BR /&gt;x21 0xbffad4b5 3220886709&lt;BR /&gt;x22 0x40000000 1073741824&lt;BR /&gt;x23 0xfffffffffbfbfbfb 18446744073642179579&lt;BR /&gt;x24 0x1 1&lt;BR /&gt;x25 0x4040404 67372036&lt;BR /&gt;x26 0xbe000000 3187671040&lt;BR /&gt;x27 0x3 3&lt;BR /&gt;x28 0xbf948b50 3214183248&lt;BR /&gt;x29 0xbf933690 3214096016&lt;BR /&gt;x30 0xbff45d80 3220462976&lt;BR /&gt;sp 0xbf933690 0xbf933690&lt;BR /&gt;pc 0xbff3b200 0xbff3b200&lt;BR /&gt;cpsr 0x800003c9 [ SP=1 EL=0 nRW=0 F I A D N ]&lt;BR /&gt;fpsr 0x0 0&lt;BR /&gt;fpcr 0x0 0&lt;BR /&gt;ELR_EL1 0x0 0x0&lt;BR /&gt;ESR_EL1 0x0 0&lt;BR /&gt;SPSR_EL1 0x0 0&lt;BR /&gt;ELR_EL2 0xbff3b200 0xbff3b200&lt;BR /&gt;ESR_EL2 0x96000044 2516582468&lt;BR /&gt;SPSR_EL2 0x800003c9 2147484617&lt;BR /&gt;ELR_EL3 0x0 0x0&lt;BR /&gt;ESR_EL3 0x0 0&lt;BR /&gt;SPSR_EL3 0x0 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
    <pubDate>Wed, 25 Aug 2021 09:55:58 GMT</pubDate>
    <dc:creator>simonng</dc:creator>
    <dc:date>2021-08-25T09:55:58Z</dc:date>
    <item>
      <title>System hang up when running uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1329367#M179067</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;We are using i.MX8MQ processor and running the mtest program on the uboot to do some memory test.&lt;/P&gt;&lt;P&gt;We found that the system may hang up after some loop tests. This hang up happens randomly and at different loop. When it happen, the processor, UART and USB have no respond. We tried to use the debugger to debug this problem. Here is the log we got. Please review and provide any solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(gdb) info reg&lt;BR /&gt;x0 0x2 2&lt;BR /&gt;x1 0xbffad2dd 3220886237&lt;BR /&gt;x2 0x5cc27dc8 1556250056&lt;BR /&gt;x3 0x4040000 67371008&lt;BR /&gt;x4 0xfffffffffffffb81 18446744073709550465&lt;BR /&gt;x5 0x10 16&lt;BR /&gt;x6 0xffffffd0 4294967248&lt;BR /&gt;x7 0x3 3&lt;BR /&gt;x8 0xbf9335f0 3214095856&lt;BR /&gt;x9 0x8 8&lt;BR /&gt;x10 0xffffffd0 4294967248&lt;BR /&gt;x11 0x6 6&lt;BR /&gt;x12 0x1869f 99999&lt;BR /&gt;x13 0xd 13&lt;BR /&gt;x14 0xc 12&lt;BR /&gt;x15 0xffffffff 4294967295&lt;BR /&gt;x16 0x1080 4224&lt;BR /&gt;x17 0x0 0&lt;BR /&gt;x18 0xbf939d70 3214122352&lt;BR /&gt;x19 0xbffd7000 3221057536&lt;BR /&gt;x20 0xbdfffff8 3187671032&lt;BR /&gt;x21 0xbffad4b5 3220886709&lt;BR /&gt;x22 0x40000000 1073741824&lt;BR /&gt;x23 0xfffffffffbfbfbfb 18446744073642179579&lt;BR /&gt;x24 0x1 1&lt;BR /&gt;x25 0x4040404 67372036&lt;BR /&gt;x26 0xbe000000 3187671040&lt;BR /&gt;x27 0x3 3&lt;BR /&gt;x28 0xbf948b50 3214183248&lt;BR /&gt;x29 0xbf933690 3214096016&lt;BR /&gt;x30 0xbff45d80 3220462976&lt;BR /&gt;sp 0xbf933690 0xbf933690&lt;BR /&gt;pc 0xbff3b200 0xbff3b200&lt;BR /&gt;cpsr 0x800003c9 [ SP=1 EL=0 nRW=0 F I A D N ]&lt;BR /&gt;fpsr 0x0 0&lt;BR /&gt;fpcr 0x0 0&lt;BR /&gt;ELR_EL1 0x0 0x0&lt;BR /&gt;ESR_EL1 0x0 0&lt;BR /&gt;SPSR_EL1 0x0 0&lt;BR /&gt;ELR_EL2 0xbff3b200 0xbff3b200&lt;BR /&gt;ESR_EL2 0x96000044 2516582468&lt;BR /&gt;SPSR_EL2 0x800003c9 2147484617&lt;BR /&gt;ELR_EL3 0x0 0x0&lt;BR /&gt;ESR_EL3 0x0 0&lt;BR /&gt;SPSR_EL3 0x0 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 09:55:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1329367#M179067</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2021-08-25T09:55:58Z</dc:date>
    </item>
    <item>
      <title>Re: System hang up when running uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1329417#M179072</link>
      <description>&lt;P&gt;Hi Simon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;reason may be improper memory settings, one can find optimal ones running ddr test&lt;/P&gt;
&lt;P&gt;and updating image as described in MSCALE_DDR_Tool_User_Guide&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 11:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1329417#M179072</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-25T11:43:09Z</dc:date>
    </item>
    <item>
      <title>Re: System hang up when running uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1330189#M179138</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;We already used the DDR Tool to run loop test of the Stress test. But no failure after many loops.&lt;/P&gt;&lt;P&gt;So we think it is not related to memory settings. Any other suggestions?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 08:47:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1330189#M179138</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2021-08-26T08:47:45Z</dc:date>
    </item>
    <item>
      <title>Re: System hang up when running uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1339705#M180043</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Do you have any other suggestions on this case?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 09:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1339705#M180043</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2021-09-14T09:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: System hang up when running uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1340345#M180110</link>
      <description>&lt;P&gt;Hi Simon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;please try to reproduce issue on i.MX8MQ EVK board.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 07:15:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1340345#M180110</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-09-15T07:15:37Z</dc:date>
    </item>
    <item>
      <title>Re: System hang up when running uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1341057#M180183</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;We can reproduce the issue on the EVKB. The debug log I posted was captured from the EVKB. What information we can get from the below log?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;(gdb) info reg&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x0 0x2 2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x1 0xbffad2dd 3220886237&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x2 0x5cc27dc8 1556250056&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x3 0x4040000 67371008&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x4 0xfffffffffffffb81 18446744073709550465&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x5 0x10 16&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x6 0xffffffd0 4294967248&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x7 0x3 3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x8 0xbf9335f0 3214095856&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x9 0x8 8&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x10 0xffffffd0 4294967248&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x11 0x6 6&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x12 0x1869f 99999&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x13 0xd 13&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x14 0xc 12&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x15 0xffffffff 4294967295&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x16 0x1080 4224&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x17 0x0 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x18 0xbf939d70 3214122352&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x19 0xbffd7000 3221057536&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x20 0xbdfffff8 3187671032&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x21 0xbffad4b5 3220886709&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x22 0x40000000 1073741824&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x23 0xfffffffffbfbfbfb 18446744073642179579&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x24 0x1 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x25 0x4040404 67372036&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x26 0xbe000000 3187671040&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x27 0x3 3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x28 0xbf948b50 3214183248&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x29 0xbf933690 3214096016&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;x30 0xbff45d80 3220462976&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;sp 0xbf933690 0xbf933690&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;pc 0xbff3b200 0xbff3b200&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;cpsr 0x800003c9 [ SP=1 EL=0 nRW=0 F I A D N ]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;fpsr 0x0 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;fpcr 0x0 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ELR_EL1 0x0 0x0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ESR_EL1 0x0 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SPSR_EL1 0x0 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ELR_EL2 0xbff3b200 0xbff3b200&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ESR_EL2 0x96000044 2516582468&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SPSR_EL2 0x800003c9 2147484617&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ELR_EL3 0x0 0x0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ESR_EL3 0x0 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SPSR_EL3 0x0 0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Simon&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 02:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1341057#M180183</guid>
      <dc:creator>simonng</dc:creator>
      <dc:date>2021-09-16T02:45:05Z</dc:date>
    </item>
    <item>
      <title>Re: System hang up when running uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1341376#M180218</link>
      <description>&lt;P&gt;please look at uboot mtest description:&lt;/P&gt;
&lt;P&gt;"This command may crash the system when the tested memory range includes areas that are needed for the operation of the U-Boot firnware (like exception vector code, or U-Boot's internal program code, stack or heap memory areas). "&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.denx.de/wiki/publish/DULG/to-delete/UBootCmdGroupMemory.html" target="_blank"&gt;https://www.denx.de/wiki/publish/DULG/to-delete/UBootCmdGroupMemory.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 08:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-hang-up-when-running-uboot/m-p/1341376#M180218</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-09-16T08:13:02Z</dc:date>
    </item>
  </channel>
</rss>