<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MX8MP ISP Custom Resolution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1329228#M179054</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm confused by this answer, since the semi-official Basler daA3840 Image Sensor Evaluation Kit has a camera with resolution 3840x2160, which is not an exact match of the 4K resolution listed in the table (3848x2168). It works out of the box, without having to convert anything.&lt;/P&gt;</description>
    <pubDate>Wed, 25 Aug 2021 07:48:32 GMT</pubDate>
    <dc:creator>df123</dc:creator>
    <dc:date>2021-08-25T07:48:32Z</dc:date>
    <item>
      <title>MX8MP ISP Custom Resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1323489#M178454</link>
      <description>&lt;P&gt;Dear Experts,&lt;/P&gt;&lt;P&gt;Regarding the ISP chapter in iMX8M Plus Reference Manual :&amp;nbsp;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ISP-Supported-Resolution.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/152868iF78829F5C3D2F039/image-size/large?v=v2&amp;amp;px=999" role="button" title="ISP-Supported-Resolution.png" alt="ISP-Supported-Resolution.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ISP-Supported-Resolution.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could someone help to confirm if the supported resolutions and formats in the above tables are inputs or outputs of ISP? And is custom resolution such as 1440x1080 also supported? If not by default, how to enable it, please ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks very much in advance,&lt;BR /&gt;Khang&lt;/P&gt;</description>
      <pubDate>Sun, 15 Aug 2021 08:16:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1323489#M178454</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2021-08-15T08:16:05Z</dc:date>
    </item>
    <item>
      <title>Re: MX8MP ISP Custom Resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1328664#M178996</link>
      <description>&lt;P&gt;Hello khang,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Those resolution are input, and you have to convert your resolution if you don't have like this.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 13:08:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1328664#M178996</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-08-24T13:08:22Z</dc:date>
    </item>
    <item>
      <title>Re: MX8MP ISP Custom Resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1328717#M179004</link>
      <description>&lt;P&gt;Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846"&gt;@Bio_TICFSL&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Did you mean that the custom resolution (such as 1440x1080) is NOT supported by default ? Could you clarify more about "convert" from custom resolution to supported resolution(s), please ?&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Khang&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 14:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1328717#M179004</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2021-08-24T14:33:02Z</dc:date>
    </item>
    <item>
      <title>Re: MX8MP ISP Custom Resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1328754#M179005</link>
      <description>&lt;P&gt;Correct! is not supported by default, you have to change the resolution or convert it.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 15:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1328754#M179005</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-08-24T15:33:32Z</dc:date>
    </item>
    <item>
      <title>Re: MX8MP ISP Custom Resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1328789#M179007</link>
      <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846"&gt;@Bio_TICFSL&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Just my last question : By changing /converting the custom resolution, do you mean to change or to convert it into one of the supported resolutions in the tables of initial message (i.e. these supported resolutions are imposed by the ISP) or could I modify some source code of ISP (if available) to handle the this custom resolution? I would have been thinking that resolution is something generic and customizable since both&lt;STRONG&gt; isp-imx&lt;/STRONG&gt; and &lt;STRONG&gt;isp-vvcam&lt;/STRONG&gt; allow to define it via &lt;STRONG&gt;width&lt;/STRONG&gt; &amp;amp; &lt;STRONG&gt;height&lt;/STRONG&gt; parameters of &lt;EM&gt;&lt;STRONG&gt;struct&lt;/STRONG&gt;&lt;/EM&gt; &lt;STRONG&gt;vvcam_mode_info&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Khang&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 16:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1328789#M179007</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2021-08-24T16:21:53Z</dc:date>
    </item>
    <item>
      <title>Re: MX8MP ISP Custom Resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1329228#M179054</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm confused by this answer, since the semi-official Basler daA3840 Image Sensor Evaluation Kit has a camera with resolution 3840x2160, which is not an exact match of the 4K resolution listed in the table (3848x2168). It works out of the box, without having to convert anything.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 07:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1329228#M179054</guid>
      <dc:creator>df123</dc:creator>
      <dc:date>2021-08-25T07:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: MX8MP ISP Custom Resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1329284#M179060</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186472"&gt;@df123&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;I would say that 3848x2168 includes certain extra pixels and / or meta-data and is not far from 3840x2160. For my own case, the total number of pixels is 1456x1098, then the effective/active number of pixels is 1456x1088. However, the recommended recording pixels is 1440x1080.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;K.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 08:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8MP-ISP-Custom-Resolution/m-p/1329284#M179060</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2021-08-25T08:36:06Z</dc:date>
    </item>
  </channel>
</rss>