<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AVB demo board selection and purchase in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/AVB-demo-board-selection-and-purchase/m-p/1329025#M179031</link>
    <description>&lt;P&gt;Hi NXP,&lt;BR /&gt;I want to setup an AVB demo project to evaluate the AVB and automotive Ethernet technology, my requirements are as follows:&lt;/P&gt;&lt;P&gt;1.Demonstrate the AVB synchronization mechanism. That is, there are two ECUs to display from the same video/audio source(Such as computer or a camera), and they are perfectly synchronized in the sreen.&lt;/P&gt;&lt;P&gt;2.Evaluate other automotive Ethernet technology such as SOA(Service Oriented Architecture), so traditional TCP/IP stack is still required.&lt;/P&gt;&lt;P&gt;3.RTOS development environment is preferred.(Maybe we don't want to learn Linux)&lt;BR /&gt;I have researced the hardware source from NXP and I think maybe SABRE platform will fulfil my requirements, so I made the following selection:&lt;/P&gt;&lt;P&gt;1. CPU base board:&amp;nbsp;MCIMXABASEV1&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. CPU card: MCIMX6DLAICPU2 ( i.MX 6DualLite/6Solo)&lt;/P&gt;&lt;P&gt;3. Ethernet card: IMXAI2ETH-BRC (Broadcom Ethernet)&lt;/P&gt;&lt;P&gt;(Because I need to simulate two ECUs, I will purchase two pieces for item 1,2,3)&lt;/P&gt;&lt;P&gt;4.Ethernet switch:SJA1105Q-EVB (Used for AVB stream data switch)&lt;/P&gt;&lt;P&gt;5.Ethernet&amp;nbsp;port convertor:RDDRONE-T1ADAPT (If the data source comes from my laptop, I need a convertor to convert RJ45 to 100 Base-T1 connector)&lt;/P&gt;&lt;P&gt;My question are as follows:&lt;/P&gt;&lt;P&gt;1.Is my hardware selection correct to fulfil my requirements?&lt;/P&gt;&lt;P&gt;2.After I purchased these EVBs listed above, where can I get the AVB stack software?&lt;/P&gt;&lt;P&gt;3.Is any technical support can be provided after I make the purchase?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 25 Aug 2021 02:58:37 GMT</pubDate>
    <dc:creator>LiaoPanther</dc:creator>
    <dc:date>2021-08-25T02:58:37Z</dc:date>
    <item>
      <title>AVB demo board selection and purchase</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AVB-demo-board-selection-and-purchase/m-p/1329025#M179031</link>
      <description>&lt;P&gt;Hi NXP,&lt;BR /&gt;I want to setup an AVB demo project to evaluate the AVB and automotive Ethernet technology, my requirements are as follows:&lt;/P&gt;&lt;P&gt;1.Demonstrate the AVB synchronization mechanism. That is, there are two ECUs to display from the same video/audio source(Such as computer or a camera), and they are perfectly synchronized in the sreen.&lt;/P&gt;&lt;P&gt;2.Evaluate other automotive Ethernet technology such as SOA(Service Oriented Architecture), so traditional TCP/IP stack is still required.&lt;/P&gt;&lt;P&gt;3.RTOS development environment is preferred.(Maybe we don't want to learn Linux)&lt;BR /&gt;I have researced the hardware source from NXP and I think maybe SABRE platform will fulfil my requirements, so I made the following selection:&lt;/P&gt;&lt;P&gt;1. CPU base board:&amp;nbsp;MCIMXABASEV1&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. CPU card: MCIMX6DLAICPU2 ( i.MX 6DualLite/6Solo)&lt;/P&gt;&lt;P&gt;3. Ethernet card: IMXAI2ETH-BRC (Broadcom Ethernet)&lt;/P&gt;&lt;P&gt;(Because I need to simulate two ECUs, I will purchase two pieces for item 1,2,3)&lt;/P&gt;&lt;P&gt;4.Ethernet switch:SJA1105Q-EVB (Used for AVB stream data switch)&lt;/P&gt;&lt;P&gt;5.Ethernet&amp;nbsp;port convertor:RDDRONE-T1ADAPT (If the data source comes from my laptop, I need a convertor to convert RJ45 to 100 Base-T1 connector)&lt;/P&gt;&lt;P&gt;My question are as follows:&lt;/P&gt;&lt;P&gt;1.Is my hardware selection correct to fulfil my requirements?&lt;/P&gt;&lt;P&gt;2.After I purchased these EVBs listed above, where can I get the AVB stack software?&lt;/P&gt;&lt;P&gt;3.Is any technical support can be provided after I make the purchase?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 02:58:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AVB-demo-board-selection-and-purchase/m-p/1329025#M179031</guid>
      <dc:creator>LiaoPanther</dc:creator>
      <dc:date>2021-08-25T02:58:37Z</dc:date>
    </item>
    <item>
      <title>Re: AVB demo board selection and purchase</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AVB-demo-board-selection-and-purchase/m-p/1332654#M179404</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regarding your questions&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1.Is my hardware selection correct to fulfil my requirements?&lt;/P&gt;
&lt;P&gt;ANSWER.&amp;nbsp; Yes, you have the correct hardware selection.&lt;/P&gt;
&lt;P&gt;2.After I purchased these EVBs listed above, where can I get the AVB stack software?&lt;/P&gt;
&lt;P&gt;ANSWER.&amp;nbsp; The AVB Stack, it is license separately, please contact your local sales, to get a quote depending on your requirement of licenses.&lt;/P&gt;
&lt;P&gt;3.Is any technical support can be provided after I make the purchase?&lt;/P&gt;
&lt;P&gt;ANSWER.&amp;nbsp; Yes, we have offer Pro Support for this License Software pack.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Aug 2021 17:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AVB-demo-board-selection-and-purchase/m-p/1332654#M179404</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2021-08-31T17:34:37Z</dc:date>
    </item>
  </channel>
</rss>