<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mm encrypted uboot failed to load linux kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1326286#M178755</link>
    <description>&lt;P&gt;I built a encrypted uboot, it can load the kernel image and dtb file, but gave an error of "Could not create optee node.ERROR: system-specific fdt fixup failed: FDT_ERR_NOTFOUND". I hangs there. Please refer to below for details. Could you advise that I used the correct versions of below modules? If not, what are the correct versions?&lt;/P&gt;&lt;P&gt;Uboot version: lf_v2021.04&lt;/P&gt;&lt;P&gt;Optee os: imx_5.4.70_2.3.0&lt;/P&gt;&lt;P&gt;Imx-atf: lf-5.4.y&lt;/P&gt;&lt;P&gt;Imx-mkimage: lf-5.10.y_2.0.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot SPL 2021.04-dirty (Aug 11 2021 - 17:15:21 +0800)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 3000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from MMC1&lt;/P&gt;&lt;P&gt;Authenticate image from DDR location 0x401fcdc0...&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2021.04-dirty (Aug 11 2021 - 17:15:21 +0800)&lt;/P&gt;&lt;P&gt;alloc space exhausted&lt;BR /&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 36C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;mxs_video lcdif@32e00000: failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;/P&gt;&lt;P&gt;[0] lcdif@32e00000, video&lt;BR /&gt;[1] mipi_dsi@32e10000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;mxs_video lcdif@32e00000: failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;SEC0: RNG instantiated&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF 7b3389d&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Net: eth0: ethernet@30be0000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;starting USB...&lt;BR /&gt;Bus usb@32e40000: Port not available.&lt;BR /&gt;USB is stopped. Please issue 'usb start' first.&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Scanning mmc 1:1...&lt;BR /&gt;47412 bytes read in 3 ms (15.1 MiB/s)&lt;BR /&gt;Scanning disk mmc@30b50000.blk...&lt;BR /&gt;Scanning disk mmc@30b60000.blk...&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;Found 16 disks&lt;BR /&gt;No EFI system partition&lt;BR /&gt;adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;mxs_video lcdif@32e00000: failed to get any video link display timings&lt;BR /&gt;Could not create optee node.&lt;BR /&gt;ERROR: system-specific fdt fixup failed: FDT_ERR_NOTFOUND&lt;BR /&gt;- must RESET the board to recover.&lt;/P&gt;&lt;P&gt;ERROR: failed to process device tree&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;Running BSP bootcmd ...&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Failed to load 'boot.scr'&lt;BR /&gt;30083672 bytes read in 318 ms (90.2 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;47412 bytes read in 3 ms (15.1 MiB/s)&lt;/P&gt;&lt;P&gt;Authenticate image from DDR location 0x40480000...&lt;/P&gt;&lt;P&gt;Secure boot enabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xcc, HAB State: 0x99&lt;BR /&gt;No HAB Events Found!&lt;/P&gt;&lt;P&gt;Moving Image from 0x40480000 to 0x40600000, end=422b0000&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt;Booting using the fdt blob at 0x43000000&lt;BR /&gt;Using Device Tree in place at 0000000043000000, end 000000004300e933&lt;BR /&gt;Could not create optee node.&lt;BR /&gt;ERROR: system-specific fdt fixup failed: FDT_ERR_NOTFOUND&lt;BR /&gt;- must RESET the board to recover.&lt;/P&gt;&lt;P&gt;FDT creation failed! hanging...### ERROR ### Please RESET the board ###&lt;/P&gt;</description>
    <pubDate>Thu, 19 Aug 2021 13:01:37 GMT</pubDate>
    <dc:creator>yanghongsing1</dc:creator>
    <dc:date>2021-08-19T13:01:37Z</dc:date>
    <item>
      <title>imx8mm encrypted uboot failed to load linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1326286#M178755</link>
      <description>&lt;P&gt;I built a encrypted uboot, it can load the kernel image and dtb file, but gave an error of "Could not create optee node.ERROR: system-specific fdt fixup failed: FDT_ERR_NOTFOUND". I hangs there. Please refer to below for details. Could you advise that I used the correct versions of below modules? If not, what are the correct versions?&lt;/P&gt;&lt;P&gt;Uboot version: lf_v2021.04&lt;/P&gt;&lt;P&gt;Optee os: imx_5.4.70_2.3.0&lt;/P&gt;&lt;P&gt;Imx-atf: lf-5.4.y&lt;/P&gt;&lt;P&gt;Imx-mkimage: lf-5.10.y_2.0.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot SPL 2021.04-dirty (Aug 11 2021 - 17:15:21 +0800)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 3000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from MMC1&lt;/P&gt;&lt;P&gt;Authenticate image from DDR location 0x401fcdc0...&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2021.04-dirty (Aug 11 2021 - 17:15:21 +0800)&lt;/P&gt;&lt;P&gt;alloc space exhausted&lt;BR /&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 36C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;mxs_video lcdif@32e00000: failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;/P&gt;&lt;P&gt;[0] lcdif@32e00000, video&lt;BR /&gt;[1] mipi_dsi@32e10000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;mxs_video lcdif@32e00000: failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;SEC0: RNG instantiated&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF 7b3389d&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Net: eth0: ethernet@30be0000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;starting USB...&lt;BR /&gt;Bus usb@32e40000: Port not available.&lt;BR /&gt;USB is stopped. Please issue 'usb start' first.&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Scanning mmc 1:1...&lt;BR /&gt;47412 bytes read in 3 ms (15.1 MiB/s)&lt;BR /&gt;Scanning disk mmc@30b50000.blk...&lt;BR /&gt;Scanning disk mmc@30b60000.blk...&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;Found 16 disks&lt;BR /&gt;No EFI system partition&lt;BR /&gt;adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;mxs_video lcdif@32e00000: failed to get any video link display timings&lt;BR /&gt;Could not create optee node.&lt;BR /&gt;ERROR: system-specific fdt fixup failed: FDT_ERR_NOTFOUND&lt;BR /&gt;- must RESET the board to recover.&lt;/P&gt;&lt;P&gt;ERROR: failed to process device tree&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;** Unrecognized filesystem type **&lt;BR /&gt;Running BSP bootcmd ...&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Failed to load 'boot.scr'&lt;BR /&gt;30083672 bytes read in 318 ms (90.2 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;47412 bytes read in 3 ms (15.1 MiB/s)&lt;/P&gt;&lt;P&gt;Authenticate image from DDR location 0x40480000...&lt;/P&gt;&lt;P&gt;Secure boot enabled&lt;/P&gt;&lt;P&gt;HAB Configuration: 0xcc, HAB State: 0x99&lt;BR /&gt;No HAB Events Found!&lt;/P&gt;&lt;P&gt;Moving Image from 0x40480000 to 0x40600000, end=422b0000&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt;Booting using the fdt blob at 0x43000000&lt;BR /&gt;Using Device Tree in place at 0000000043000000, end 000000004300e933&lt;BR /&gt;Could not create optee node.&lt;BR /&gt;ERROR: system-specific fdt fixup failed: FDT_ERR_NOTFOUND&lt;BR /&gt;- must RESET the board to recover.&lt;/P&gt;&lt;P&gt;FDT creation failed! hanging...### ERROR ### Please RESET the board ###&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 13:01:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1326286#M178755</guid>
      <dc:creator>yanghongsing1</dc:creator>
      <dc:date>2021-08-19T13:01:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm encrypted uboot failed to load linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1326516#M178780</link>
      <description>&lt;P&gt;Hi Hong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can recheck optee configuration described on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_encrypted_boot.txt?h=lf_v2021.04" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_encrypted_boot.txt?h=lf_v2021.04&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In general using aligned&amp;nbsp; versions is important, so for v5.10.y recommended to use&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=lf-5.10.y" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/?h=lf-5.10.y&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-optee-os/tree/?h=lf-5.10.y_2.0.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-optee-os/tree/?h=lf-5.10.y_2.0.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 20 Aug 2021 00:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1326516#M178780</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-20T00:03:12Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm encrypted uboot failed to load linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1327230#M178866</link>
      <description>&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your advise.&lt;/P&gt;&lt;P&gt;Could you also advise which version of imx-atf and uboot-imx are aligned to lf-5.10.y? There is no lf-5.10.y at link below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-atf" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-atf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 22 Aug 2021 10:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1327230#M178866</guid>
      <dc:creator>yanghongsing1</dc:creator>
      <dc:date>2021-08-22T10:44:15Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm encrypted uboot failed to load linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1327233#M178867</link>
      <description>&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/?h=lf_v2021.04" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/?h=lf_v2021.04&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/153612i058F7F2A01C7661A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sun, 22 Aug 2021 12:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1327233#M178867</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-22T12:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm encrypted uboot failed to load linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1327706#M178906</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use modules below to build a signed flash.bin and try to generate dek_spl_blob.bin. But I got an error message of "Cannot get OP-TEE device". Could you advise what wrong with me?&lt;/P&gt;&lt;P&gt;uboot-imx: v2021.04&lt;/P&gt;&lt;P&gt;imx-optee-os: lf-5.10_2.2.0.0&lt;/P&gt;&lt;P&gt;imx-atf: lf-5.4.y&lt;/P&gt;&lt;P&gt;imx-mkimage: lf-5.10_2.0.0&lt;/P&gt;</description>
      <pubDate>Mon, 23 Aug 2021 10:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1327706#M178906</guid>
      <dc:creator>yanghongsing1</dc:creator>
      <dc:date>2021-08-23T10:00:44Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm encrypted uboot failed to load linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1349298#M180910</link>
      <description>&lt;P&gt;Hello Hong,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please check that imx-atf was built with "SPD=opteed" as decribed by the &lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_encrypted_boot.txt?h=lf_v2021.04" target="_blank" rel="noopener"&gt;U-boot documentation Igor linked above?&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="elginallen_0-1633028501535.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158032iF1C0FDFF9CB565FD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="elginallen_0-1633028501535.png" alt="elginallen_0-1633028501535.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;elginallen_0-1633028501535.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;That was my issue when I encountered "Cannot get OP-TEE device".&lt;/P&gt;
&lt;P&gt;Best,&lt;/P&gt;
&lt;P&gt;Elgin&lt;/P&gt;</description>
      <pubDate>Thu, 30 Sep 2021 19:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-encrypted-uboot-failed-to-load-linux-kernel/m-p/1349298#M180910</guid>
      <dc:creator>elginallen</dc:creator>
      <dc:date>2021-09-30T19:02:34Z</dc:date>
    </item>
  </channel>
</rss>