<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Relationship between waveform disturbance and operation problem in MIPI HS mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Relationship-between-waveform-disturbance-and-operation-problem/m-p/1326208#M178744</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I am trying to send an image from MCIMX8M-EVK to the original DSI panel with MIPI-DSI, but it does not work.&lt;BR /&gt;It worked a few times, but when I restart the EVK after it works, it doesn't work.&lt;BR /&gt;Most likely it won't work.&lt;BR /&gt;The only change in the state before and after restarting is connecting and disconnecting the connection cable.&lt;BR /&gt;(The state expressed as working is the state in which the number of received image frames on the panel side is increasing.)&lt;/P&gt;&lt;P&gt;The waveform of the HS mode data line is attached.&lt;BR /&gt;When the left side moves, when the right side does not move.&lt;/P&gt;&lt;P&gt;Is there a possibility that the register setting is bad as the cause of the above not working?&lt;/P&gt;&lt;P&gt;The DSI panel cannot receive data just by restarting the EVK, and the HS mode waveform is distorted. I don't know the reason for this.&lt;/P&gt;&lt;P&gt;Regarding EMI (mixture of noise), I think it is different because there is no noise in the LP mode waveform.&lt;/P&gt;&lt;P&gt;best regards.&lt;/P&gt;&lt;P&gt;Takuya.&lt;/P&gt;</description>
    <pubDate>Sat, 21 Aug 2021 01:23:05 GMT</pubDate>
    <dc:creator>Takuya-k</dc:creator>
    <dc:date>2021-08-21T01:23:05Z</dc:date>
    <item>
      <title>Relationship between waveform disturbance and operation problem in MIPI HS mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Relationship-between-waveform-disturbance-and-operation-problem/m-p/1326208#M178744</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I am trying to send an image from MCIMX8M-EVK to the original DSI panel with MIPI-DSI, but it does not work.&lt;BR /&gt;It worked a few times, but when I restart the EVK after it works, it doesn't work.&lt;BR /&gt;Most likely it won't work.&lt;BR /&gt;The only change in the state before and after restarting is connecting and disconnecting the connection cable.&lt;BR /&gt;(The state expressed as working is the state in which the number of received image frames on the panel side is increasing.)&lt;/P&gt;&lt;P&gt;The waveform of the HS mode data line is attached.&lt;BR /&gt;When the left side moves, when the right side does not move.&lt;/P&gt;&lt;P&gt;Is there a possibility that the register setting is bad as the cause of the above not working?&lt;/P&gt;&lt;P&gt;The DSI panel cannot receive data just by restarting the EVK, and the HS mode waveform is distorted. I don't know the reason for this.&lt;/P&gt;&lt;P&gt;Regarding EMI (mixture of noise), I think it is different because there is no noise in the LP mode waveform.&lt;/P&gt;&lt;P&gt;best regards.&lt;/P&gt;&lt;P&gt;Takuya.&lt;/P&gt;</description>
      <pubDate>Sat, 21 Aug 2021 01:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Relationship-between-waveform-disturbance-and-operation-problem/m-p/1326208#M178744</guid>
      <dc:creator>Takuya-k</dc:creator>
      <dc:date>2021-08-21T01:23:05Z</dc:date>
    </item>
    <item>
      <title>Re: Relationship between waveform disturbance and operation problem in MIPI HS mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Relationship-between-waveform-disturbance-and-operation-problem/m-p/1327163#M178860</link>
      <description>&lt;P&gt;Hi　Sir,&lt;BR /&gt;Withdraw the question.&lt;BR /&gt;&lt;BR /&gt;Regards.&lt;BR /&gt;Takuya.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 21 Aug 2021 01:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Relationship-between-waveform-disturbance-and-operation-problem/m-p/1327163#M178860</guid>
      <dc:creator>Takuya-k</dc:creator>
      <dc:date>2021-08-21T01:24:53Z</dc:date>
    </item>
  </channel>
</rss>