<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX RT 1176 GPIO_SNVS_00 function in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-1176-GPIO-SNVS-00-function/m-p/1325870#M178703</link>
    <description>&lt;P&gt;Hello, experts&lt;/P&gt;&lt;P&gt;I'm using the GPIO_SNVS_00 function of i.mx RT 1176 , but it sames that the GPIO functon did not work.&lt;/P&gt;&lt;P&gt;As there is a discription 'For GPIO13_IO3-GPIO13_IO12, GPIO functions are not available on devices that support tamper' in the datasheet.&lt;/P&gt;&lt;P&gt;So, could you please help check does the part number'PIMXRT1176DVMAA' support the&amp;nbsp;GPIO_SNVS_00 function ? If yes , are there any other configs that this fucntion needs?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;</description>
    <pubDate>Thu, 19 Aug 2021 06:05:24 GMT</pubDate>
    <dc:creator>starwarrior</dc:creator>
    <dc:date>2021-08-19T06:05:24Z</dc:date>
    <item>
      <title>i.MX RT 1176 GPIO_SNVS_00 function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-1176-GPIO-SNVS-00-function/m-p/1325870#M178703</link>
      <description>&lt;P&gt;Hello, experts&lt;/P&gt;&lt;P&gt;I'm using the GPIO_SNVS_00 function of i.mx RT 1176 , but it sames that the GPIO functon did not work.&lt;/P&gt;&lt;P&gt;As there is a discription 'For GPIO13_IO3-GPIO13_IO12, GPIO functions are not available on devices that support tamper' in the datasheet.&lt;/P&gt;&lt;P&gt;So, could you please help check does the part number'PIMXRT1176DVMAA' support the&amp;nbsp;GPIO_SNVS_00 function ? If yes , are there any other configs that this fucntion needs?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 06:05:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-1176-GPIO-SNVS-00-function/m-p/1325870#M178703</guid>
      <dc:creator>starwarrior</dc:creator>
      <dc:date>2021-08-19T06:05:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT 1176 GPIO_SNVS_00 function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-1176-GPIO-SNVS-00-function/m-p/1327766#M178909</link>
      <description>&lt;P&gt;According to the latest Rev.1 Data Sheet documents for the i.MX RT117x parts, &lt;BR /&gt;only the MIMXRT1173CVM8A part has the Tamper functionality, so, the GPIO &lt;BR /&gt;functionality should be available on the GPIO_SNVS_00 - GPIO_SNVS_09 pads for &lt;BR /&gt;all i.MX RT1176 parts.&lt;/P&gt;
&lt;P&gt;To use this functionality, you first have to select the correct IOMUX function &lt;BR /&gt;in the SW_MUX_CTL_PAD_GPIO_SNVS_00_DIG register, then enable and configure the &lt;BR /&gt;pad functionality in the SW_PAD_CTL_PAD_GPIO_SNVS_00_DIG register, and then &lt;BR /&gt;appropriately configure the GPIO functionality for the GPIO13_IO03 istance. For &lt;BR /&gt;details, please refer to the Sections 12.4.1.5, 12.4.1.21 and Chapter 13 of the &lt;BR /&gt;i.MX RT1170 Processor Reference Manual document, available on the processor's &lt;BR /&gt;Documentation web page:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-mcus/i-mx-rt1170-crossover-mcu-family-first-ghz-mcu-with-arm-cortex-m7-and-cortex-m4-cores:i.MX-RT1170?tab=Documentation_Tab" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-mcus/i-mx-rt1170-crossover-mcu-family-first-ghz-mcu-with-arm-cortex-m7-and-cortex-m4-cores:i.MX-RT1170?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Artur&lt;/P&gt;</description>
      <pubDate>Mon, 23 Aug 2021 11:37:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-1176-GPIO-SNVS-00-function/m-p/1327766#M178909</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2021-08-23T11:37:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX RT 1176 GPIO_SNVS_00 function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-1176-GPIO-SNVS-00-function/m-p/1330220#M179142</link>
      <description>&lt;P&gt;Hello ,Artur&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply. As my chip is a prototye sample. It seams that the sample is default to enable the tamper function. As I write the fuse 860H to 0000C000,&amp;nbsp; I can use the GPIO function.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Nick&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 09:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-RT-1176-GPIO-SNVS-00-function/m-p/1330220#M179142</guid>
      <dc:creator>starwarrior</dc:creator>
      <dc:date>2021-08-26T09:06:20Z</dc:date>
    </item>
  </channel>
</rss>