<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Required Documents related to create Android Application APK for IMX8MM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Required-Documents-related-to-create-Android-Application-APK-for/m-p/1325139#M178638</link>
    <description>&lt;P&gt;I have built application to access the GPIO pin but i am not able to but if i am connecting to Putty and using command line .. And type su command which goes to the root permisssion then only i am able to access the gpio. But due to i am using Android I have to access through application layer only . I am not able to provide even run time command as su.&lt;/P&gt;&lt;P&gt;Any one sample code Application is also fyn .I can build Application having reference to that .But the Sample should be purely with respect to NXP imx8mm board only.. Because i try with digi, tordex, vardin, varsitice.. Those application is not supporting to our nxp imx8mm.&lt;/P&gt;&lt;P&gt;Kindly provide more details&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Ruban&lt;/P&gt;</description>
    <pubDate>Wed, 18 Aug 2021 03:45:12 GMT</pubDate>
    <dc:creator>Ruban1</dc:creator>
    <dc:date>2021-08-18T03:45:12Z</dc:date>
    <item>
      <title>Required Documents related to create Android Application APK for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Required-Documents-related-to-create-Android-Application-APK-for/m-p/1322598#M178333</link>
      <description>&lt;P&gt;Required Documents related to create Android Application APK for IMX8MM.&lt;/P&gt;&lt;P&gt;How to access from application the hardware like GPIO, I2C, UART etc .&lt;/P&gt;&lt;P&gt;How to execute su command from Application APK.&lt;/P&gt;&lt;P&gt;Kindly provide every related documents for accessing NXP IMX8MM from Android Application APK.&lt;/P&gt;&lt;P&gt;Thanks and Regard&lt;/P&gt;&lt;P&gt;Ruban&lt;/P&gt;</description>
      <pubDate>Thu, 12 Aug 2021 11:06:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Required-Documents-related-to-create-Android-Application-APK-for/m-p/1322598#M178333</guid>
      <dc:creator>Ruban1</dc:creator>
      <dc:date>2021-08-12T11:06:50Z</dc:date>
    </item>
    <item>
      <title>Re: Required Documents related to create Android Application APK for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Required-Documents-related-to-create-Android-Application-APK-for/m-p/1324998#M178618</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You may refer to the google documentation for this, please check the following link:&lt;BR /&gt;&lt;A href="https://developer.android.com/" target="_blank"&gt;https://developer.android.com/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 23:12:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Required-Documents-related-to-create-Android-Application-APK-for/m-p/1324998#M178618</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-08-17T23:12:23Z</dc:date>
    </item>
    <item>
      <title>Re: Required Documents related to create Android Application APK for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Required-Documents-related-to-create-Android-Application-APK-for/m-p/1325139#M178638</link>
      <description>&lt;P&gt;I have built application to access the GPIO pin but i am not able to but if i am connecting to Putty and using command line .. And type su command which goes to the root permisssion then only i am able to access the gpio. But due to i am using Android I have to access through application layer only . I am not able to provide even run time command as su.&lt;/P&gt;&lt;P&gt;Any one sample code Application is also fyn .I can build Application having reference to that .But the Sample should be purely with respect to NXP imx8mm board only.. Because i try with digi, tordex, vardin, varsitice.. Those application is not supporting to our nxp imx8mm.&lt;/P&gt;&lt;P&gt;Kindly provide more details&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Ruban&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 03:45:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Required-Documents-related-to-create-Android-Application-APK-for/m-p/1325139#M178638</guid>
      <dc:creator>Ruban1</dc:creator>
      <dc:date>2021-08-18T03:45:12Z</dc:date>
    </item>
  </channel>
</rss>