<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: M4 core i2c example code not working when we Boot A53 with linux 5.10.3</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/M4-core-i2c-example-code-not-working-when-we-Boot-A53-with-linux/m-p/1325003#M178620</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Have you tried using the imx8mm-evk-rpmsg.dtb?&lt;BR /&gt;This device tree blob already have disabled the IPs needed for the M4 SDK examples for our EVK.&lt;BR /&gt;&lt;BR /&gt;You may change default dtb with the following steps:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Stop the boot process at U-boot.&lt;/LI&gt;
&lt;LI&gt;Type the uboot command:&lt;BR /&gt;&amp;gt; setenv fdt_file imx8mm-evk-rpmsg.dtb&lt;BR /&gt;&amp;gt; saveenv&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;BR /&gt;Also, please note that the changes to dtsi you have shared are for the i.MX8MN not the i.MX8MM&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Tue, 17 Aug 2021 23:28:08 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2021-08-17T23:28:08Z</dc:date>
    <item>
      <title>M4 core i2c example code not working when we Boot A53 with linux 5.10.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/M4-core-i2c-example-code-not-working-when-we-Boot-A53-with-linux/m-p/1323222#M178413</link>
      <description>&lt;P&gt;Hello Sir,&lt;/P&gt;&lt;P&gt;We are using imx8m mini evk board&amp;nbsp;&lt;/P&gt;&lt;P&gt;Both core we are using M4 core and A53&amp;nbsp;&lt;/P&gt;&lt;P&gt;On M4 core side we uploaded i2c example code&amp;nbsp;i2c_polling_b2b_transfer_master.bin and on A53 core linux 5.10&lt;/P&gt;&lt;P&gt;Initally M4 core working fine but when we boot A53 with linux , M4 core stops working even it is I2C example code only not modified any thing in I2C example code.&lt;/P&gt;&lt;P&gt;also we have disabled all I2C in .dtsi file and then checked but still same issue&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But in android it is working (M4 I2C example and A53 core with android 10)&lt;/P&gt;&lt;P&gt;but only it is not working on linux&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have attached i2c example code , .dtsi file and linux version screenshot.&lt;/P&gt;&lt;P&gt;Please suggest&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Aug 2021 12:05:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/M4-core-i2c-example-code-not-working-when-we-Boot-A53-with-linux/m-p/1323222#M178413</guid>
      <dc:creator>anilpathrut</dc:creator>
      <dc:date>2021-08-13T12:05:17Z</dc:date>
    </item>
    <item>
      <title>Re: M4 core i2c example code not working when we Boot A53 with linux 5.10.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/M4-core-i2c-example-code-not-working-when-we-Boot-A53-with-linux/m-p/1325003#M178620</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Have you tried using the imx8mm-evk-rpmsg.dtb?&lt;BR /&gt;This device tree blob already have disabled the IPs needed for the M4 SDK examples for our EVK.&lt;BR /&gt;&lt;BR /&gt;You may change default dtb with the following steps:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Stop the boot process at U-boot.&lt;/LI&gt;
&lt;LI&gt;Type the uboot command:&lt;BR /&gt;&amp;gt; setenv fdt_file imx8mm-evk-rpmsg.dtb&lt;BR /&gt;&amp;gt; saveenv&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;BR /&gt;Also, please note that the changes to dtsi you have shared are for the i.MX8MN not the i.MX8MM&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 23:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/M4-core-i2c-example-code-not-working-when-we-Boot-A53-with-linux/m-p/1325003#M178620</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-08-17T23:28:08Z</dc:date>
    </item>
  </channel>
</rss>