<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mx6pep Driver when loaded, board reboots continuously in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mx6pep-Driver-when-loaded-board-reboots-continuously/m-p/1324467#M178555</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using iMX6DL processor which runs in Windows IoT Core BSP for our project. we had mx6pep driver (as part of BSP) which will be used for power management. We can see that driver as part of a FFU image, but in loaded drivers, it's not included. When we tried to load mx6pep driver, board is continuously resetting.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why loading the mx6pep driver causes board to reboot? and is their any reason for that driver to be not loaded automatically?&lt;/P&gt;</description>
    <pubDate>Tue, 17 Aug 2021 07:37:13 GMT</pubDate>
    <dc:creator>Zaid_Noordeen</dc:creator>
    <dc:date>2021-08-17T07:37:13Z</dc:date>
    <item>
      <title>mx6pep Driver when loaded, board reboots continuously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx6pep-Driver-when-loaded-board-reboots-continuously/m-p/1324467#M178555</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using iMX6DL processor which runs in Windows IoT Core BSP for our project. we had mx6pep driver (as part of BSP) which will be used for power management. We can see that driver as part of a FFU image, but in loaded drivers, it's not included. When we tried to load mx6pep driver, board is continuously resetting.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why loading the mx6pep driver causes board to reboot? and is their any reason for that driver to be not loaded automatically?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 07:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx6pep-Driver-when-loaded-board-reboots-continuously/m-p/1324467#M178555</guid>
      <dc:creator>Zaid_Noordeen</dc:creator>
      <dc:date>2021-08-17T07:37:13Z</dc:date>
    </item>
  </channel>
</rss>