<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: stuck in the kernel using trained DDR bin in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324348#M178540</link>
    <description>&lt;P&gt;The purpose of using this board is preparing for our board that is made with IMX8M chips, and our board is in the works.&lt;/P&gt;&lt;P&gt;I just want to run the&amp;nbsp;minimum system on this board, for this target, the ddr issue seem to be the last problem.&lt;/P&gt;&lt;P&gt;And we also use the DDR4 in our board, so I think it is important to find the solution out.&lt;/P&gt;&lt;P&gt;we could talk about this issue and if it is our board.&lt;/P&gt;&lt;P&gt;So let's focus on the issue itself.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 17 Aug 2021 05:37:55 GMT</pubDate>
    <dc:creator>peter-vzense</dc:creator>
    <dc:date>2021-08-17T05:37:55Z</dc:date>
    <item>
      <title>stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1323442#M178446</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use one third-part I.MX8MM board to pre-debug for our project.&lt;/P&gt;&lt;P&gt;this board use DDR4 that is&amp;nbsp;MT40A512M16LY-062E&lt;/P&gt;&lt;P&gt;After the DDR training, I put the ddr4_timing.c into the uboot. After that the uboot works fine, but it stuck in the kernel when the login come out.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I have some questions like below:&lt;/P&gt;&lt;P&gt;1. Except changing the ddr timing files in the uboot, which steps need to be done?&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. In the&amp;nbsp;MX8M_Mini_DDR4_RPA_v15.xlsx, there are only 2&amp;nbsp;frequency setpoints can be chosen, and only 533 or 668 can be the sencond setpoint value. But in the LPDDR4 RPA, there are 3 setpoints and can set it manually. why have this limitation? if I want to change the setpoints to other value, how can I do that?&lt;/P&gt;&lt;P&gt;3. In the kernel, will the DDR frequncy be changed or not? I do not see any ddr frquency value in the dts file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 14 Aug 2021 07:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1323442#M178446</guid>
      <dc:creator>peter-vzense</dc:creator>
      <dc:date>2021-08-14T07:39:47Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1323941#M178507</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Peter&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. ddr size can be adjusted using&amp;nbsp;#define PHYS_SDRAM_SIZE in&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8mm_evk.h?h=imx_v2020.04_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8mm_evk.h?h=imx_v2020.04_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also first recommended to try without OP-Tee, use sect.5.6.10 OP-TEE enablement&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_blank" rel="noopener"&gt;i.MX Yocto Project User’s Guide​&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. number of setpoints is limited in below codes:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/ddr/imx/imx8m/ddrphy_utils.c?h=imx_v2020.04_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/ddr/imx/imx8m/ddrphy_utils.c?h=imx_v2020.04_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/clk/imx/clk-imx8mm.c?h=imx_v2020.04_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/clk/imx/clk-imx8mm.c?h=imx_v2020.04_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-atf/tree/plat/imx/imx8m/ddr/clock.c?h=imx_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-atf/tree/plat/imx/imx8m/ddr/clock.c?h=imx_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3. no&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 16 Aug 2021 13:38:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1323941#M178507</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-16T13:38:37Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324179#M178526</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;thank you for you reply.&lt;/P&gt;&lt;P&gt;sorry for the missing msg.&lt;/P&gt;&lt;P&gt;1. I already changed the SDRAM_SIZE based on the board.&lt;/P&gt;&lt;P&gt;2. I do not use the TEE&lt;/P&gt;&lt;P&gt;3. I create one new board based on the imx8mm_evk in uboot, and I changed the ddr4_timing.c(from DDR tool), pmic init code(DDR4 voltage),&amp;nbsp;IMX8M_DDR4 config. And the result is like I said at the beginning.&lt;/P&gt;&lt;P&gt;About my frequncy setpoint question, I don't understand that the evk using LPDDR4 and 100,400,3000 timing table in the timing file, and I change it to the DDR4 with 1066, 2400.&lt;/P&gt;&lt;P&gt;do I need to modify somthing for that?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on your&amp;nbsp;experience, do i miss or do something wrong steps on it?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 02:01:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324179#M178526</guid>
      <dc:creator>peter-vzense</dc:creator>
      <dc:date>2021-08-17T02:01:33Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324326#M178535</link>
      <description>&lt;P&gt;you wrote:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;I use one third-part I.MX8MM board to pre-debug for our project.&lt;BR /&gt;..&lt;BR /&gt;&amp;gt;3. I create one new board based on the imx8mm_evk in uboot..&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;if it is some third party board, you can ask sources for that board from its vendor.&lt;/P&gt;
&lt;P&gt;"imx8mm_evk" build machine configuration can not be used for third party board since&lt;/P&gt;
&lt;P&gt;it is different from NXP i.MX8M Mini EVK board.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 05:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324326#M178535</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-17T05:12:51Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324348#M178540</link>
      <description>&lt;P&gt;The purpose of using this board is preparing for our board that is made with IMX8M chips, and our board is in the works.&lt;/P&gt;&lt;P&gt;I just want to run the&amp;nbsp;minimum system on this board, for this target, the ddr issue seem to be the last problem.&lt;/P&gt;&lt;P&gt;And we also use the DDR4 in our board, so I think it is important to find the solution out.&lt;/P&gt;&lt;P&gt;we could talk about this issue and if it is our board.&lt;/P&gt;&lt;P&gt;So let's focus on the issue itself.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 05:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324348#M178540</guid>
      <dc:creator>peter-vzense</dc:creator>
      <dc:date>2021-08-17T05:37:55Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324698#M178584</link>
      <description>&lt;P&gt;add some information.&lt;/P&gt;&lt;P&gt;my board use two 16bit DDR as 32bit, so could you check the parameters in my RPA? is it correct?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="WechatIMG37.jpeg" style="width: 523px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/153185i76802FCAA6D1576C/image-size/large?v=v2&amp;amp;px=999" role="button" title="WechatIMG37.jpeg" alt="WechatIMG37.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;WechatIMG37.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 11:25:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324698#M178584</guid>
      <dc:creator>peter-vzense</dc:creator>
      <dc:date>2021-08-17T11:25:59Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324733#M178591</link>
      <description>&lt;P&gt;such configuration 2xMT40A512M16LY is used on NXP i.MX8M Mini&amp;nbsp;DDR4 EVK board&lt;/P&gt;
&lt;H3 class="media-flex-heading"&gt;&lt;A id="docsAndSoftware_designResultTitle1_3" class="dtmcustomrulelink" href="https://www.nxp.com/webapp/Download?colCode=8MMINID4-EVK-DESIGNFILES" target="_blank" rel="noopener" data-dtmaction="Documents and Software Results - Software Link click" data-dtmsubaction="i.MX 8M Mini Evaluation Kit DDR4 Design Files"&gt;i.MX 8M Mini Evaluation Kit DDR4 Design Files&lt;/A&gt;&lt;/H3&gt;
&lt;P&gt;RPA Tool for it&amp;nbsp; &amp;nbsp;&lt;A id="link_15" class="lia-link-navigation attachment-link" href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443?attachment-id=117988" target="_blank" rel="noopener"&gt;MX8M_Mini_DDR4_RPA_v15.xlsx&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/153189iB879673B14945C0B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So if ddr test passed, no need for modifications in NXP uboot/linux codes for ddr. &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 12:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324733#M178591</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-17T12:27:07Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324736#M178592</link>
      <description>&lt;P&gt;just retried this configuration, bad news is having the some issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;do you have any idea for this ?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 12:22:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324736#M178592</guid>
      <dc:creator>peter-vzense</dc:creator>
      <dc:date>2021-08-17T12:22:28Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324739#M178593</link>
      <description>&lt;P&gt;please use common guidelines for DDR4 provided in sect.3.4. DDR design recommendations&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_3" href="https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Mini Hardware Developer’s Guide&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 12:31:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324739#M178593</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-17T12:31:54Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324740#M178594</link>
      <description>&lt;P&gt;one more found and share with you, hope can help us find the root.&lt;/P&gt;&lt;P&gt;I just replaced the ddr4_timing.c to the 3rd part timing file in their sdk, after that everything works fine.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So it seem the ddr timing is the key point. But I found the fsp_table have 3 value that is 2400, 400, 100 in the 3rd part sdk. and in the RPA, there can not be set to there frequncy.&amp;nbsp;&lt;/P&gt;&lt;P&gt;the code I pushed on the below link, you could reference.&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://cowtransfer.com/s/178706385ccf44" target="_blank"&gt;https://cowtransfer.com/s/178706385ccf44&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 12:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324740#M178594</guid>
      <dc:creator>peter-vzense</dc:creator>
      <dc:date>2021-08-17T12:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324829#M178606</link>
      <description>&lt;P&gt;for "3rd part timing file" suggest to apply for help to vendor of that software bsp.&lt;/P&gt;
&lt;P&gt;NXP supports only i.MX8M Mini EVK which works fine with configurations defined in&lt;/P&gt;
&lt;P&gt;RPA Tool for it&amp;nbsp; &amp;nbsp;&lt;A id="link_15" class="lia-link-navigation attachment-link" href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443?attachment-id=117988" target="_blank" rel="noopener"&gt;MX8M_Mini_DDR4_RPA_v15.xlsx&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;NXP linux documentation:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 14:55:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1324829#M178606</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-17T14:55:53Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1325049#M178628</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think NXP is one great IC company not an EVK vendor. You sell the IC itself, not just the EVK.&lt;/P&gt;&lt;P&gt;My question is about the minimum system with the I.MX8MM, not driver development with the board.&lt;/P&gt;&lt;P&gt;As you said, if I have questions on my board with NXP IC, don't you have duty to support?&lt;/P&gt;&lt;P&gt;I apologize in advance if I have some misunderstand. Or do I need to search the support from other way, you could tell us directly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 01:32:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1325049#M178628</guid>
      <dc:creator>peter-vzense</dc:creator>
      <dc:date>2021-08-18T01:32:56Z</dc:date>
    </item>
    <item>
      <title>Re: stuck in the kernel using trained DDR bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1325200#M178641</link>
      <description>&lt;P&gt;this question is about the IMX8MM_EVK, in the uboot code, the ddr4_timing.c have one struct&amp;nbsp;ddr4_dram_fsp_msg &lt;SPAN&gt;that have three rate value config 2400, 400, 100.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And in the RPA files, there are only two frequency can be set.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;do I need modify the RPA or the uboot code?&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1629265210092.jpg" style="width: 508px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/153290i95F772294F715A0B/image-size/large?v=v2&amp;amp;px=999" role="button" title="1629265210092.jpg" alt="1629265210092.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1629265210092.jpg&lt;/span&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="WechatIMG37.jpeg" style="width: 523px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/153291i3537C113C13C2183/image-size/large?v=v2&amp;amp;px=999" role="button" title="WechatIMG37.jpeg" alt="WechatIMG37.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;WechatIMG37.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 05:53:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/stuck-in-the-kernel-using-trained-DDR-bin/m-p/1325200#M178641</guid>
      <dc:creator>peter-vzense</dc:creator>
      <dc:date>2021-08-18T05:53:31Z</dc:date>
    </item>
  </channel>
</rss>