<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: device_remove error log from u-boot with i.MX8MM EVK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/device-remove-error-log-from-u-boot-with-i-MX8MM-EVK/m-p/1323806#M178495</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;
&lt;P&gt;Can I get any help or feedback?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;BR/Cliff&lt;/P&gt;</description>
    <pubDate>Mon, 16 Aug 2021 08:39:08 GMT</pubDate>
    <dc:creator>cliffkong</dc:creator>
    <dc:date>2021-08-16T08:39:08Z</dc:date>
    <item>
      <title>device_remove error log from u-boot with i.MX8MM EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/device-remove-error-log-from-u-boot-with-i-MX8MM-EVK/m-p/1314984#M177614</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;
&lt;P&gt;Customer is running L5.10.9 BSP from development board based on ii.M8MM.&amp;nbsp;u-boot and kernel booting is okay and no issue.&amp;nbsp;They report error message output from u-boot while jumping into Kernel.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;unable to select a mode&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;device_remove: Device 'mmc@30b60000.blk' failed to remove, but children are gone&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;I tested it from i.MX8MM EVK board based on same L5.10.9 and I could also see the same error message. Please refer to below log dump. Customer is cleaning up the log output and don't want to have error log from production.&lt;/P&gt;
&lt;P&gt;how to remove this error log? and why this error happen?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;U-Boot 2020.04-5.10.9-1.0.0+gad7b74b415a (Mar 05 2021 - 07:05:56 +0000)&lt;/P&gt;
&lt;P&gt;CPU: i.MX8MMQ rev1.0 at 1200MHz&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 41C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... OK&lt;BR /&gt;[*]-Video Link 0Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;/P&gt;
&lt;P&gt;[0] lcdif@32e00000, video&lt;BR /&gt;[1] mipi_dsi@32e10000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;
&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF ba76d33&lt;BR /&gt;- U-Boot 2020.04-5.10.9-1.0.0+gad7b74b415a&lt;/P&gt;
&lt;P&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Net: eth0: ethernet@30be0000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;29280768 bytes read in 161 ms (173.4 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;46889 bytes read in 12 ms (3.7 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt;Booting using the fdt blob at 0x43000000&lt;BR /&gt;Using Device Tree in place at 0000000043000000, end 000000004300e728&lt;BR /&gt;Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;failed to get any video link display timings&lt;BR /&gt;probe video device failed, ret -22&lt;/P&gt;
&lt;P&gt;Starting kernel ...&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;unable to select a mode&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;device_remove: Device 'mmc@30b60000.blk' failed to remove, but children are gone&lt;/STRONG&gt;&lt;BR /&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]&lt;BR /&gt;[ 0.000000] Linux version 5.10.9-1.0.0+g32513c25d8c7 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.0.20200730) #1 SMP PREEMPT Tue Mar&lt;/P&gt;
&lt;P&gt;...&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 03:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/device-remove-error-log-from-u-boot-with-i-MX8MM-EVK/m-p/1314984#M177614</guid>
      <dc:creator>cliffkong</dc:creator>
      <dc:date>2021-07-29T03:55:05Z</dc:date>
    </item>
    <item>
      <title>Re: device_remove error log from u-boot with i.MX8MM EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/device-remove-error-log-from-u-boot-with-i-MX8MM-EVK/m-p/1323806#M178495</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;
&lt;P&gt;Can I get any help or feedback?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;BR/Cliff&lt;/P&gt;</description>
      <pubDate>Mon, 16 Aug 2021 08:39:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/device-remove-error-log-from-u-boot-with-i-MX8MM-EVK/m-p/1323806#M178495</guid>
      <dc:creator>cliffkong</dc:creator>
      <dc:date>2021-08-16T08:39:08Z</dc:date>
    </item>
    <item>
      <title>Re: device_remove error log from u-boot with i.MX8MM EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/device-remove-error-log-from-u-boot-with-i-MX8MM-EVK/m-p/1347935#M180776</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me share my progress. Error log has been disappeared with workaround to disable&amp;nbsp;"MMC_HS400_ES_SUPPORT" from u-boot config.&lt;/P&gt;
&lt;P&gt;I see the failure log is caused by failure in setting speed mode to HS400ES. So the workaround is to deselect "MMC_HS400_ES_SUPPORT" from u-boot config. It allows to set emmc speed mode as HS400, instead of HS400ES(best mode). I still don't know why it failed in HS400ES mode although the device support it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Then I will close this ticket myself.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 02:25:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/device-remove-error-log-from-u-boot-with-i-MX8MM-EVK/m-p/1347935#M180776</guid>
      <dc:creator>cliffkong</dc:creator>
      <dc:date>2021-09-29T02:25:49Z</dc:date>
    </item>
  </channel>
</rss>