<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6 IPU waveform set in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-waveform-set/m-p/1322723#M178352</link>
    <description>&lt;P&gt;Can anyone tell me what the waveform set is actually doing?&amp;nbsp; I looked at the timing generation in the reference manual but don't fully understand what this does.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I use set 2 which was the default setting of the IMX6 SDK I believe, I get a very slow strange ghosting affecting.&amp;nbsp; It starts in the corners of the display and moves slowly into the center.&lt;/P&gt;&lt;P&gt;When I use a set of 3 it seems better but I'm just not sure why.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm also using an RGB to MIPI converter but this was originally used with an IMX53 with not issues.&lt;/P&gt;</description>
    <pubDate>Thu, 12 Aug 2021 15:43:18 GMT</pubDate>
    <dc:creator>mjrudy</dc:creator>
    <dc:date>2021-08-12T15:43:18Z</dc:date>
    <item>
      <title>IMX6 IPU waveform set</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-waveform-set/m-p/1322723#M178352</link>
      <description>&lt;P&gt;Can anyone tell me what the waveform set is actually doing?&amp;nbsp; I looked at the timing generation in the reference manual but don't fully understand what this does.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I use set 2 which was the default setting of the IMX6 SDK I believe, I get a very slow strange ghosting affecting.&amp;nbsp; It starts in the corners of the display and moves slowly into the center.&lt;/P&gt;&lt;P&gt;When I use a set of 3 it seems better but I'm just not sure why.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm also using an RGB to MIPI converter but this was originally used with an IMX53 with not issues.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Aug 2021 15:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-waveform-set/m-p/1322723#M178352</guid>
      <dc:creator>mjrudy</dc:creator>
      <dc:date>2021-08-12T15:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 IPU waveform set</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-waveform-set/m-p/1322834#M178363</link>
      <description>&lt;P&gt;Hi Micah&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can look at sect.37.4.10.3 Timing generator&amp;nbsp; &lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX6DQRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 6Dual/6Quad Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and example&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX53-How-to-move-VGA-external-HSYNC-and-VSYNC-signals-to/m-p/173296#294603" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX53-How-to-move-VGA-external-HSYNC-and-VSYNC-signals-to/m-p/173296#294603&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 13 Aug 2021 00:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-waveform-set/m-p/1322834#M178363</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-13T00:13:21Z</dc:date>
    </item>
  </channel>
</rss>