<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6UL Custom Board Booting Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Custom-Board-Booting-Issue/m-p/1320078#M178050</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have been facing a issue with booting of my i.MX6UL custom board, the changes done in the hardware is we are booting from MMC0, for MMC1 we have connected eMMC.&lt;/P&gt;&lt;P&gt;We have been using the yocto source and in the U-Boot we have changed MMC1 to MMC0 and the image as been tested in i.MX6UL EVK with MMC0 and it was working fine.&lt;/P&gt;&lt;P&gt;The changes done in the U-Boot are as follows&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SD card(mmc 0) :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;• In file board/freescale/mx6ul_14x14_evk/mx6ul_14x14_evk.c at 482 line comment return devno; add return 0;&lt;/SPAN&gt; &lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN&gt;/* If not boot from sd/mmc, use default value */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;if (bootsel != 1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;return CONFIG_SYS_MMC_ENV_DEV;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;/* BOOT_CFG2[3] and BOOT_CFG2[4] */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;dev_no = (soc_sbmr &amp;amp; 0x00001800) &amp;gt;&amp;gt; 11;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;if (dev_no == 1 &amp;amp;&amp;amp; mx6_esdhc_fused(USDHC1_BASE_ADDR))&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;dev_no = 0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;//return dev_no;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* comment this line */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;return 0;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;• In file include/configs/mx6ul_14x14_evk.h&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;#define CONFIG_SYS_MMC_ENV_DEV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;• In file include/configs/mx6ul_14x14_evk.h&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;#define CONFIG_MMCROOT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "/dev/mmcblk0p2"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The attached is the screenshot of the debug log&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Uttej Ravuri&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 09 Aug 2021 05:13:41 GMT</pubDate>
    <dc:creator>uttej_ravuri</dc:creator>
    <dc:date>2021-08-09T05:13:41Z</dc:date>
    <item>
      <title>i.MX6UL Custom Board Booting Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Custom-Board-Booting-Issue/m-p/1320078#M178050</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have been facing a issue with booting of my i.MX6UL custom board, the changes done in the hardware is we are booting from MMC0, for MMC1 we have connected eMMC.&lt;/P&gt;&lt;P&gt;We have been using the yocto source and in the U-Boot we have changed MMC1 to MMC0 and the image as been tested in i.MX6UL EVK with MMC0 and it was working fine.&lt;/P&gt;&lt;P&gt;The changes done in the U-Boot are as follows&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SD card(mmc 0) :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;• In file board/freescale/mx6ul_14x14_evk/mx6ul_14x14_evk.c at 482 line comment return devno; add return 0;&lt;/SPAN&gt; &lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN&gt;/* If not boot from sd/mmc, use default value */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;if (bootsel != 1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;return CONFIG_SYS_MMC_ENV_DEV;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;/* BOOT_CFG2[3] and BOOT_CFG2[4] */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;dev_no = (soc_sbmr &amp;amp; 0x00001800) &amp;gt;&amp;gt; 11;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;if (dev_no == 1 &amp;amp;&amp;amp; mx6_esdhc_fused(USDHC1_BASE_ADDR))&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;dev_no = 0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;//return dev_no;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* comment this line */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;return 0;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;• In file include/configs/mx6ul_14x14_evk.h&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;#define CONFIG_SYS_MMC_ENV_DEV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;• In file include/configs/mx6ul_14x14_evk.h&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;#define CONFIG_MMCROOT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "/dev/mmcblk0p2"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The attached is the screenshot of the debug log&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Uttej Ravuri&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Aug 2021 05:13:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Custom-Board-Booting-Issue/m-p/1320078#M178050</guid>
      <dc:creator>uttej_ravuri</dc:creator>
      <dc:date>2021-08-09T05:13:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL Custom Board Booting Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Custom-Board-Booting-Issue/m-p/1321785#M178235</link>
      <description>&lt;P&gt;Which version of BSP are you using? And have you set the right boot command line in u-boot?&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 09:19:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Custom-Board-Booting-Issue/m-p/1321785#M178235</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-08-11T09:19:35Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL Custom Board Booting Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Custom-Board-Booting-Issue/m-p/1321800#M178238</link>
      <description>&lt;P&gt;We are using Distro 4.19-warrior, kernal version -&lt;SPAN&gt;4.19.35-1.1.0+g8507afc3a397&lt;/SPAN&gt;&amp;nbsp; and we have also tested with Rocko.&lt;/P&gt;&lt;P&gt;The U-Boot itself is not loading, it is resetting in U-Boot the below is the log.&lt;/P&gt;&lt;P&gt;U-Boot 2015.04-dirty (Aug 10 2021 - 14:52:06)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6UL rev1.2 at 396 MHz&lt;BR /&gt;CPU: Temperature 47 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6UL 14x14 EVK&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Display: TFT43AB (480x272)&lt;BR /&gt;Video: 480x272x24&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;Net: Phy 1 not found&lt;BR /&gt;PHY reset timed out&lt;BR /&gt;FEC1&lt;BR /&gt;Error: FEC1 address not set.&lt;/P&gt;&lt;P&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt; U-Boot 2015.04-dirty (Aug 10 U-Boot 2015.04-dirty (Aug 10 U-Boot 2015.04-dirty (Aug 10 U-Boot 2015.04-dirty (Aug 10 U-Boot&lt;/P&gt;&lt;P&gt;(without hitting any key it is directly giving arrows (=&amp;gt;) and the autoboot count is not decreasing to 3 to 0. It is directly going to 0 and resetting&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;U&gt;we also tried with mfg tool the below is the log&lt;/U&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot 2015.04-imx_v2015.04_4.1.15_1.0.0_ga+g384e1c1 (Mar 13 2016 - 17:39:55)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6UL rev1.2 at 396 MHz&lt;BR /&gt;CPU: Temperature 50 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6UL 14x14 EVK&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Card did not respond to voltage select!&lt;BR /&gt;MMC init failed&lt;BR /&gt;Using default environment&lt;/P&gt;&lt;P&gt;Display: TFT43AB (480x272)&lt;BR /&gt;Video: 480x272x24&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Card did not respond to voltage select!&lt;BR /&gt;Net: Phy 1 not found&lt;BR /&gt;PHY reset timed out&lt;BR /&gt;FEC1&lt;BR /&gt;Error: FEC1 address not set.&lt;/P&gt;&lt;P&gt;Boot from USB for mfgtools&lt;BR /&gt;Use default environment for mfgtools&lt;BR /&gt;Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x552a48 ]&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 83800000 ...&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-imx6&lt;BR /&gt;Image Type: ARM Linux RAMDisk Image (gzip compressed)&lt;BR /&gt;Data Size: 7565864 Bytes = 7.2 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt;Booting using the fdt blob at 0x83000000&lt;BR /&gt;Using Device Tree in place at 83000000, end 8300b7c9&lt;BR /&gt;Modify /soc/aips-bus@02000000/bee@02044000:status disabled&lt;BR /&gt;ft_system_setup for mx6&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Linux version 4.1.15-1.0.0-mfgtool+g3924425 (bamboo@shlinux12) (gcc version 5.2.0 (GCC) ) #1 SMP PREEMPT Sun Mar 13 17:19:17 CST 2016&lt;BR /&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board&lt;BR /&gt;cma: Reserved 320 MiB at 0x8c000000&lt;BR /&gt;Memory policy: Data cache writealloc&lt;BR /&gt;PERCPU: Embedded 12 pages/cpu @8bb32000 s16768 r8192 d24192 u49152&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_massd&lt;BR /&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;BR /&gt;Memory: 173408K/524288K available (6895K kernel code, 319K rwdata, 2412K rodata, 388K init, 423K bss, 23200K reserved, 327680K cma-reserved, )&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt;vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt;fixmap : 0xffc00000 - 0xfff00000 (3072 kB)&lt;BR /&gt;vmalloc : 0xa0800000 - 0xff000000 (1512 MB)&lt;BR /&gt;lowmem : 0x80000000 - 0xa0000000 ( 512 MB)&lt;BR /&gt;pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)&lt;BR /&gt;modules : 0x7f000000 - 0x7fe00000 ( 14 MB)&lt;BR /&gt;.text : 0x80008000 - 0x8091ef88 (9308 kB)&lt;BR /&gt;.init : 0x8091f000 - 0x80980000 ( 388 kB)&lt;BR /&gt;.data : 0x80980000 - 0x809cff00 ( 320 kB)&lt;BR /&gt;.bss : 0x809d2000 - 0x80a3bf14 ( 424 kB)&lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt;Additional per-CPU info printed with stalls.&lt;BR /&gt;RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.&lt;BR /&gt;RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1&lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16&lt;BR /&gt;mxc_clocksource_init 24000000&lt;BR /&gt;Switching to timer-based delay loop, resolution 41ns&lt;BR /&gt;sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns&lt;BR /&gt;clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;/cpus/cpu@0 missing clock-frequency property&lt;BR /&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;Setting up static identity map for 0x80008280 - 0x800082f0&lt;BR /&gt;Brought up 1 CPUs&lt;BR /&gt;SMP: Total of 1 processors activated (48.00 BogoMIPS).&lt;BR /&gt;CPU: All CPU(s) started in SVC mode.&lt;BR /&gt;devtmpfs: initialized&lt;BR /&gt;device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"&lt;BR /&gt;VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5&lt;BR /&gt;clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns&lt;BR /&gt;pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;BR /&gt;cpuidle: using governor ladder&lt;BR /&gt;cpuidle: using governor menu&lt;BR /&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.&lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 8 bytes.&lt;BR /&gt;imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver&lt;BR /&gt;mxs-dma 1804000.dma-apbh: initialized&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-0: can't use DMA&lt;BR /&gt;i2c i2c-1: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-1: can't use DMA&lt;BR /&gt;Linux video capture interface: v2.00&lt;BR /&gt;pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;giometti@linux.it&amp;gt;&lt;BR /&gt;PTP clock support registered&lt;BR /&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;Switched to clocksource mxc_timer1&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;TCP established hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;TCP bind hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 4096 bind 4096)&lt;BR /&gt;UDP hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;Trying to unpack rootfs image as initramfs...&lt;BR /&gt;Freeing initrd memory: 7392K (83800000 - 83f38000)&lt;BR /&gt;imx rpmsg driver is registered.&lt;BR /&gt;Bus freq driver module loaded&lt;BR /&gt;futex hash table entries: 256 (order: 2, 16384 bytes)&lt;BR /&gt;VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;BR /&gt;NFS: Registering the id_resolver key type&lt;BR /&gt;Key type id_resolver registered&lt;BR /&gt;Key type id_legacy registered&lt;BR /&gt;jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.&lt;BR /&gt;fuse init (API version 7.23)&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;imx-weim 21b8000.weim: Driver registered.&lt;BR /&gt;backlight supply power not found, using dummy regulator&lt;BR /&gt;21c8000.lcdif supply lcd not found, using dummy regulator&lt;BR /&gt;mxsfb 21c8000.lcdif: failed to find mxc display driver&lt;BR /&gt;Console: switching to colour frame buffer device 60x34&lt;BR /&gt;mxsfb 21c8000.lcdif: initialized&lt;BR /&gt;imx-sdma 20ec000.sdma: no event needs to be remapped&lt;BR /&gt;imx-sdma 20ec000.sdma: loaded firmware 3.3&lt;BR /&gt;imx-sdma 20ec000.sdma: initialized&lt;BR /&gt;2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a IMX&lt;BR /&gt;console [ttymxc0] enabled&lt;BR /&gt;21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 235, base_baud = 5000000) is a IMX&lt;BR /&gt;imx sema4 driver is registered.&lt;BR /&gt;[drm] Initialized drm 1.1.0 20060810&lt;BR /&gt;[drm] Initialized vivante 1.0.0 20120216 on minor 0&lt;BR /&gt;brd: module loaded&lt;BR /&gt;loop: module loaded&lt;BR /&gt;fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff&lt;BR /&gt;fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed&lt;BR /&gt;20b4000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps0: new PPS source ptp0&lt;BR /&gt;fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00&lt;BR /&gt;fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 52:88:f6:cc:09:9c&lt;BR /&gt;libphy: fec_enet_mii_bus: probed&lt;BR /&gt;fec 20b4000.ethernet eth0: registered PHC device 0&lt;BR /&gt;2188000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps1: new PPS source ptp1&lt;BR /&gt;fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00&lt;BR /&gt;fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: c2:dd:f7:65:e0:db&lt;BR /&gt;fec 2188000.ethernet eth1: registered PHC device 1&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;ehci-mxc: Freescale On-Chip EHCI Host driver&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;2184800.usbmisc supply vbus-wakeup not found, using dummy regulator&lt;BR /&gt;2184000.usb supply vbus not found, using dummy regulator&lt;BR /&gt;2184200.usb supply vbus not found, using dummy regulator&lt;BR /&gt;ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;BR /&gt;ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1&lt;BR /&gt;ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 1 port detected&lt;BR /&gt;Mass Storage Function, version: 2009/09/11&lt;BR /&gt;LUN: removable file: (no medium)&lt;BR /&gt;LUN: removable read only file: /fat&lt;BR /&gt;Number of LUNs=1&lt;BR /&gt;Number of LUNs=1&lt;BR /&gt;g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11&lt;BR /&gt;g_mass_storage gadget: g_mass_storage ready&lt;BR /&gt;mousedev: PS/2 mouse device common for all mice&lt;BR /&gt;input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0&lt;BR /&gt;input: iMX6UL TouchScreen Controller as /devices/platform/soc/2000000.aips-bus/2040000.tsc/input/input1&lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;IR NEC protocol handler initialized&lt;BR /&gt;IR RC5(x/sz) protocol handler initialized&lt;BR /&gt;IR RC6 protocol handler initialized&lt;BR /&gt;IR JVC protocol handler initialized&lt;BR /&gt;IR Sony protocol handler initialized&lt;BR /&gt;IR SANYO protocol handler initialized&lt;BR /&gt;IR Sharp protocol handler initialized&lt;BR /&gt;IR MCE Keyboard/mouse protocol handler initialized&lt;BR /&gt;IR XMP protocol handler initialized&lt;BR /&gt;pxp-v4l2 pxp_v4l2: initialized&lt;BR /&gt;imx2-wdt 20bc000.wdog: use WDOG_B to reboot.&lt;BR /&gt;imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found&lt;BR /&gt;g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage&lt;BR /&gt;mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA&lt;BR /&gt;usbcore: registered new interface driver usbhid&lt;BR /&gt;usbhid: USB HID core driver&lt;BR /&gt;NET: Registered protocol family 10&lt;BR /&gt;sit: IPv6 over IPv4 tunneling driver&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;Key type dns_resolver registered&lt;BR /&gt;cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)&lt;BR /&gt;Registering SWP/SWPB emulation handler&lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)&lt;BR /&gt;can-3v3: disabling&lt;BR /&gt;clk: Not disabling unused clocks&lt;BR /&gt;ALSA device list:&lt;BR /&gt;No soundcards found.&lt;BR /&gt;Freeing unused kernel memory: 388K (8091f000 - 80980000)&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;BR /&gt;imx-uart 2020000.serial: Rx FIFO overrun&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 09:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Custom-Board-Booting-Issue/m-p/1321800#M178238</guid>
      <dc:creator>uttej_ravuri</dc:creator>
      <dc:date>2021-08-11T09:35:16Z</dc:date>
    </item>
  </channel>
</rss>