<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 MYS-6ULY2 bitbake: linux-imx do_copy_defconfig</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-copy-defconfig/m-p/1319984#M178043</link>
    <description>&lt;P&gt;After changes I've done like I wrote in &lt;A href="https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-fetch-error/m-p/1319981#M178042" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-fetch-error/m-p/1319981#M178042&lt;/A&gt;&amp;nbsp;some time later bitbaking failed with error&amp;nbsp;&lt;EM&gt;do_copy_defconfig, Task 67.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;ERROR: linux-imx-4.1.15-r0 do_copy_defconfig: Function failed: do_copy_defconfig (log file is located at /home/totalit/MYS6ULx-devel/fsl-release-yocto/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_copy_defconfig.2774)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/totalit/MYS6ULx-devel/fsl-release-yocto/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_copy_defconfig.2774&lt;BR /&gt;Log data follows:&lt;/P&gt;&lt;P&gt;| DEBUG: Executing shell function do_copy_defconfig&lt;BR /&gt;| cp: cannot stat '/home/totalit/MYS6ULx-devel/fsl-release-yocto/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.1.15-r0/git/arch/arm/configs/imx_v7_defconfig': No such file or directory&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_copy_defconfig (log file is located at /home/totalit/MYS6ULx-devel/fsl-release-yocto/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_copy_defconfig.2774)&lt;/P&gt;&lt;P&gt;ERROR: Task 67 (/home/totalit/MYS6ULx-devel/fsl-release-yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.1.15.bb, do_copy_defconfig) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 1300 tasks of which 1298 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 09 Aug 2021 10:54:58 GMT</pubDate>
    <dc:creator>totalit</dc:creator>
    <dc:date>2021-08-09T10:54:58Z</dc:date>
    <item>
      <title>MYS-6ULY2 bitbake: linux-imx do_copy_defconfig</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-copy-defconfig/m-p/1319984#M178043</link>
      <description>&lt;P&gt;After changes I've done like I wrote in &lt;A href="https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-fetch-error/m-p/1319981#M178042" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-fetch-error/m-p/1319981#M178042&lt;/A&gt;&amp;nbsp;some time later bitbaking failed with error&amp;nbsp;&lt;EM&gt;do_copy_defconfig, Task 67.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;ERROR: linux-imx-4.1.15-r0 do_copy_defconfig: Function failed: do_copy_defconfig (log file is located at /home/totalit/MYS6ULx-devel/fsl-release-yocto/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_copy_defconfig.2774)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/totalit/MYS6ULx-devel/fsl-release-yocto/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_copy_defconfig.2774&lt;BR /&gt;Log data follows:&lt;/P&gt;&lt;P&gt;| DEBUG: Executing shell function do_copy_defconfig&lt;BR /&gt;| cp: cannot stat '/home/totalit/MYS6ULx-devel/fsl-release-yocto/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.1.15-r0/git/arch/arm/configs/imx_v7_defconfig': No such file or directory&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_copy_defconfig (log file is located at /home/totalit/MYS6ULx-devel/fsl-release-yocto/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_copy_defconfig.2774)&lt;/P&gt;&lt;P&gt;ERROR: Task 67 (/home/totalit/MYS6ULx-devel/fsl-release-yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.1.15.bb, do_copy_defconfig) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 1300 tasks of which 1298 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Aug 2021 10:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-copy-defconfig/m-p/1319984#M178043</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-08-09T10:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: MYS-6ULY2 bitbake: linux-imx do_copy_defconfig</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-copy-defconfig/m-p/1324940#M178616</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188988"&gt;@totalit&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The issue is that you are taking the incorrect layer, you need the i.MX6UL and you take from yocto the imx6qsabresd, that is why you get that error.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 20:07:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-copy-defconfig/m-p/1324940#M178616</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-08-17T20:07:36Z</dc:date>
    </item>
  </channel>
</rss>