<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic rtl8188eus in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/rtl8188eus/m-p/1319936#M178039</link>
    <description>&lt;P&gt;&amp;nbsp; &amp;nbsp;lsusb can see rtl8188eus device,but when i us ifconfig -a ,i can't see wlan0. why?Attached files is the log? i don't know why ?I use a usb rtl8188eus wlan card&amp;nbsp; ,use the USB_OTG2 which is used as a host port ,then through GL850 ,then to USB type a port ,5v of the port is always on .anybody can help me&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 07 Aug 2021 11:34:22 GMT</pubDate>
    <dc:creator>hahhahha</dc:creator>
    <dc:date>2021-08-07T11:34:22Z</dc:date>
    <item>
      <title>rtl8188eus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/rtl8188eus/m-p/1319936#M178039</link>
      <description>&lt;P&gt;&amp;nbsp; &amp;nbsp;lsusb can see rtl8188eus device,but when i us ifconfig -a ,i can't see wlan0. why?Attached files is the log? i don't know why ?I use a usb rtl8188eus wlan card&amp;nbsp; ,use the USB_OTG2 which is used as a host port ,then through GL850 ,then to USB type a port ,5v of the port is always on .anybody can help me&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 07 Aug 2021 11:34:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/rtl8188eus/m-p/1319936#M178039</guid>
      <dc:creator>hahhahha</dc:creator>
      <dc:date>2021-08-07T11:34:22Z</dc:date>
    </item>
    <item>
      <title>Re: rtl8188eus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/rtl8188eus/m-p/1319989#M178045</link>
      <description>&lt;P&gt;Hi&amp;nbsp; Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;rtl8188eus is used in toradex boards:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.toradex.com/t/install-driver-rtl8188eu-for-usb-wifi-adapter-tl-wn725n/7591/4" target="_blank"&gt;https://community.toradex.com/t/install-driver-rtl8188eu-for-usb-wifi-adapter-tl-wn725n/7591/4&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.toradex.com/t/realtek-wifi-dongo-not-working-based-on-rtl8188-chipset/10238" target="_blank"&gt;https://community.toradex.com/t/realtek-wifi-dongo-not-working-based-on-rtl8188-chipset/10238&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 09 Aug 2021 00:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/rtl8188eus/m-p/1319989#M178045</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-09T00:34:56Z</dc:date>
    </item>
  </channel>
</rss>