<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8MP: Uboot and Linux Repo</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Uboot-and-Linux-Repo/m-p/1319570#M178005</link>
    <description>&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;1) Where can I find uboot files for i.MX 8M Plus EVK?&lt;/P&gt;&lt;P&gt;2) Is there any linux repo exists for this platform? If yes, where can I find the repo?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Saqib&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 06 Aug 2021 07:48:22 GMT</pubDate>
    <dc:creator>Saqib</dc:creator>
    <dc:date>2021-08-06T07:48:22Z</dc:date>
    <item>
      <title>IMX8MP: Uboot and Linux Repo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Uboot-and-Linux-Repo/m-p/1319570#M178005</link>
      <description>&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;1) Where can I find uboot files for i.MX 8M Plus EVK?&lt;/P&gt;&lt;P&gt;2) Is there any linux repo exists for this platform? If yes, where can I find the repo?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Saqib&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Aug 2021 07:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Uboot-and-Linux-Repo/m-p/1319570#M178005</guid>
      <dc:creator>Saqib</dc:creator>
      <dc:date>2021-08-06T07:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP: Uboot and Linux Repo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Uboot-and-Linux-Repo/m-p/1321467#M178182</link>
      <description>&lt;P&gt;1) you can download uboot standalone source code and build it, then get the uboot file under the&amp;nbsp; build folder&lt;/P&gt;
&lt;P&gt;we also release the uboot demo images for downloading, you can find it from the link as below:&lt;BR /&gt;"&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&amp;quot;" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX"&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2) board doesn't have repo, you can build it on ubuntu by yourself&lt;/P&gt;
&lt;P&gt;3.2 Setting up the repo utility&lt;BR /&gt;Repo is a tool built on top of Git that makes it easier to manage projects that contain multiple repositories, which do not need to be&lt;BR /&gt;on the same server. Repo complements very well the layered nature of the Yocto Project, making it easier for users to add their&lt;BR /&gt;own layers to the BSP.&lt;BR /&gt;To install the “repo” utility, perform these steps:&lt;BR /&gt;1. Create a bin folder in the home directory.&lt;BR /&gt;$ mkdir ~/bin (this step may not be needed if the bin folder already exists)&lt;BR /&gt;$ curl &lt;A href="https://storage.googleapis.com/git-repo-downloads/repo" target="_blank"&gt;https://storage.googleapis.com/git-repo-downloads/repo&lt;/A&gt; &amp;gt; ~/bin/repo&lt;BR /&gt;$ chmod a+x ~/bin/repo&lt;BR /&gt;2. Add the following line to the .bashrc file to ensure that the ~/bin folder is in your PATH variable.&lt;BR /&gt;export PATH=~/bin:$PATH&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 02:43:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Uboot-and-Linux-Repo/m-p/1321467#M178182</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-08-11T02:43:14Z</dc:date>
    </item>
  </channel>
</rss>