<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMYS-6ULY2 bitbake: linux-imx do_fetch error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-fetch-error/m-p/1319096#M177971</link>
    <description>&lt;P&gt;I do "bitbake core-image-base" for&amp;nbsp;MYS-6ULY2-256N2. It's going fine (~30%) until fetching from the source repository. The error screenshot is in attachments.The thing is, the address in vendor's files is no longer valid.&amp;nbsp;As I understand, I need to modify commit_id in&amp;nbsp;linux-imx_4.1.15.bb&amp;nbsp;according&amp;nbsp;to&amp;nbsp;source.codeaurora.org/external/imx/fsl-arm-yocto-bsp, since git.freescale is no longer relevant. What id do I need in this case:&amp;nbsp;&amp;nbsp;imx-4.1-krogoth,&amp;nbsp;&amp;nbsp;imx-4.1.15-1.0.0_ga&amp;nbsp;or something else?&lt;/P&gt;</description>
    <pubDate>Thu, 05 Aug 2021 13:48:24 GMT</pubDate>
    <dc:creator>totalit</dc:creator>
    <dc:date>2021-08-05T13:48:24Z</dc:date>
    <item>
      <title>MYS-6ULY2 bitbake: linux-imx do_fetch error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-fetch-error/m-p/1319096#M177971</link>
      <description>&lt;P&gt;I do "bitbake core-image-base" for&amp;nbsp;MYS-6ULY2-256N2. It's going fine (~30%) until fetching from the source repository. The error screenshot is in attachments.The thing is, the address in vendor's files is no longer valid.&amp;nbsp;As I understand, I need to modify commit_id in&amp;nbsp;linux-imx_4.1.15.bb&amp;nbsp;according&amp;nbsp;to&amp;nbsp;source.codeaurora.org/external/imx/fsl-arm-yocto-bsp, since git.freescale is no longer relevant. What id do I need in this case:&amp;nbsp;&amp;nbsp;imx-4.1-krogoth,&amp;nbsp;&amp;nbsp;imx-4.1.15-1.0.0_ga&amp;nbsp;or something else?&lt;/P&gt;</description>
      <pubDate>Thu, 05 Aug 2021 13:48:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-fetch-error/m-p/1319096#M177971</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-08-05T13:48:24Z</dc:date>
    </item>
    <item>
      <title>Re: MYS-6ULY2 bitbake: linux-imx do_fetch error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-fetch-error/m-p/1319981#M178042</link>
      <description>&lt;P&gt;So, I solved the case, modified a couple of strings in /MYS6ULx-devel/fsl-release-yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.1.15.bb according to a new repository:&lt;/P&gt;&lt;P&gt;SRCBRANCH = "imx-4.1.15-1.0.0_ga"&lt;BR /&gt;SRCREV = "d5a63e0034a40833531d2adbb58c230efaa3a89c"&lt;BR /&gt;KERNEL_SRC ?= "git://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp.git;protocol=git"&lt;/P&gt;&lt;P&gt;Also I removed patch URI, since it couldn't be installed (and shouldn't?). But then I have got another error. I'll create a new post.&lt;/P&gt;</description>
      <pubDate>Sun, 08 Aug 2021 21:08:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MYS-6ULY2-bitbake-linux-imx-do-fetch-error/m-p/1319981#M178042</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-08-08T21:08:02Z</dc:date>
    </item>
  </channel>
</rss>