<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8M Nano: Test GPU without MIPI-DSI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Nano-Test-GPU-without-MIPI-DSI/m-p/1317819#M177857</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I want to test GPU function in INX8M Nano customer board without any display device.&lt;/P&gt;&lt;P&gt;I try to use the /opt/imx-gpu-sdk/ and /opt/viv_samples/ tool to test GPU , but most of the tools cannot be executed and return the following log.&lt;/P&gt;&lt;P&gt;vdk_create_display(955): wl_display_connect failed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
    <pubDate>Wed, 04 Aug 2021 06:13:31 GMT</pubDate>
    <dc:creator>joshua_jhan</dc:creator>
    <dc:date>2021-08-04T06:13:31Z</dc:date>
    <item>
      <title>IMX8M Nano: Test GPU without MIPI-DSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Nano-Test-GPU-without-MIPI-DSI/m-p/1317819#M177857</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I want to test GPU function in INX8M Nano customer board without any display device.&lt;/P&gt;&lt;P&gt;I try to use the /opt/imx-gpu-sdk/ and /opt/viv_samples/ tool to test GPU , but most of the tools cannot be executed and return the following log.&lt;/P&gt;&lt;P&gt;vdk_create_display(955): wl_display_connect failed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 06:13:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Nano-Test-GPU-without-MIPI-DSI/m-p/1317819#M177857</guid>
      <dc:creator>joshua_jhan</dc:creator>
      <dc:date>2021-08-04T06:13:31Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Nano: Test GPU without MIPI-DSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Nano-Test-GPU-without-MIPI-DSI/m-p/1318075#M177879</link>
      <description>&lt;P&gt;Hi Joshua&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;seems lcd is always used, one can try to modify rm67191 driver, comment functions where driver&lt;/P&gt;
&lt;P&gt;expects answer from lcd&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mn-evk-rm67191.dts?h=lf-5.10.y" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mn-evk-rm67191.dts?h=lf-5.10.y&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/panel/panel-raydium-rm67191.c?h=lf-5.10.y" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/panel/panel-raydium-rm67191.c?h=lf-5.10.y&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 10:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Nano-Test-GPU-without-MIPI-DSI/m-p/1318075#M177879</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-04T10:55:28Z</dc:date>
    </item>
  </channel>
</rss>