<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 [i.MX8MP] How to generate xserver-xorg package for Yocto LF_v5.10_1.0.0 BSP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-How-to-generate-xserver-xorg-package-for-Yocto-LF-v5-10/m-p/1317748#M177854</link>
    <description>&lt;P&gt;When I use Yocto L5.4.3_2.0.0 BSP, it can generate the xserver-xorg package for i.MX8MP with the following command:&lt;/P&gt;&lt;P&gt;EULA=1 DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk source imx-setup-release.sh -b imx8mpevk_imx-image-full&lt;BR /&gt;bitbake imx-image-full&lt;/P&gt;&lt;P&gt;Build xserver-xorg directory:&lt;BR /&gt;../imx8mpevk_imx-image-full/tmp/work/aarch64-mx8mp-poky-linux/xserver-xorg&lt;/P&gt;&lt;P&gt;When I use Yocto LF_v5.10_1.0.0 BSP, it cannot build the xserver-xorg package with the above command.&lt;/P&gt;&lt;P&gt;Can you tell me how to use Yocto LF_v5.10_1.0.0 BSP to generate xserver-xorg package for i.MX8MP?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Wed, 04 Aug 2021 05:25:32 GMT</pubDate>
    <dc:creator>alex_cheng611</dc:creator>
    <dc:date>2021-08-04T05:25:32Z</dc:date>
    <item>
      <title>[i.MX8MP] How to generate xserver-xorg package for Yocto LF_v5.10_1.0.0 BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-How-to-generate-xserver-xorg-package-for-Yocto-LF-v5-10/m-p/1317748#M177854</link>
      <description>&lt;P&gt;When I use Yocto L5.4.3_2.0.0 BSP, it can generate the xserver-xorg package for i.MX8MP with the following command:&lt;/P&gt;&lt;P&gt;EULA=1 DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk source imx-setup-release.sh -b imx8mpevk_imx-image-full&lt;BR /&gt;bitbake imx-image-full&lt;/P&gt;&lt;P&gt;Build xserver-xorg directory:&lt;BR /&gt;../imx8mpevk_imx-image-full/tmp/work/aarch64-mx8mp-poky-linux/xserver-xorg&lt;/P&gt;&lt;P&gt;When I use Yocto LF_v5.10_1.0.0 BSP, it cannot build the xserver-xorg package with the above command.&lt;/P&gt;&lt;P&gt;Can you tell me how to use Yocto LF_v5.10_1.0.0 BSP to generate xserver-xorg package for i.MX8MP?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 05:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-How-to-generate-xserver-xorg-package-for-Yocto-LF-v5-10/m-p/1317748#M177854</guid>
      <dc:creator>alex_cheng611</dc:creator>
      <dc:date>2021-08-04T05:25:32Z</dc:date>
    </item>
  </channel>
</rss>