<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Bluetooth not functioning for linux 5.10.35 under imx8mminilpddr4evkb in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Bluetooth-not-functioning-for-linux-5-10-35-under/m-p/1317317#M177811</link>
    <description>&lt;P&gt;We are using the imx8mminilpddr4 evk board and have installed the linux 5.10.35 demo image.&lt;BR /&gt;The wifi module is enable and up by using the commands given in the Linux user guide Rev. (LF5.10.35_2.0.0, 30 June 2021). However the Bluetooh is not able to enable and having an error as below.&lt;/P&gt;&lt;P&gt;when the command "hciattach /dev/ttymxc1 any 3000000 flow" is given, it shows timeout and then EVM hangs;&lt;BR /&gt;the log is given below;&lt;BR /&gt;-----------------------------------------------------------------------------------------&lt;BR /&gt;root@imx8mm-lpddr4-evk:~# hciattach /dev/ttymxc1 any 3000000 flow&lt;BR /&gt;Setting TTY to N_HCI line discipline&lt;BR /&gt;[ 75.838884] Bluetooth: hci0: command 0x1003 tx timeout&lt;BR /&gt;[ 77.854872] Bluetooth: hci0: command 0x1001 tx timeout&lt;BR /&gt;[ 79.870884] Bluetooth: hci0: command 0x1009 tx timeout&lt;/P&gt;</description>
    <pubDate>Tue, 03 Aug 2021 11:32:18 GMT</pubDate>
    <dc:creator>sandeepcp</dc:creator>
    <dc:date>2021-08-03T11:32:18Z</dc:date>
    <item>
      <title>Bluetooth not functioning for linux 5.10.35 under imx8mminilpddr4evkb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bluetooth-not-functioning-for-linux-5-10-35-under/m-p/1317317#M177811</link>
      <description>&lt;P&gt;We are using the imx8mminilpddr4 evk board and have installed the linux 5.10.35 demo image.&lt;BR /&gt;The wifi module is enable and up by using the commands given in the Linux user guide Rev. (LF5.10.35_2.0.0, 30 June 2021). However the Bluetooh is not able to enable and having an error as below.&lt;/P&gt;&lt;P&gt;when the command "hciattach /dev/ttymxc1 any 3000000 flow" is given, it shows timeout and then EVM hangs;&lt;BR /&gt;the log is given below;&lt;BR /&gt;-----------------------------------------------------------------------------------------&lt;BR /&gt;root@imx8mm-lpddr4-evk:~# hciattach /dev/ttymxc1 any 3000000 flow&lt;BR /&gt;Setting TTY to N_HCI line discipline&lt;BR /&gt;[ 75.838884] Bluetooth: hci0: command 0x1003 tx timeout&lt;BR /&gt;[ 77.854872] Bluetooth: hci0: command 0x1001 tx timeout&lt;BR /&gt;[ 79.870884] Bluetooth: hci0: command 0x1009 tx timeout&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 11:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bluetooth-not-functioning-for-linux-5-10-35-under/m-p/1317317#M177811</guid>
      <dc:creator>sandeepcp</dc:creator>
      <dc:date>2021-08-03T11:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: Bluetooth not functioning for linux 5.10.35 under imx8mminilpddr4evkb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bluetooth-not-functioning-for-linux-5-10-35-under/m-p/1317581#M177837</link>
      <description>&lt;P&gt;Hi Sandeep&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for that board 88W8987 is used as described in Table 49. On-board chips and external solutions for Bluetooth and Wi-Fi support&lt;/P&gt;
&lt;P&gt;&lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_blank" rel="noopener"&gt;i.MX Linux Reference Manual​&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;One can try to follow &lt;A id="relatedDocsClick_2" href="https://www.nxp.com/docs/en/user-guide/UM11483.pdf" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Linux OS - User manual (public)&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 00:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bluetooth-not-functioning-for-linux-5-10-35-under/m-p/1317581#M177837</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-04T00:01:06Z</dc:date>
    </item>
  </channel>
</rss>