<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can't built boost-1.75, &amp;quot;not a valid ELF file&amp;quot; in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-built-boost-1-75-quot-not-a-valid-ELF-file-quot/m-p/1317109#M177782</link>
    <description>&lt;P&gt;I'm trying to `bitbake imx-image-full` for the imx8mpevk, but it is failing on boost 1.75. The full error is as follows:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;ERROR: boost-1.75.0-r0 do_package: dwarfsrcfiles failed with exit code 1 (cmd was ['dwarfsrcfiles', '/home/colin/imx-yocto-bsp/build-full2/tmp/work/cortexa53-crypto-poky-linux/boost/1.75.0-r0/package/usr/lib/libboost_log.a']):
dwarfsrcfiles: /home/colin/imx-yocto-bsp/build-full2/tmp/work/cortexa53-crypto-poky-linux/boost/1.75.0-r0/package/usr/lib/libboost_log.a: not a valid ELF file

ERROR: Logfile of failure stored in: /home/colin/imx-yocto-bsp/build-full2/tmp/work/cortexa53-crypto-poky-linux/boost/1.75.0-r0/temp/log.do_package.22126
ERROR: Task (/home/colin/imx-yocto-bsp/sources/poky/meta/recipes-support/boost/boost_1.75.0.bb:do_package) failed with exit code '1'&lt;/LI-CODE&gt;&lt;P&gt;Any tips? I'm quite new to this stuff. Thanks.&lt;/P&gt;</description>
    <pubDate>Tue, 03 Aug 2021 07:16:24 GMT</pubDate>
    <dc:creator>colinbroderick</dc:creator>
    <dc:date>2021-08-03T07:16:24Z</dc:date>
    <item>
      <title>Can't built boost-1.75, "not a valid ELF file"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-built-boost-1-75-quot-not-a-valid-ELF-file-quot/m-p/1317109#M177782</link>
      <description>&lt;P&gt;I'm trying to `bitbake imx-image-full` for the imx8mpevk, but it is failing on boost 1.75. The full error is as follows:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;ERROR: boost-1.75.0-r0 do_package: dwarfsrcfiles failed with exit code 1 (cmd was ['dwarfsrcfiles', '/home/colin/imx-yocto-bsp/build-full2/tmp/work/cortexa53-crypto-poky-linux/boost/1.75.0-r0/package/usr/lib/libboost_log.a']):
dwarfsrcfiles: /home/colin/imx-yocto-bsp/build-full2/tmp/work/cortexa53-crypto-poky-linux/boost/1.75.0-r0/package/usr/lib/libboost_log.a: not a valid ELF file

ERROR: Logfile of failure stored in: /home/colin/imx-yocto-bsp/build-full2/tmp/work/cortexa53-crypto-poky-linux/boost/1.75.0-r0/temp/log.do_package.22126
ERROR: Task (/home/colin/imx-yocto-bsp/sources/poky/meta/recipes-support/boost/boost_1.75.0.bb:do_package) failed with exit code '1'&lt;/LI-CODE&gt;&lt;P&gt;Any tips? I'm quite new to this stuff. Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 07:16:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-built-boost-1-75-quot-not-a-valid-ELF-file-quot/m-p/1317109#M177782</guid>
      <dc:creator>colinbroderick</dc:creator>
      <dc:date>2021-08-03T07:16:24Z</dc:date>
    </item>
    <item>
      <title>Re: Can't built boost-1.75, "not a valid ELF file"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-built-boost-1-75-quot-not-a-valid-ELF-file-quot/m-p/1317132#M177784</link>
      <description>&lt;P&gt;Problem solved. Fixed by doing a `bitbake -c cleanall boost`. Must have been bad files left over from a previous failed attempt.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 07:37:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-built-boost-1-75-quot-not-a-valid-ELF-file-quot/m-p/1317132#M177784</guid>
      <dc:creator>colinbroderick</dc:creator>
      <dc:date>2021-08-03T07:37:05Z</dc:date>
    </item>
  </channel>
</rss>