<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX7D internal ram memory map in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-internal-ram-memory-map/m-p/1316214#M177715</link>
    <description>&lt;P&gt;Hello Yuri!&lt;BR /&gt;&lt;BR /&gt;Do I understand correctly, that I can't use adresses 0x00900000-0x0090ffff for storing my Cortex-M4 firmware because this range is reserved by Linux kernel and is used by it during boot process?&lt;BR /&gt;&lt;BR /&gt;As I see from FreeRTOS linker scripts - they all use 0x00910000 as a start address. I tried to edit default linker script to use first 0x00900000 and then 0x00901000 adresses as a start address along with disabling corresponding ocram entries in the devicetree, but I see that my M4 firmware stops working right after kernel starts booting.&lt;BR /&gt;&lt;BR /&gt;I use imx-5.4.47 kernel&lt;BR /&gt;My modifications:&lt;BR /&gt;imx7d.dtsi:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="javascript"&gt;		ocram: sram@901000 {
			compatible = "mmio-sram";
			reg = &amp;lt;0x901000 0x1f000&amp;gt;;
			clocks = &amp;lt;&amp;amp;clks IMX7D_OCRAM_CLK&amp;gt;;
+           status = "disabled";
		};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;my devicetree:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="javascript"&gt;	reserved-memory {
		#address-cells = &amp;lt;1&amp;gt;;
		#size-cells = &amp;lt;1&amp;gt;;
		ranges;

		m4_reserved: m4@0x00901000 {
			no-map;
			reg = &amp;lt;0x00901000 0x1f000&amp;gt;;
		};
	};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;Did I miss something?&lt;BR /&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Sat, 31 Jul 2021 14:29:47 GMT</pubDate>
    <dc:creator>ivan_nikolaenko</dc:creator>
    <dc:date>2021-07-31T14:29:47Z</dc:date>
    <item>
      <title>iMX7D internal ram memory map</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-internal-ram-memory-map/m-p/846992#M129681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is a user problem reading + understanding manual:&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ocrammap.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62668i53EDEB04A08D44B1/image-size/large?v=v2&amp;amp;px=999" role="button" title="ocrammap.jpg" alt="ocrammap.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The figure says 224 is free&amp;nbsp; (&amp;nbsp; = 128(EPDC) + 64(128 - 64res) + 32(PXP) ), and "see note".&lt;/P&gt;&lt;P&gt;In note:&amp;nbsp; "The entire OCRAM region can be used freely post boot. ... "&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;So can the entire OCRAM 288KB be used freely post boot, or only 224?&amp;nbsp; &amp;nbsp;(I can't say why I can't understand the doc ... ).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;And if the 64KB is still reserved, what is it reserved for&amp;nbsp; .. (is it secret :smileyhappy:)&amp;nbsp;?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Aug 2018 03:20:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7D-internal-ram-memory-map/m-p/846992#M129681</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2018-08-13T03:20:54Z</dc:date>
    </item>
    <item>
      <title>Re: iMX7D internal ram memory map</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-internal-ram-memory-map/m-p/846993#M129682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;The entire OCRAM 288KB be used freely post boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct Answer &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Aug 2018 04:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7D-internal-ram-memory-map/m-p/846993#M129682</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-08-13T04:55:06Z</dc:date>
    </item>
    <item>
      <title>Re: iMX7D internal ram memory map</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-internal-ram-memory-map/m-p/846994#M129683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Yuri !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Aug 2018 08:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7D-internal-ram-memory-map/m-p/846994#M129683</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2018-08-13T08:07:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX7D internal ram memory map</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-internal-ram-memory-map/m-p/1316214#M177715</link>
      <description>&lt;P&gt;Hello Yuri!&lt;BR /&gt;&lt;BR /&gt;Do I understand correctly, that I can't use adresses 0x00900000-0x0090ffff for storing my Cortex-M4 firmware because this range is reserved by Linux kernel and is used by it during boot process?&lt;BR /&gt;&lt;BR /&gt;As I see from FreeRTOS linker scripts - they all use 0x00910000 as a start address. I tried to edit default linker script to use first 0x00900000 and then 0x00901000 adresses as a start address along with disabling corresponding ocram entries in the devicetree, but I see that my M4 firmware stops working right after kernel starts booting.&lt;BR /&gt;&lt;BR /&gt;I use imx-5.4.47 kernel&lt;BR /&gt;My modifications:&lt;BR /&gt;imx7d.dtsi:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="javascript"&gt;		ocram: sram@901000 {
			compatible = "mmio-sram";
			reg = &amp;lt;0x901000 0x1f000&amp;gt;;
			clocks = &amp;lt;&amp;amp;clks IMX7D_OCRAM_CLK&amp;gt;;
+           status = "disabled";
		};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;my devicetree:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="javascript"&gt;	reserved-memory {
		#address-cells = &amp;lt;1&amp;gt;;
		#size-cells = &amp;lt;1&amp;gt;;
		ranges;

		m4_reserved: m4@0x00901000 {
			no-map;
			reg = &amp;lt;0x00901000 0x1f000&amp;gt;;
		};
	};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;Did I miss something?&lt;BR /&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Sat, 31 Jul 2021 14:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7D-internal-ram-memory-map/m-p/1316214#M177715</guid>
      <dc:creator>ivan_nikolaenko</dc:creator>
      <dc:date>2021-07-31T14:29:47Z</dc:date>
    </item>
  </channel>
</rss>