<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Interfacing a parallel image sensor to i.mx 7ulp with FlexIO</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-a-parallel-image-sensor-to-i-mx-7ulp-with-FlexIO/m-p/1313913#M177526</link>
    <description>&lt;P&gt;Hello kunf,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The MX7ULP has MIPI for camera interface, if you want to interface flexio you have to develop the interface with gpio.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 27 Jul 2021 13:08:35 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2021-07-27T13:08:35Z</dc:date>
    <item>
      <title>Interfacing a parallel image sensor to i.mx 7ulp with FlexIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-a-parallel-image-sensor-to-i-mx-7ulp-with-FlexIO/m-p/1312702#M177408</link>
      <description>&lt;P&gt;Does any one have experience with Interfacing 8bit parallel Image sensor to i.mx 7ulp with FlexIO?&lt;/P&gt;&lt;P&gt;What is the maximum possible resolution with e.g. YUV422 or RGB888?&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jul 2021 17:41:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-a-parallel-image-sensor-to-i-mx-7ulp-with-FlexIO/m-p/1312702#M177408</guid>
      <dc:creator>kunf</dc:creator>
      <dc:date>2021-07-23T17:41:03Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing a parallel image sensor to i.mx 7ulp with FlexIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-a-parallel-image-sensor-to-i-mx-7ulp-with-FlexIO/m-p/1313913#M177526</link>
      <description>&lt;P&gt;Hello kunf,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The MX7ULP has MIPI for camera interface, if you want to interface flexio you have to develop the interface with gpio.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 13:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-a-parallel-image-sensor-to-i-mx-7ulp-with-FlexIO/m-p/1313913#M177526</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-07-27T13:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing a parallel image sensor to i.mx 7ulp with FlexIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-a-parallel-image-sensor-to-i-mx-7ulp-with-FlexIO/m-p/1313941#M177529</link>
      <description>&lt;P&gt;Thank you for your answer. according to the reference manual, the i.mx 7ulp (in contrast to the solo and dual variants) does not have a MIPI camera interface. The only camera interface available is the VIU, which has only very limited options for the maximum possible resolution. Therefore my question is whether a camera stream of higher quality can be achieved via the FlexIO module and GPIOs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 13:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-a-parallel-image-sensor-to-i-mx-7ulp-with-FlexIO/m-p/1313941#M177529</guid>
      <dc:creator>kunf</dc:creator>
      <dc:date>2021-07-27T13:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing a parallel image sensor to i.mx 7ulp with FlexIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-a-parallel-image-sensor-to-i-mx-7ulp-with-FlexIO/m-p/1314569#M177591</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The MX7ULP has MIPI DSI not for camera, for camera it has parallel IF/F. No you can not connect the camera with high resolution through FlexIO.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 13:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-a-parallel-image-sensor-to-i-mx-7ulp-with-FlexIO/m-p/1314569#M177591</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-07-28T13:10:18Z</dc:date>
    </item>
  </channel>
</rss>