<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic It can't use LAN function in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1313002#M177438</link>
    <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;We have a srg_imx8mplus platform (base imx8mplus). In this HW design, we have 2 LANs.&lt;BR /&gt;Now the functions of LAN1 and LAN2 are disabled. We check the hardware circuit is with&lt;BR /&gt;imx8mplus is the same. In Uboot mode, “Could not get PHY for FEC0:addr1” will appear.&lt;BR /&gt;I measure the MDC signal, MDC does not have a clock.&lt;/P&gt;&lt;P&gt;Can imx8mplus CPU provide clock to MDC?&lt;BR /&gt;How to modify the code?&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jul 2021 05:52:11 GMT</pubDate>
    <dc:creator>t2865k5</dc:creator>
    <dc:date>2021-07-26T05:52:11Z</dc:date>
    <item>
      <title>It can't use LAN function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1313002#M177438</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;We have a srg_imx8mplus platform (base imx8mplus). In this HW design, we have 2 LANs.&lt;BR /&gt;Now the functions of LAN1 and LAN2 are disabled. We check the hardware circuit is with&lt;BR /&gt;imx8mplus is the same. In Uboot mode, “Could not get PHY for FEC0:addr1” will appear.&lt;BR /&gt;I measure the MDC signal, MDC does not have a clock.&lt;/P&gt;&lt;P&gt;Can imx8mplus CPU provide clock to MDC?&lt;BR /&gt;How to modify the code?&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 05:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1313002#M177438</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-26T05:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: It can't use LAN function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1313027#M177441</link>
      <description>&lt;P&gt;Dear NXP ,&lt;/P&gt;&lt;P&gt;Code base:&lt;/P&gt;&lt;P&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0.xml&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 06:33:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1313027#M177441</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-26T06:33:42Z</dc:date>
    </item>
    <item>
      <title>Re: It can't use LAN function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1313487#M177489</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184266"&gt;@t2865k5&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Default bsp can provide MDC clock.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 01:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1313487#M177489</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-07-27T01:56:47Z</dc:date>
    </item>
    <item>
      <title>Re: It can't use LAN function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314161#M177546</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;Please call me how to set CPU clock to MDC.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 01:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314161#M177546</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-28T01:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: It can't use LAN function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314284#M177560</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;The hardware engineer modified the hardware, LAN1 does not have a clock, and LAN2 has a clock. So LAN2 can work normally, but LAN1 can't work normally.&lt;/P&gt;&lt;P&gt;Does the default BSP code provide a setting of clocks to LAN1 and LAN2 MDC at the same time? Or provide two setting of clocks to MDC1/MDC2 separately?&lt;/P&gt;&lt;P&gt;Please tell me how to modify the code?&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 05:47:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314284#M177560</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-28T05:47:42Z</dc:date>
    </item>
    <item>
      <title>Re: It can't use LAN function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314291#M177563</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Does the default BSP code provide a setting of clocks to LAN1 and LAN2 MDC at the same time? Or provide two setting of clocks to MDC1/MDC2 separately?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;---&amp;gt;yes,default BSP code provide two&amp;nbsp; MDC, they are two different pad.&lt;/SPAN&gt;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;pinctrl_eqos: eqosgrp {
		fsl,pins = &amp;lt;
			MX8MP_IOMUXC_ENET_MDC__ENET_QOS_MDC	0x3
			MX8MP_IOMUXC_ENET_MDIO__ENET_QOS_MDIO	0x3
			MX8MP_IOMUXC_ENET_RD0__ENET_QOS_RGMII_RD0	0x91
			MX8MP_IOMUXC_ENET_RD1__ENET_QOS_RGMII_RD1	0x91
			MX8MP_IOMUXC_ENET_RD2__ENET_QOS_RGMII_RD2	0x91
			MX8MP_IOMUXC_ENET_RD3__ENET_QOS_RGMII_RD3	0x91
			MX8MP_IOMUXC_ENET_RXC__CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK	0x91
			MX8MP_IOMUXC_ENET_RX_CTL__ENET_QOS_RGMII_RX_CTL	0x91
			MX8MP_IOMUXC_ENET_TD0__ENET_QOS_RGMII_TD0		0x1f
			MX8MP_IOMUXC_ENET_TD1__ENET_QOS_RGMII_TD1		0x1f
			MX8MP_IOMUXC_ENET_TD2__ENET_QOS_RGMII_TD2		0x1f
			MX8MP_IOMUXC_ENET_TD3__ENET_QOS_RGMII_TD3		0x1f
			MX8MP_IOMUXC_ENET_TX_CTL__ENET_QOS_RGMII_TX_CTL	0x1f
			MX8MP_IOMUXC_ENET_TXC__CCM_ENET_QOS_CLOCK_GENERATE_TX_CLK	0x1f
			MX8MP_IOMUXC_SAI2_RXC__GPIO4_IO22		0x19
		&amp;gt;;
	};

	pinctrl_fec: fecgrp {
		fsl,pins = &amp;lt;
			MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC		0x3
			MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO		0x3
			MX8MP_IOMUXC_SAI1_RXD4__ENET1_RGMII_RD0		0x91
			MX8MP_IOMUXC_SAI1_RXD5__ENET1_RGMII_RD1		0x91
			MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2		0x91
			MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3		0x91
			MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC		0x91
			MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL	0x91
			MX8MP_IOMUXC_SAI1_TXD0__ENET1_RGMII_TD0		0x1f
			MX8MP_IOMUXC_SAI1_TXD1__ENET1_RGMII_TD1		0x1f
			MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2		0x1f
			MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3		0x1f
			MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL	0x1f
			MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC		0x1f
			MX8MP_IOMUXC_SAI1_RXD0__GPIO4_IO02		0x19
		&amp;gt;;
	};&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 05:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314291#M177563</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-07-28T05:57:23Z</dc:date>
    </item>
    <item>
      <title>Re: It can't use LAN function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314311#M177568</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;(1) I check the&amp;nbsp;u-boot_imx8mp-evk.dts (arch/arm/dts/imx8mp-evk.dts) and&amp;nbsp;kernel-imx8mp-evk.dts (arch/arm64/boot/dts/freescale/imx8mp-evk.dts).&lt;/P&gt;&lt;P&gt;Their settings are the same as yours. Please help me to check them again if the settings of my two files are correct.&lt;/P&gt;&lt;P&gt;(2)&amp;nbsp;&lt;/P&gt;&lt;P&gt;MX8MP_IOMUXC_ENET_MDC__ENET_QOS_MDC 0x3&lt;BR /&gt;MX8MP_IOMUXC_ENET_MDIO__ENET_QOS_MDIO 0x3&lt;/P&gt;&lt;P&gt;MX8MP_IOMUXC_ENET_RXC__CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK 0x91&lt;/P&gt;&lt;P&gt;Should these be LAN MDC clock settings?&lt;BR /&gt;Are there relevant documents that explain the meaning of these values?&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 06:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314311#M177568</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-28T06:50:54Z</dc:date>
    </item>
    <item>
      <title>Re: It can't use LAN function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314315#M177569</link>
      <description>&lt;P&gt;Their are gpio setting value in i.MX8MP datasheet, i think you should check your hardware again because the evk can use two eth at the same time. It means the two rtl8211 chip is working at the same time.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 06:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/It-can-t-use-LAN-function/m-p/1314315#M177569</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-07-28T06:57:06Z</dc:date>
    </item>
  </channel>
</rss>