<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: The system cannot recognize the USB  flash drive in imx8mplus platform. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1312971#M177436</link>
    <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;You can refer the&amp;nbsp;USB_HUB_circuit.jpg and USB2.jpg&lt;/P&gt;</description>
    <pubDate>Mon, 26 Jul 2021 03:56:17 GMT</pubDate>
    <dc:creator>t2865k5</dc:creator>
    <dc:date>2021-07-26T03:56:17Z</dc:date>
    <item>
      <title>The system cannot recognize the USB  flash drive in imx8mplus platform.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1312845#M177420</link>
      <description>&lt;P&gt;The system cannot recognize the USB flash drive in imx8mplus platform&lt;/P&gt;&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;GL3523 is a USB HUB IC&lt;BR /&gt;We have done some experiments:&lt;/P&gt;&lt;P&gt;(1) Use a USB flash drive to plug in 4 USB PORTs. Both USB 2.0 ports can be recognized by the system. The 2 USB 3.0 ports can't&amp;nbsp; be recognized by the system.&lt;BR /&gt;(2) As shown in the figure, jumper the GL3523 IC USB3.0 pin to the USB cable, and plug in the USB cable to the computer's USB 2.0 slot, so that GL3523 can receive the computer's USB signal.&lt;BR /&gt;(3) Plug in the USB flash drive to the srg_imx8mplus USB 3.0 slot, the system can recognize the USB flash drive.&lt;/P&gt;&lt;P&gt;I think imx8mplus does not provide USB 3.0 signal to&lt;BR /&gt;GL3523. So the flash drive in the USB 3.0 slot cannot be recognized.&lt;/P&gt;&lt;P&gt;Can you tell me how to modify the USB code?&lt;/P&gt;</description>
      <pubDate>Sun, 25 Jul 2021 08:41:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1312845#M177420</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-25T08:41:52Z</dc:date>
    </item>
    <item>
      <title>Re: The system cannot recognize the USB  flash drive in imx8mplus platform.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1312941#M177429</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;You can refer the&amp;nbsp;USB_HUB_circuit.jpg .&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 03:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1312941#M177429</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-26T03:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: The system cannot recognize the USB  flash drive in imx8mplus platform.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1312968#M177434</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;Supplementary explanation, 4 USB ports (2 USB 2.0, 2 USB 3.0)&lt;BR /&gt;They are Type A USB. There is no Type C USB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 03:48:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1312968#M177434</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-26T03:48:59Z</dc:date>
    </item>
    <item>
      <title>Re: The system cannot recognize the USB  flash drive in imx8mplus platform.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1312971#M177436</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;You can refer the&amp;nbsp;USB_HUB_circuit.jpg and USB2.jpg&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 03:56:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1312971#M177436</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-26T03:56:17Z</dc:date>
    </item>
    <item>
      <title>Re: The system cannot recognize the USB  flash drive in imx8mplus platform.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1313029#M177442</link>
      <description>&lt;P&gt;Dear NXP ,&lt;/P&gt;&lt;P&gt;Code base:&lt;/P&gt;&lt;P&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0.xml&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 06:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1313029#M177442</guid>
      <dc:creator>t2865k5</dc:creator>
      <dc:date>2021-07-26T06:34:12Z</dc:date>
    </item>
    <item>
      <title>Re: The system cannot recognize the USB  flash drive in imx8mplus platform.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1364098#M182347</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If this is still prove helpful, it will be difficult to provide much without logs, even so I think you may refer to the USB3 sour code, for the code structure you may refer to the i.MX Reference Manual chapter 4.10 USB3&lt;BR /&gt;&lt;BR /&gt;Also, it may be useful to try using the Unit test to check the USB functionality, you'll find more information in the same document i.MX Reference Manual chapter 10.3.7 USB&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Sat, 30 Oct 2021 01:11:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-system-cannot-recognize-the-USB-flash-drive-in-imx8mplus/m-p/1364098#M182347</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-10-30T01:11:29Z</dc:date>
    </item>
  </channel>
</rss>