<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Which-RPA-version-to-use-for-i-MX-8QXP-C0-rev-using-SCFW-version/m-p/1311757#M177325</link>
    <description>&lt;P&gt;yes for i.MX8QXP LPDDR4 it is v.16.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 22 Jul 2021 06:06:07 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2021-07-22T06:06:07Z</dc:date>
    <item>
      <title>Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-RPA-version-to-use-for-i-MX-8QXP-C0-rev-using-SCFW-version/m-p/1311255#M177271</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am worrking on a custom hardware having i.mx8qxp-&lt;STRONG&gt;c0&lt;/STRONG&gt; revision cpu.&lt;BR /&gt;&lt;BR /&gt;I am using LF5.10.35_2.0.0 from &lt;A href="https://www.nxp.com/docs/en/release-note/IMX_LINUX_RELEASE_NOTES.pdf" target="_self"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;As per this guide i have downloaded scfw-kit-1.9.0.&lt;/P&gt;&lt;P&gt;I have used MT53D1024M32D4DT-053 AAT:D LPDDR4 micro.&lt;/P&gt;&lt;P&gt;I have been through the &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519" target="_self"&gt;link&lt;/A&gt; provided.&lt;BR /&gt;&lt;BR /&gt;My query is which RPA tool will be aligned with scfw-kit-1.9.0. and LF5.10.35_2.0.0 ?&lt;BR /&gt;&lt;BR /&gt;Also I am not able to find LPDDR's parameters(Density per channel , total DRAM density, total number of CS used etc.) or datasheet from micron technology, so how do i proceed ?&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;Thanks&lt;BR /&gt;Rutvij&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jul 2021 12:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-RPA-version-to-use-for-i-MX-8QXP-C0-rev-using-SCFW-version/m-p/1311255#M177271</guid>
      <dc:creator>r_trivedi123</dc:creator>
      <dc:date>2021-07-21T12:56:47Z</dc:date>
    </item>
    <item>
      <title>Re: Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-RPA-version-to-use-for-i-MX-8QXP-C0-rev-using-SCFW-version/m-p/1311608#M177305</link>
      <description>&lt;P&gt;Hi Rutvij&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can use latest version from link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming-Aid-RPA/ta-p/1166302" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming-Aid-RPA/ta-p/1166302&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jul 2021 00:01:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-RPA-version-to-use-for-i-MX-8QXP-C0-rev-using-SCFW-version/m-p/1311608#M177305</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-07-22T00:01:54Z</dc:date>
    </item>
    <item>
      <title>Re: Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-RPA-version-to-use-for-i-MX-8QXP-C0-rev-using-SCFW-version/m-p/1311721#M177316</link>
      <description>&lt;P&gt;Hi Igor,&lt;BR /&gt;Thanks for the quick replay.&lt;BR /&gt;&lt;BR /&gt;The suggested link has versions 15,16,21 available(image attached), will version 16 be good to go with?&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;Thanks&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jul 2021 05:12:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-RPA-version-to-use-for-i-MX-8QXP-C0-rev-using-SCFW-version/m-p/1311721#M177316</guid>
      <dc:creator>r_trivedi123</dc:creator>
      <dc:date>2021-07-22T05:12:16Z</dc:date>
    </item>
    <item>
      <title>Re: Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-RPA-version-to-use-for-i-MX-8QXP-C0-rev-using-SCFW-version/m-p/1311757#M177325</link>
      <description>&lt;P&gt;yes for i.MX8QXP LPDDR4 it is v.16.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jul 2021 06:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-RPA-version-to-use-for-i-MX-8QXP-C0-rev-using-SCFW-version/m-p/1311757#M177325</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-07-22T06:06:07Z</dc:date>
    </item>
  </channel>
</rss>