<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKernel getting stuck</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-getting-stuck/m-p/1310279#M177179</link>
    <description>&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;We are using the Zeus Yocto version and we switched the uboot version from 2019 to 2020 and after that Kernel getting stuck with the following errors.&lt;/P&gt;&lt;P&gt;What can we do to resolve this issue?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;Warning: ethernet@30be0000 (eth0) using random MAC address - 26:af:ec:a9:a5:9e&lt;BR /&gt;eth0: ethernet@30be0000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;5746340 bytes read in 77 ms (71.2 MiB/s)&lt;BR /&gt;Uncompressed size: 13113352 = 0xC81808&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;fdt_file=imx8mm-var-dart.dtb&lt;BR /&gt;43335 bytes read in 17 ms (2.4 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt;Booting using the fdt blob at 0x43000000&lt;BR /&gt;Using Device Tree in place at 0000000043000000, end 000000004300d946&lt;BR /&gt;&lt;BR /&gt;Starting kernel ...&lt;BR /&gt;&lt;BR /&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]&lt;BR /&gt;[ 0.000000] Linux version 5.4.3-imx8mm+gb40ccfdb73ea (oe-user@oe-host) (gcc 1&lt;BR /&gt;[ 0.000000] Machine model: Variscite DART-MX8MM&lt;BR /&gt;[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000078000000, B&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id sharl&lt;BR /&gt;[ 0.000000] NUMA: No NUMA configuration found&lt;BR /&gt;[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bffffff]&lt;BR /&gt;[ 0.000000] NUMA: NODE_DATA [mem 0xbfbc9800-0xbfbcafff]&lt;BR /&gt;[ 0.000000] Zone ranges:&lt;BR /&gt;[ 0.000000] DMA32 [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] Normal empty&lt;BR /&gt;[ 0.000000] Movable zone start for each node&lt;BR /&gt;[ 0.000000] Early memory node ranges&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] psci: probing for conduit method from DT.&lt;BR /&gt;[ 0.000000] psci: PSCIv1.1 detected in firmware.&lt;BR /&gt;[ 0.000000] psci: Using standard PSCI v0.2 function IDs&lt;BR /&gt;[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.&lt;BR /&gt;[ 0.000000] psci: SMC Calling Convention v1.1&lt;BR /&gt;[ 0.000000] percpu: Embedded 21 pages/cpu s48664 r8192 d29160 u86016&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;BR /&gt;[ 0.000000] CPU features: detected: ARM erratum 845719&lt;BR /&gt;[ 0.000000] CPU features: detected: GIC system register CPU interface&lt;BR /&gt;[ 0.000000] Speculative Store Bypass Disable mitigation not required&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096&lt;BR /&gt;[ 0.000000] Policy zone: DMA32&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p1 M&lt;BR /&gt;[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)&lt;BR /&gt;[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes,)&lt;BR /&gt;[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off&lt;BR /&gt;[ 0.000000] Memory: 1388060K/2097152K available (7934K kernel code, 582K rwd)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;[ 0.000000] rcu: Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.&lt;BR /&gt;[ 0.000000] Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 ji.&lt;BR /&gt;[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4&lt;BR /&gt;[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0&lt;BR /&gt;[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode&lt;BR /&gt;[ 0.000000] GICv3: 128 SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: 0 Extended SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: Distributor has no Range Selector support&lt;BR /&gt;[ 0.000000] GICv3: 16 PPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: no VLPI support, no direct LPI support&lt;BR /&gt;[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000&lt;BR /&gt;[ 0.000000] ITS: No ITS available, not enabling LPIs&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0x2b4/0x434 wi0&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycless&lt;BR /&gt;[ 0.000003] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199s&lt;BR /&gt;[ 0.000313] Console: colour dummy device 80x25&lt;BR /&gt;[ 0.000369] Calibrating delay loop (skipped), value calculated using timer f)&lt;BR /&gt;[ 0.000380] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.000471] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, lin)&lt;BR /&gt;[ 0.000482] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;[ 0.024004] ASID allocator initialised with 32768 entries&lt;BR /&gt;[ 0.032002] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.052041] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 0.084163] Detected VIPT I-cache on CPU1&lt;BR /&gt;[ 0.084187] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000&lt;BR /&gt;[ 0.084216] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]&lt;BR /&gt;[ 0.116195] Detected VIPT I-cache on CPU2&lt;BR /&gt;[ 0.116211] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000&lt;BR /&gt;[ 0.116229] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]&lt;BR /&gt;[ 0.148243] Detected VIPT I-cache on CPU3&lt;BR /&gt;[ 0.148257] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000&lt;BR /&gt;[ 0.148273] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]&lt;BR /&gt;[ 0.148329] smp: Brought up 1 node, 4 CPUs&lt;BR /&gt;[ 0.148351] SMP: Total of 4 processors activated.&lt;BR /&gt;[ 0.148356] CPU features: detected: 32-bit EL0 Support&lt;BR /&gt;[ 0.148363] CPU features: detected: CRC32 instructions&lt;BR /&gt;[ 0.152336] CPU: All CPU(s) started at EL2&lt;BR /&gt;[ 0.152353] alternatives: patching kernel code&lt;BR /&gt;[ 0.153407] devtmpfs: initialized&lt;BR /&gt;[ 0.158918] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ms&lt;BR /&gt;[ 0.158934] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)&lt;BR /&gt;[ 0.173282] pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;[ 0.174033] NET: Registered protocol family 16&lt;BR /&gt;[ 0.177136] DMA: preallocated 256 KiB pool for atomic allocations&lt;BR /&gt;[ 0.177562] cpuidle: using governor menu&lt;BR /&gt;[ 0.177734] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.&lt;BR /&gt;[ 0.177946] imx mu driver is registered.&lt;BR /&gt;[ 0.177966] imx rpmsg driver is registered.&lt;BR /&gt;[ 0.182134] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.194148] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.194157] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.194162] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.194168] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.198691] iommu: Default domain type: Translated&lt;BR /&gt;[ 0.198792] vgaarb: loaded&lt;BR /&gt;[ 0.199819] mc: Linux media interface: v0.10&lt;BR /&gt;[ 0.199849] videodev: Linux video capture interface: v2.00&lt;BR /&gt;[ 0.199886] pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;[ 0.199891] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giom&amp;gt;&lt;BR /&gt;[ 0.199905] PTP clock support registered&lt;BR /&gt;[ 0.201150] clocksource: Switched to clocksource arch_sys_counter&lt;BR /&gt;[ 0.206391] thermal_sys: Registered thermal governor 'step_wise'&lt;BR /&gt;[ 0.206395] thermal_sys: Registered thermal governor 'power_allocator'&lt;BR /&gt;[ 0.206697] NET: Registered protocol family 2&lt;BR /&gt;[ 0.207067] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 163)&lt;BR /&gt;[ 0.207097] TCP established hash table entries: 16384 (order: 5, 131072 byte)&lt;BR /&gt;[ 0.207205] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, line)&lt;BR /&gt;[ 0.207433] TCP: Hash tables configured (established 16384 bind 16384)&lt;BR /&gt;[ 0.207510] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.207552] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.207673] NET: Registered protocol family 1&lt;BR /&gt;[ 0.208042] RPC: Registered named UNIX socket transport module.&lt;BR /&gt;[ 0.208048] RPC: Registered udp transport module.&lt;BR /&gt;[ 0.208054] RPC: Registered tcp transport module.&lt;BR /&gt;[ 0.208057] RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;[ 0.208068] PCI: CLS 0 bytes, default 64&lt;BR /&gt;[ 0.208594] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters ae&lt;BR /&gt;[ 0.209680] Initialise system trusted keyrings&lt;BR /&gt;[ 0.209801] workingset: timestamp_bits=44 max_order=19 bucket_order=0&lt;BR /&gt;[ 0.214191] NFS: Registering the id_resolver key type&lt;BR /&gt;[ 0.214215] Key type id_resolver registered&lt;BR /&gt;[ 0.214221] Key type id_legacy registered&lt;BR /&gt;[ 0.214231] nfs4filelayout_init: NFSv4 File Layout Driver Registering...&lt;BR /&gt;[ 0.214498] Key type asymmetric registered&lt;BR /&gt;[ 0.214503] Asymmetric key parser 'x509' registered&lt;BR /&gt;[ 0.214527] Block layer SCSI generic (bsg) driver version 0.4 loaded (major )&lt;BR /&gt;[ 0.214627] io scheduler mq-deadline registered&lt;BR /&gt;[ 0.214632] io scheduler kyber registered&lt;BR /&gt;[ 0.215736] pwm-backlight backlight: backlight supply power not found, usingr&lt;BR /&gt;[ 0.220486] mxs-dma 33000000.dma-controller: initialized&lt;BR /&gt;[ 0.221008] Bus freq driver module loaded&lt;BR /&gt;[ 0.223134] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled&lt;BR /&gt;[ 0.224745] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 30, base_baudX&lt;BR /&gt;[ 0.982507] printk: console [ttymxc0] enabled&lt;BR /&gt;[ 0.987277] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 31, base_baudX&lt;BR /&gt;[ 0.996447] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 32, base_baudX&lt;BR /&gt;[ 1.005670] 30a60000.serial: ttymxc3 at MMIO 0x30a60000 (irq = 38, base_baudX&lt;BR /&gt;[ 1.016859] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).&lt;BR /&gt;[ 1.023509] [drm] No driver support for vblank timestamp query.&lt;BR /&gt;[ 1.029514] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-cr)&lt;BR /&gt;[ 1.038916] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200&lt;BR /&gt;[ 1.046136] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32ei&lt;BR /&gt;[ 1.054470] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim brid7&lt;BR /&gt;[ 1.062254] imx-drm soc@0:bus@32c00000:display-subsystem: failed to bind 32e7&lt;BR /&gt;[ 1.073118] imx-drm soc@0:bus@32c00000:display-subsystem: master bind failed7&lt;BR /&gt;[ 1.082172] libphy: Fixed MDIO Bus: probed&lt;BR /&gt;[ 1.086589] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/so0&lt;BR /&gt;[ 1.100493] i2c /dev entries driver&lt;BR /&gt;[ 1.104185] mx6s-csi 32e20000.csi1_bridge: initialising&lt;BR /&gt;[ 1.109869] mxc_mipi-csi 32e30000.mipi_csi: 32e30000.mipi_csi supply mipi-phr&lt;BR /&gt;[ 1.120034] mxc_mipi-csi 32e30000.mipi_csi: mipi csi v4l2 device registered&lt;BR /&gt;[ 1.127008] CSI: Registered sensor subdevice: mxc_mipi-csi.0&lt;BR /&gt;[ 1.132689] mxc_mipi-csi 32e30000.mipi_csi: lanes: 2, hs_settle: 13, clk_set0&lt;BR /&gt;[ 1.145689] imx2-wdt 30280000.watchdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;[ 1.152840] sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;[ 1.159032] sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;[ 1.163393] sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;[ 1.169628] mmc0: CQHCI version 5.10&lt;BR /&gt;[ 1.204928] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA&lt;BR /&gt;[ 1.212404] mmc1: CQHCI version 5.10&lt;BR /&gt;[ 1.216494] mmc2: CQHCI version 5.10&lt;BR /&gt;[ 1.253416] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA&lt;BR /&gt;[ 1.262302] ledtrig-cpu: registered to indicate activity on CPUs&lt;BR /&gt;[ 1.269213] caam 30900000.crypto: device ID = 0x0a16040100000000 (Era 9)&lt;BR /&gt;[ 1.275969] caam 30900000.crypto: job rings = 3, qi = 0&lt;BR /&gt;[ 1.292822] caam algorithms registered in /proc/crypto&lt;BR /&gt;[ 1.299553] caam 30900000.crypto: caam pkc algorithms registered in /proc/cro&lt;BR /&gt;[ 1.309105] caam_jr 30901000.jr0: registering rng-caam&lt;BR /&gt;[ 1.316744] caam-snvs 30370000.caam-snvs: can't get snvs clock&lt;BR /&gt;[ 1.322769] caam-snvs 30370000.caam-snvs: violation handlers armed - non-sece&lt;BR /&gt;[ 1.331092] hidraw: raw HID events driver (C) Jiri Kosina&lt;BR /&gt;[ 1.339734] NET: Registered protocol family 17&lt;BR /&gt;[ 1.344273] 8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;[ 1.348507] Key type dns_resolver registered&lt;BR /&gt;[ 1.353301] Loading compiled-in X.509 certificates&lt;BR /&gt;[ 1.375401] regulator-eth-phy GPIO handle specifies active low - ignored&lt;BR /&gt;[ 1.382646] gpio-142 (scl): enforced open drain please flag it properly in De&lt;BR /&gt;[ 1.392626] rohm-bd718x7 0-004b: Failed to set masks in 0x2a: -6&lt;BR /&gt;[ 1.398659] rohm-bd718x7 0-004b: Failed to add irq_chip&lt;BR /&gt;[ 1.404091] i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;[ 1.409176] gpio-144 (scl): enforced open drain please flag it properly in De&lt;BR /&gt;[ 1.419161] mmc2: Command Queue Engine enabled&lt;BR /&gt;[ 1.423626] mmc2: new HS400 MMC card at address 0001&lt;BR /&gt;[ 1.429366] mmcblk2: mmc2:0001 S0J56X 14.8 GiB&lt;BR /&gt;[ 1.434038] mmcblk2boot0: mmc2:0001 S0J56X partition 1 31.5 MiB&lt;BR /&gt;[ 1.440085] mmcblk2boot1: mmc2:0001 S0J56X partition 2 31.5 MiB&lt;BR /&gt;[ 1.446725] mmcblk2rpmb: mmc2:0001 S0J56X partition 3 4.00 MiB, chardev (244)&lt;BR /&gt;[ 1.458683] mmcblk2: p1&lt;BR /&gt;[ 1.757739] i2c i2c-1: SCL is stuck low, exit recovery&lt;BR /&gt;[ 1.763057] edt_ft5x06 1-0038: touchscreen probe failed&lt;BR /&gt;[ 1.768418] edt_ft5x06: probe of 1-0038 failed with error -11&lt;BR /&gt;[ 1.774496] ov5640_mipi 1-003c: 1-003c supply DOVDD not found, using dummy rr&lt;BR /&gt;[ 1.782299] ov5640_mipi 1-003c: 1-003c supply DVDD not found, using dummy rer&lt;BR /&gt;[ 1.789992] ov5640_mipi 1-003c: 1-003c supply AVDD not found, using dummy rer&lt;BR /&gt;[ 1.869702] i2c i2c-1: SCL is stuck low, exit recovery&lt;BR /&gt;[ 1.875019] ov5640_mipi 1-003c: Read reg error: reg=300a&lt;BR /&gt;[ 1.880339] ov5640_mipi 1-003c: Camera is not found&lt;BR /&gt;[ 1.885342] i2c i2c-1: IMX I2C adapter registered&lt;BR /&gt;[ 1.890413] gpio-146 (scl): enforced open drain please flag it properly in De&lt;BR /&gt;[ 1.899966] i2c i2c-2: IMX I2C adapter registered&lt;BR /&gt;[ 1.904989] gpio-148 (scl): enforced open drain please flag it properly in De&lt;BR /&gt;[ 1.914784] i2c i2c-3: IMX I2C adapter registered&lt;BR /&gt;[ 1.919849] pwm-backlight backlight: backlight supply power not found, usingr&lt;BR /&gt;[ 1.928762] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).&lt;BR /&gt;[ 1.935384] [drm] No driver support for vblank timestamp query.&lt;BR /&gt;[ 1.941358] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-cr)&lt;BR /&gt;[ 1.950734] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200&lt;BR /&gt;[ 1.957963] panel-sitronix-st7703 32e10000.mipi_dsi.0: 32e10000.mipi_dsi.0 sr&lt;BR /&gt;[ 1.968704] panel-sitronix-st7703 32e10000.mipi_dsi.0: 32e10000.mipi_dsi.0 sr&lt;BR /&gt;[ 1.979608] panel-sitronix-st7703 32e10000.mipi_dsi.0: 640x1280@60 24bpp dsiy&lt;BR /&gt;[ 1.987754] imx-drm soc@0:bus@32c00000:display-subsystem: bound 32e10000.mip)&lt;BR /&gt;[ 1.998139] [drm] Initialized imx-drm 1.0.0 20120507 for soc@0:bus@32c00000:0&lt;BR /&gt;[ 3.170883] Console: switching to colour frame buffer device 80x80&lt;BR /&gt;[ 3.195221] imx-drm soc@0:bus@32c00000:display-subsystem: fb0: imx-drmdrmfb e&lt;BR /&gt;[ 3.204167] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 2 mkt segment 2 s4&lt;BR /&gt;[ 3.213280] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 500000 z&lt;BR /&gt;[ 3.220635] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changez&lt;/P&gt;</description>
    <pubDate>Tue, 20 Jul 2021 08:24:38 GMT</pubDate>
    <dc:creator>sd05</dc:creator>
    <dc:date>2021-07-20T08:24:38Z</dc:date>
    <item>
      <title>Kernel getting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-getting-stuck/m-p/1310279#M177179</link>
      <description>&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;We are using the Zeus Yocto version and we switched the uboot version from 2019 to 2020 and after that Kernel getting stuck with the following errors.&lt;/P&gt;&lt;P&gt;What can we do to resolve this issue?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;Warning: ethernet@30be0000 (eth0) using random MAC address - 26:af:ec:a9:a5:9e&lt;BR /&gt;eth0: ethernet@30be0000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;5746340 bytes read in 77 ms (71.2 MiB/s)&lt;BR /&gt;Uncompressed size: 13113352 = 0xC81808&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;fdt_file=imx8mm-var-dart.dtb&lt;BR /&gt;43335 bytes read in 17 ms (2.4 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt;Booting using the fdt blob at 0x43000000&lt;BR /&gt;Using Device Tree in place at 0000000043000000, end 000000004300d946&lt;BR /&gt;&lt;BR /&gt;Starting kernel ...&lt;BR /&gt;&lt;BR /&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]&lt;BR /&gt;[ 0.000000] Linux version 5.4.3-imx8mm+gb40ccfdb73ea (oe-user@oe-host) (gcc 1&lt;BR /&gt;[ 0.000000] Machine model: Variscite DART-MX8MM&lt;BR /&gt;[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000078000000, B&lt;BR /&gt;[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id sharl&lt;BR /&gt;[ 0.000000] NUMA: No NUMA configuration found&lt;BR /&gt;[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bffffff]&lt;BR /&gt;[ 0.000000] NUMA: NODE_DATA [mem 0xbfbc9800-0xbfbcafff]&lt;BR /&gt;[ 0.000000] Zone ranges:&lt;BR /&gt;[ 0.000000] DMA32 [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] Normal empty&lt;BR /&gt;[ 0.000000] Movable zone start for each node&lt;BR /&gt;[ 0.000000] Early memory node ranges&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]&lt;BR /&gt;[ 0.000000] psci: probing for conduit method from DT.&lt;BR /&gt;[ 0.000000] psci: PSCIv1.1 detected in firmware.&lt;BR /&gt;[ 0.000000] psci: Using standard PSCI v0.2 function IDs&lt;BR /&gt;[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.&lt;BR /&gt;[ 0.000000] psci: SMC Calling Convention v1.1&lt;BR /&gt;[ 0.000000] percpu: Embedded 21 pages/cpu s48664 r8192 d29160 u86016&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;BR /&gt;[ 0.000000] CPU features: detected: ARM erratum 845719&lt;BR /&gt;[ 0.000000] CPU features: detected: GIC system register CPU interface&lt;BR /&gt;[ 0.000000] Speculative Store Bypass Disable mitigation not required&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096&lt;BR /&gt;[ 0.000000] Policy zone: DMA32&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p1 M&lt;BR /&gt;[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)&lt;BR /&gt;[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes,)&lt;BR /&gt;[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off&lt;BR /&gt;[ 0.000000] Memory: 1388060K/2097152K available (7934K kernel code, 582K rwd)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;[ 0.000000] rcu: Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.&lt;BR /&gt;[ 0.000000] Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 ji.&lt;BR /&gt;[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4&lt;BR /&gt;[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0&lt;BR /&gt;[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode&lt;BR /&gt;[ 0.000000] GICv3: 128 SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: 0 Extended SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: Distributor has no Range Selector support&lt;BR /&gt;[ 0.000000] GICv3: 16 PPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: no VLPI support, no direct LPI support&lt;BR /&gt;[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000&lt;BR /&gt;[ 0.000000] ITS: No ITS available, not enabling LPIs&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0x2b4/0x434 wi0&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycless&lt;BR /&gt;[ 0.000003] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199s&lt;BR /&gt;[ 0.000313] Console: colour dummy device 80x25&lt;BR /&gt;[ 0.000369] Calibrating delay loop (skipped), value calculated using timer f)&lt;BR /&gt;[ 0.000380] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.000471] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, lin)&lt;BR /&gt;[ 0.000482] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;[ 0.024004] ASID allocator initialised with 32768 entries&lt;BR /&gt;[ 0.032002] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.052041] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 0.084163] Detected VIPT I-cache on CPU1&lt;BR /&gt;[ 0.084187] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000&lt;BR /&gt;[ 0.084216] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]&lt;BR /&gt;[ 0.116195] Detected VIPT I-cache on CPU2&lt;BR /&gt;[ 0.116211] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000&lt;BR /&gt;[ 0.116229] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]&lt;BR /&gt;[ 0.148243] Detected VIPT I-cache on CPU3&lt;BR /&gt;[ 0.148257] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000&lt;BR /&gt;[ 0.148273] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]&lt;BR /&gt;[ 0.148329] smp: Brought up 1 node, 4 CPUs&lt;BR /&gt;[ 0.148351] SMP: Total of 4 processors activated.&lt;BR /&gt;[ 0.148356] CPU features: detected: 32-bit EL0 Support&lt;BR /&gt;[ 0.148363] CPU features: detected: CRC32 instructions&lt;BR /&gt;[ 0.152336] CPU: All CPU(s) started at EL2&lt;BR /&gt;[ 0.152353] alternatives: patching kernel code&lt;BR /&gt;[ 0.153407] devtmpfs: initialized&lt;BR /&gt;[ 0.158918] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ms&lt;BR /&gt;[ 0.158934] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)&lt;BR /&gt;[ 0.173282] pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;[ 0.174033] NET: Registered protocol family 16&lt;BR /&gt;[ 0.177136] DMA: preallocated 256 KiB pool for atomic allocations&lt;BR /&gt;[ 0.177562] cpuidle: using governor menu&lt;BR /&gt;[ 0.177734] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.&lt;BR /&gt;[ 0.177946] imx mu driver is registered.&lt;BR /&gt;[ 0.177966] imx rpmsg driver is registered.&lt;BR /&gt;[ 0.182134] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.194148] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.194157] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.194162] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.194168] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.198691] iommu: Default domain type: Translated&lt;BR /&gt;[ 0.198792] vgaarb: loaded&lt;BR /&gt;[ 0.199819] mc: Linux media interface: v0.10&lt;BR /&gt;[ 0.199849] videodev: Linux video capture interface: v2.00&lt;BR /&gt;[ 0.199886] pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;[ 0.199891] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giom&amp;gt;&lt;BR /&gt;[ 0.199905] PTP clock support registered&lt;BR /&gt;[ 0.201150] clocksource: Switched to clocksource arch_sys_counter&lt;BR /&gt;[ 0.206391] thermal_sys: Registered thermal governor 'step_wise'&lt;BR /&gt;[ 0.206395] thermal_sys: Registered thermal governor 'power_allocator'&lt;BR /&gt;[ 0.206697] NET: Registered protocol family 2&lt;BR /&gt;[ 0.207067] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 163)&lt;BR /&gt;[ 0.207097] TCP established hash table entries: 16384 (order: 5, 131072 byte)&lt;BR /&gt;[ 0.207205] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, line)&lt;BR /&gt;[ 0.207433] TCP: Hash tables configured (established 16384 bind 16384)&lt;BR /&gt;[ 0.207510] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.207552] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)&lt;BR /&gt;[ 0.207673] NET: Registered protocol family 1&lt;BR /&gt;[ 0.208042] RPC: Registered named UNIX socket transport module.&lt;BR /&gt;[ 0.208048] RPC: Registered udp transport module.&lt;BR /&gt;[ 0.208054] RPC: Registered tcp transport module.&lt;BR /&gt;[ 0.208057] RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;[ 0.208068] PCI: CLS 0 bytes, default 64&lt;BR /&gt;[ 0.208594] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters ae&lt;BR /&gt;[ 0.209680] Initialise system trusted keyrings&lt;BR /&gt;[ 0.209801] workingset: timestamp_bits=44 max_order=19 bucket_order=0&lt;BR /&gt;[ 0.214191] NFS: Registering the id_resolver key type&lt;BR /&gt;[ 0.214215] Key type id_resolver registered&lt;BR /&gt;[ 0.214221] Key type id_legacy registered&lt;BR /&gt;[ 0.214231] nfs4filelayout_init: NFSv4 File Layout Driver Registering...&lt;BR /&gt;[ 0.214498] Key type asymmetric registered&lt;BR /&gt;[ 0.214503] Asymmetric key parser 'x509' registered&lt;BR /&gt;[ 0.214527] Block layer SCSI generic (bsg) driver version 0.4 loaded (major )&lt;BR /&gt;[ 0.214627] io scheduler mq-deadline registered&lt;BR /&gt;[ 0.214632] io scheduler kyber registered&lt;BR /&gt;[ 0.215736] pwm-backlight backlight: backlight supply power not found, usingr&lt;BR /&gt;[ 0.220486] mxs-dma 33000000.dma-controller: initialized&lt;BR /&gt;[ 0.221008] Bus freq driver module loaded&lt;BR /&gt;[ 0.223134] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled&lt;BR /&gt;[ 0.224745] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 30, base_baudX&lt;BR /&gt;[ 0.982507] printk: console [ttymxc0] enabled&lt;BR /&gt;[ 0.987277] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 31, base_baudX&lt;BR /&gt;[ 0.996447] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 32, base_baudX&lt;BR /&gt;[ 1.005670] 30a60000.serial: ttymxc3 at MMIO 0x30a60000 (irq = 38, base_baudX&lt;BR /&gt;[ 1.016859] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).&lt;BR /&gt;[ 1.023509] [drm] No driver support for vblank timestamp query.&lt;BR /&gt;[ 1.029514] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-cr)&lt;BR /&gt;[ 1.038916] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200&lt;BR /&gt;[ 1.046136] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32ei&lt;BR /&gt;[ 1.054470] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim brid7&lt;BR /&gt;[ 1.062254] imx-drm soc@0:bus@32c00000:display-subsystem: failed to bind 32e7&lt;BR /&gt;[ 1.073118] imx-drm soc@0:bus@32c00000:display-subsystem: master bind failed7&lt;BR /&gt;[ 1.082172] libphy: Fixed MDIO Bus: probed&lt;BR /&gt;[ 1.086589] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/so0&lt;BR /&gt;[ 1.100493] i2c /dev entries driver&lt;BR /&gt;[ 1.104185] mx6s-csi 32e20000.csi1_bridge: initialising&lt;BR /&gt;[ 1.109869] mxc_mipi-csi 32e30000.mipi_csi: 32e30000.mipi_csi supply mipi-phr&lt;BR /&gt;[ 1.120034] mxc_mipi-csi 32e30000.mipi_csi: mipi csi v4l2 device registered&lt;BR /&gt;[ 1.127008] CSI: Registered sensor subdevice: mxc_mipi-csi.0&lt;BR /&gt;[ 1.132689] mxc_mipi-csi 32e30000.mipi_csi: lanes: 2, hs_settle: 13, clk_set0&lt;BR /&gt;[ 1.145689] imx2-wdt 30280000.watchdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;[ 1.152840] sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;[ 1.159032] sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;[ 1.163393] sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;[ 1.169628] mmc0: CQHCI version 5.10&lt;BR /&gt;[ 1.204928] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA&lt;BR /&gt;[ 1.212404] mmc1: CQHCI version 5.10&lt;BR /&gt;[ 1.216494] mmc2: CQHCI version 5.10&lt;BR /&gt;[ 1.253416] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA&lt;BR /&gt;[ 1.262302] ledtrig-cpu: registered to indicate activity on CPUs&lt;BR /&gt;[ 1.269213] caam 30900000.crypto: device ID = 0x0a16040100000000 (Era 9)&lt;BR /&gt;[ 1.275969] caam 30900000.crypto: job rings = 3, qi = 0&lt;BR /&gt;[ 1.292822] caam algorithms registered in /proc/crypto&lt;BR /&gt;[ 1.299553] caam 30900000.crypto: caam pkc algorithms registered in /proc/cro&lt;BR /&gt;[ 1.309105] caam_jr 30901000.jr0: registering rng-caam&lt;BR /&gt;[ 1.316744] caam-snvs 30370000.caam-snvs: can't get snvs clock&lt;BR /&gt;[ 1.322769] caam-snvs 30370000.caam-snvs: violation handlers armed - non-sece&lt;BR /&gt;[ 1.331092] hidraw: raw HID events driver (C) Jiri Kosina&lt;BR /&gt;[ 1.339734] NET: Registered protocol family 17&lt;BR /&gt;[ 1.344273] 8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;[ 1.348507] Key type dns_resolver registered&lt;BR /&gt;[ 1.353301] Loading compiled-in X.509 certificates&lt;BR /&gt;[ 1.375401] regulator-eth-phy GPIO handle specifies active low - ignored&lt;BR /&gt;[ 1.382646] gpio-142 (scl): enforced open drain please flag it properly in De&lt;BR /&gt;[ 1.392626] rohm-bd718x7 0-004b: Failed to set masks in 0x2a: -6&lt;BR /&gt;[ 1.398659] rohm-bd718x7 0-004b: Failed to add irq_chip&lt;BR /&gt;[ 1.404091] i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;[ 1.409176] gpio-144 (scl): enforced open drain please flag it properly in De&lt;BR /&gt;[ 1.419161] mmc2: Command Queue Engine enabled&lt;BR /&gt;[ 1.423626] mmc2: new HS400 MMC card at address 0001&lt;BR /&gt;[ 1.429366] mmcblk2: mmc2:0001 S0J56X 14.8 GiB&lt;BR /&gt;[ 1.434038] mmcblk2boot0: mmc2:0001 S0J56X partition 1 31.5 MiB&lt;BR /&gt;[ 1.440085] mmcblk2boot1: mmc2:0001 S0J56X partition 2 31.5 MiB&lt;BR /&gt;[ 1.446725] mmcblk2rpmb: mmc2:0001 S0J56X partition 3 4.00 MiB, chardev (244)&lt;BR /&gt;[ 1.458683] mmcblk2: p1&lt;BR /&gt;[ 1.757739] i2c i2c-1: SCL is stuck low, exit recovery&lt;BR /&gt;[ 1.763057] edt_ft5x06 1-0038: touchscreen probe failed&lt;BR /&gt;[ 1.768418] edt_ft5x06: probe of 1-0038 failed with error -11&lt;BR /&gt;[ 1.774496] ov5640_mipi 1-003c: 1-003c supply DOVDD not found, using dummy rr&lt;BR /&gt;[ 1.782299] ov5640_mipi 1-003c: 1-003c supply DVDD not found, using dummy rer&lt;BR /&gt;[ 1.789992] ov5640_mipi 1-003c: 1-003c supply AVDD not found, using dummy rer&lt;BR /&gt;[ 1.869702] i2c i2c-1: SCL is stuck low, exit recovery&lt;BR /&gt;[ 1.875019] ov5640_mipi 1-003c: Read reg error: reg=300a&lt;BR /&gt;[ 1.880339] ov5640_mipi 1-003c: Camera is not found&lt;BR /&gt;[ 1.885342] i2c i2c-1: IMX I2C adapter registered&lt;BR /&gt;[ 1.890413] gpio-146 (scl): enforced open drain please flag it properly in De&lt;BR /&gt;[ 1.899966] i2c i2c-2: IMX I2C adapter registered&lt;BR /&gt;[ 1.904989] gpio-148 (scl): enforced open drain please flag it properly in De&lt;BR /&gt;[ 1.914784] i2c i2c-3: IMX I2C adapter registered&lt;BR /&gt;[ 1.919849] pwm-backlight backlight: backlight supply power not found, usingr&lt;BR /&gt;[ 1.928762] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).&lt;BR /&gt;[ 1.935384] [drm] No driver support for vblank timestamp query.&lt;BR /&gt;[ 1.941358] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-cr)&lt;BR /&gt;[ 1.950734] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200&lt;BR /&gt;[ 1.957963] panel-sitronix-st7703 32e10000.mipi_dsi.0: 32e10000.mipi_dsi.0 sr&lt;BR /&gt;[ 1.968704] panel-sitronix-st7703 32e10000.mipi_dsi.0: 32e10000.mipi_dsi.0 sr&lt;BR /&gt;[ 1.979608] panel-sitronix-st7703 32e10000.mipi_dsi.0: 640x1280@60 24bpp dsiy&lt;BR /&gt;[ 1.987754] imx-drm soc@0:bus@32c00000:display-subsystem: bound 32e10000.mip)&lt;BR /&gt;[ 1.998139] [drm] Initialized imx-drm 1.0.0 20120507 for soc@0:bus@32c00000:0&lt;BR /&gt;[ 3.170883] Console: switching to colour frame buffer device 80x80&lt;BR /&gt;[ 3.195221] imx-drm soc@0:bus@32c00000:display-subsystem: fb0: imx-drmdrmfb e&lt;BR /&gt;[ 3.204167] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 2 mkt segment 2 s4&lt;BR /&gt;[ 3.213280] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 500000 z&lt;BR /&gt;[ 3.220635] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changez&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jul 2021 08:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-getting-stuck/m-p/1310279#M177179</guid>
      <dc:creator>sd05</dc:creator>
      <dc:date>2021-07-20T08:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel getting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-getting-stuck/m-p/1310417#M177196</link>
      <description>&lt;P&gt;Hi Sunidhi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;from log : "Linux version 5.4.3-imx8mm", linux 5.4.3 was used while for uboot version 2020&lt;/P&gt;
&lt;P&gt;linux 5.4.24 version or newer is required, so may be suggested to upgrade linux:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/varigit/linux-imx/tree/imx_5.4.24_2.1.0_var01" target="_blank"&gt;https://github.com/varigit/linux-imx/tree/imx_5.4.24_2.1.0_var01&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jul 2021 11:30:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-getting-stuck/m-p/1310417#M177196</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-07-20T11:30:14Z</dc:date>
    </item>
  </channel>
</rss>