<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8M PLUS LPDDR4 routing recommendations in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-PLUS-LPDDR4-routing-recommendations/m-p/1309783#M177140</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm designing the PCB with i.MX8M Plus according to&lt;BR /&gt;"i.MX 8M Plus Hardware Developer's Guide, Rev.0, 03/2021".&lt;/P&gt;&lt;P&gt;I cannot meet the following two recommendations at the same time.&lt;/P&gt;&lt;P&gt;(A). On Page 22, it is recommended that "11. In general, the 200-ball LPDDR4 package should be placed 200 mils from the i.MX 8M Plus&lt;BR /&gt;(B). In Table 20, it is recommended that "CA3, CA2, CA1, CA0 match within 2ps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In my present design, (A) is OK, but (B) is NG.&lt;BR /&gt;CA3, CA2, CA1, CA0 matches only within 48ps.&lt;/P&gt;&lt;P&gt;On the other hand, CA3, CA2, CA1, CA0 can match within CK_t +- 50ps.&lt;/P&gt;&lt;P&gt;Do I have to consider (B)?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If (B) is mandatory, Can I igone (A)?&lt;BR /&gt;If I ignore (A) and place LPDDR4 300mils from the SoC, I expect to be able to consider (B).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you for your reply.&lt;/P&gt;</description>
    <pubDate>Mon, 19 Jul 2021 10:41:29 GMT</pubDate>
    <dc:creator>shimpei_sonoda</dc:creator>
    <dc:date>2021-07-19T10:41:29Z</dc:date>
    <item>
      <title>i.MX8M PLUS LPDDR4 routing recommendations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-PLUS-LPDDR4-routing-recommendations/m-p/1309783#M177140</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm designing the PCB with i.MX8M Plus according to&lt;BR /&gt;"i.MX 8M Plus Hardware Developer's Guide, Rev.0, 03/2021".&lt;/P&gt;&lt;P&gt;I cannot meet the following two recommendations at the same time.&lt;/P&gt;&lt;P&gt;(A). On Page 22, it is recommended that "11. In general, the 200-ball LPDDR4 package should be placed 200 mils from the i.MX 8M Plus&lt;BR /&gt;(B). In Table 20, it is recommended that "CA3, CA2, CA1, CA0 match within 2ps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In my present design, (A) is OK, but (B) is NG.&lt;BR /&gt;CA3, CA2, CA1, CA0 matches only within 48ps.&lt;/P&gt;&lt;P&gt;On the other hand, CA3, CA2, CA1, CA0 can match within CK_t +- 50ps.&lt;/P&gt;&lt;P&gt;Do I have to consider (B)?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If (B) is mandatory, Can I igone (A)?&lt;BR /&gt;If I ignore (A) and place LPDDR4 300mils from the SoC, I expect to be able to consider (B).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you for your reply.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 10:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-PLUS-LPDDR4-routing-recommendations/m-p/1309783#M177140</guid>
      <dc:creator>shimpei_sonoda</dc:creator>
      <dc:date>2021-07-19T10:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M PLUS LPDDR4 routing recommendations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-PLUS-LPDDR4-routing-recommendations/m-p/1312249#M177373</link>
      <description>&lt;P&gt;Hi Shimpei&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;if it is not possible to follow those two recommendations at the same time, recommended&lt;/P&gt;
&lt;P&gt;to use ibis modelling to verify that timings conform to memory specifications.&lt;/P&gt;
&lt;H5 class="design-res-title"&gt;&lt;A id="designResources_title2" href="https://www.nxp.com/lgfiles/bsps/ibis_imx8mp_v2_20201023.zip" data-dtmaction="Software &amp;amp; Tools tab: Developer Resources - Download Link click" data-dtmsubaction="i.MX 8M Plus 15x15 IBIS Model" target="_blank"&gt;i.MX 8M Plus 15x15 IBIS Model&lt;/A&gt;&lt;/H5&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jul 2021 00:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-PLUS-LPDDR4-routing-recommendations/m-p/1312249#M177373</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-07-23T00:21:14Z</dc:date>
    </item>
  </channel>
</rss>