<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6 eCSPI Write/Read Timing Understanding</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eCSPI-Write-Read-Timing-Understanding/m-p/1309513#M177111</link>
    <description>&lt;P&gt;In looking at the Electrical Characteristics for the i.MX6 ULL processor (IMX6ULLCED PDF), Figure 35 and Table 47 indicate that there is a SPI Write timing of 15ns while there is a SPI Read Timing of 43ns (CS1) in Master Mode.&lt;BR /&gt;&lt;BR /&gt;I read this to mean that the MISO data will not be registered correctly by the i.MX6 ULL processor if the i.MX6 is generating a SPI SCLK at a frequency greater than 23MHz (43ns). Therefore, if the i.MX6 wants to be able to register MISO data correctly, it must always run with a SPI clock slower than 43ns, or change between a faster clock when it doesn't care about the MISO data and a slower clock, when it does care to receive valid data.&lt;/P&gt;&lt;P&gt;Is this a correct understanding of these two timing parameters?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;</description>
    <pubDate>Mon, 19 Jul 2021 04:46:31 GMT</pubDate>
    <dc:creator>chris_lambrecht</dc:creator>
    <dc:date>2021-07-19T04:46:31Z</dc:date>
    <item>
      <title>i.MX6 eCSPI Write/Read Timing Understanding</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eCSPI-Write-Read-Timing-Understanding/m-p/1309513#M177111</link>
      <description>&lt;P&gt;In looking at the Electrical Characteristics for the i.MX6 ULL processor (IMX6ULLCED PDF), Figure 35 and Table 47 indicate that there is a SPI Write timing of 15ns while there is a SPI Read Timing of 43ns (CS1) in Master Mode.&lt;BR /&gt;&lt;BR /&gt;I read this to mean that the MISO data will not be registered correctly by the i.MX6 ULL processor if the i.MX6 is generating a SPI SCLK at a frequency greater than 23MHz (43ns). Therefore, if the i.MX6 wants to be able to register MISO data correctly, it must always run with a SPI clock slower than 43ns, or change between a faster clock when it doesn't care about the MISO data and a slower clock, when it does care to receive valid data.&lt;/P&gt;&lt;P&gt;Is this a correct understanding of these two timing parameters?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 04:46:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eCSPI-Write-Read-Timing-Understanding/m-p/1309513#M177111</guid>
      <dc:creator>chris_lambrecht</dc:creator>
      <dc:date>2021-07-19T04:46:31Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 eCSPI Write/Read Timing Understanding</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eCSPI-Write-Read-Timing-Understanding/m-p/1309546#M177114</link>
      <description>&lt;P&gt;Hi Chris&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;yes your understanding is correct.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 05:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eCSPI-Write-Read-Timing-Understanding/m-p/1309546#M177114</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-07-19T05:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 eCSPI Write/Read Timing Understanding</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eCSPI-Write-Read-Timing-Understanding/m-p/1310177#M177168</link>
      <description>&lt;P&gt;Thanks!!&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jul 2021 04:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eCSPI-Write-Read-Timing-Understanding/m-p/1310177#M177168</guid>
      <dc:creator>chris_lambrecht</dc:creator>
      <dc:date>2021-07-20T04:17:30Z</dc:date>
    </item>
  </channel>
</rss>