<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX 8QXP DDR Stress Test</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1308715#M177025</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The default setting of SCFW is 3GB, change it to 4GB, rebuild SCFW and change scfw_download.bin in ddr_strss_test.&lt;/P&gt;</description>
    <pubDate>Fri, 16 Jul 2021 01:24:53 GMT</pubDate>
    <dc:creator>carolyn_zhang</dc:creator>
    <dc:date>2021-07-16T01:24:53Z</dc:date>
    <item>
      <title>i.MX 8QXP DDR Stress Test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1152778#M161740</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There is a 4GB DDR4 on my board, then I do the DDR stress test, region 2 is failed, it could not go to t0.2. However, it is ok if I set the device information as same as the MEK board, which means it is ok when I tested as 3GB DDR4. Could someone give me some advices please? Thanks.&lt;/P&gt;&lt;P&gt;The log is:&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;MX8 DDR Stress Test Version: ER14&lt;BR /&gt;Built on Mar 27 2020 12:28:23&lt;BR /&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;--Set up the MMU and enable I and D cache--&lt;BR /&gt;- This is the Cortex-A35 core&lt;BR /&gt;- Check if I cache is enabled&lt;BR /&gt;- Enabling I cache since it was disabled&lt;BR /&gt;- Push base address of TTB to TTBR0_EL3&lt;BR /&gt;- Config TCR_EL3&lt;BR /&gt;- Config MAIR_EL3&lt;BR /&gt;- Enable MMU&lt;BR /&gt;- Data Cache has been enabled&lt;BR /&gt;- Check system memory register, only for debug&lt;/P&gt;&lt;P&gt;- VMCR Check:&lt;BR /&gt;- ttbr0_el3: 0x13d000&lt;BR /&gt;- tcr_el3: 0x2051c&lt;BR /&gt;- mair_el3: 0x774400&lt;BR /&gt;- sctlr_el3: 0xc01815&lt;BR /&gt;- id_aa64mmfr0_el1: 0x101122&lt;/P&gt;&lt;P&gt;- MMU and cache setup complete&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;ARM Clock(CA35): 1200MHz&lt;BR /&gt;DDR Clock: 1200MHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;DDR type is LPDDR4&lt;BR /&gt;Data width: 32, bank num: 8&lt;BR /&gt;Row size: 16, col size: 10&lt;BR /&gt;Two chip selects are used&lt;BR /&gt;Number of DDR controllers used on the SoC: 1&lt;BR /&gt;Density per chip select: 2048MB&lt;BR /&gt;Density per controller is: 4096MB&lt;BR /&gt;Total density detected on the board is: 4096MB&lt;/P&gt;&lt;P&gt;Command Bus Training was executed&lt;BR /&gt;No DDR data training errors detected for DDRC0&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;MX8QXP: Cortex-A35 is found&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;DDR Stress Test Iteration 1&lt;BR /&gt;--------------------------------&lt;BR /&gt;--Running DDR test on region 1--&lt;BR /&gt;--------------------------------&lt;/P&gt;&lt;P&gt;t0.1: data is addr test&lt;BR /&gt;....&lt;BR /&gt;t0.2: row hop read test&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;t1: memcpy SSN armv8_x32 test&lt;BR /&gt;....&lt;BR /&gt;t2: byte-wise SSN armv8_x32 test&lt;BR /&gt;..&lt;BR /&gt;t3: memcpy pseudo random pattern test&lt;BR /&gt;....................................................................&lt;BR /&gt;t4: IRAM_to_DDRv1 test&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;t5: IRAM_to_DDRv2 test&lt;BR /&gt;--------------------------------&lt;BR /&gt;--Running DDR test on region2--&lt;BR /&gt;--------------------------------&lt;/P&gt;&lt;P&gt;t0.1: data is addr test&lt;BR /&gt;...&lt;/P&gt;</description>
      <pubDate>Mon, 14 Sep 2020 09:23:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1152778#M161740</guid>
      <dc:creator>carolyn_zhang</dc:creator>
      <dc:date>2020-09-14T09:23:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8QXP DDR Stress Test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1152852#M161744</link>
      <description>&lt;P&gt;Hi&amp;nbsp;carolyn_zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can check that latest RPA tool was used and versions of&lt;/P&gt;
&lt;P&gt;RPA tool, SCFW and kernel were aligned to each other as described on below link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 14 Sep 2020 10:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1152852#M161744</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-09-14T10:29:31Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8QXP DDR Stress Test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1153109#M161785</link>
      <description>&lt;P&gt;Hi, Igorpadykov,&lt;/P&gt;&lt;P&gt;Thanks for your reply, but the website is useless since community changed a new revision. However, I have solved this problem by modified SCFW.&lt;/P&gt;&lt;P&gt;Thank you all the same.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 01:42:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1153109#M161785</guid>
      <dc:creator>carolyn_zhang</dc:creator>
      <dc:date>2020-09-15T01:42:17Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8QXP DDR Stress Test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1153110#M161786</link>
      <description>&lt;P&gt;Totally speaking, I don't like the new community, it always show 'Article or Comment Not Found'.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 01:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1153110#M161786</guid>
      <dc:creator>carolyn_zhang</dc:creator>
      <dc:date>2020-09-15T01:44:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8QXP DDR Stress Test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1308506#M177013</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/163145"&gt;@carolyn_zhang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I have the same problem on our custom board can you share with me your fix to figure out on this problem.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;Tommaso&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jul 2021 15:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1308506#M177013</guid>
      <dc:creator>scott3303</dc:creator>
      <dc:date>2021-07-15T15:13:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8QXP DDR Stress Test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1308715#M177025</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The default setting of SCFW is 3GB, change it to 4GB, rebuild SCFW and change scfw_download.bin in ddr_strss_test.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jul 2021 01:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QXP-DDR-Stress-Test/m-p/1308715#M177025</guid>
      <dc:creator>carolyn_zhang</dc:creator>
      <dc:date>2021-07-16T01:24:53Z</dc:date>
    </item>
  </channel>
</rss>